Code Exchange
  • Technologies
  • More
Code Exchange
Forum Python 3 code Question
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 3 answers
  • Subscribers 53 subscribers
  • Views 3336 views
  • Users 0 members are here
  • Code Exchange
Related

Python 3 code Question

ellip
ellip over 9 years ago

Hi.  I am new to the Raspberry Pi.  I have a Raspberry Pi 3 and a PiFace 2.  I am trying to update a Christmas decoration made over 40 years ago by my father. It was run by a rotisserie motor and a wooden cylinder with copper strips and screws to make contact and light the stars up in sequences.

 

I have 5 stars in the following formation:

 

     1          2

 

          5

 

     4          3

 

I am trying to have the stars light up in a certain sequence with a small delay in between each function

 

1

2

3

4

5

1,2,3

2,3,4

3,4,1

4,1,2

1,2,5

2,3,5

3,4,5

4,5,1

1,2,3,4,5

then begin the sequence again.

I have tried following as many of the posts as I can and receive errors on everything from syntax to int and tuples.

I am sure that it is something that is simple to the rest of you but just eludes me.  Any help in any way will be greatly appreciated.

Elli

  • Sign in to reply
  • Cancel

Top Replies

  • jdlui
    jdlui over 9 years ago +3 suggested
    Hi Ellen, Suggestion: With any problem I think it's helpful try and break things into pieces. Share more info with us on what you've tried, what isn't working, what code you are using. I.E. Have you tested…
  • mgillett
    mgillett over 8 years ago in reply to dougw +3
    I appreciated the two of you demonstrating two solutions to this problem. Further I appreciate seeing the first examples of going line by line through the code then the "better" coding style making the…
  • urkraft
    urkraft over 9 years ago in reply to urkraft +1 suggested
    To Douglas Wong: Sorry, i see now that your post was not directed to me. Was not very focused when i read it. I did notice that there was a very important bug in my code in that it did not handle interrupts…
Parents
  • jdlui
    0 jdlui over 9 years ago

    Hi Ellen,

     

    Suggestion: With any problem I think it's helpful try and break things into pieces. Share more info with us on what you've tried, what isn't working, what code you are using.

    I.E. Have you tested a basic python script to get PiFace to turn on a single light yet? Confirm that this is working before you proceed. Test it on a random light like an LED. Then test it on your ornament.

     

    Hardware - PiFace

    I've never worked with PiFace so I don't know what your hookup options are to your ornament. I assume you have already made your electrical connections? Completed to the point where you can turn on a light if you run some basic blink script? There seems to

     

     

    Code - The Loop

    What code have you tried so far? Share it and we can help you more easily.

    Here is an example code that will look through your lighting combinations. This will go through each lighting combination and wait 1 second in between. Try running it and see how it works. You can modify the wait time as well.

     

    Hope this helps!

     

    J

     

    import time
    # Example of a script to cycle through and change light sequence
    
    
    # Every lighting combination can be summarized as a '1' for an on light and an '0' for an off light.
    # Those combinations are shown below.
    lights = ['10000','01000','00100','00010','00001','11100','01110','10110','11010','11001','01101','00111','10011','11111']
    
    
    # Define wait time for our function
    waittime = 1 # Number of seconds between light sequences, measured in seconds.
    
    
    # We want this script to run perpetually so we create a while True loop
    while True:
      # We iterate through each item in our list of light combinations, which is called 'lights'
      for index,item in enumerate(lights):
      # Putting a bunch of text print outs so you can see how the loop iterates
      print('We are now printing combination number',index+1,'in our light sequence')
      print('Light combination is',item)
    
      # Here is where you would send the data to the PiFace to control its lighting.
      print('If we send these commands to a lighting system \nlight 1 is',item[0],'light 2 is',item[1],'light 3 is',item[2],'light 4 is',item[3],'light 5 is',item[4],'\n')
      # Insert some lighting command here. Use the on/off data stored in the item variable to turn your lights on or off.
    
    
    
    
      # Now we use time command to put a delay in between lighting instruction
      time.sleep(waittime)
      print('Completed all sequences. repeating')

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jdlui
    0 jdlui over 9 years ago

    Hi Ellen,

     

    Suggestion: With any problem I think it's helpful try and break things into pieces. Share more info with us on what you've tried, what isn't working, what code you are using.

    I.E. Have you tested a basic python script to get PiFace to turn on a single light yet? Confirm that this is working before you proceed. Test it on a random light like an LED. Then test it on your ornament.

     

    Hardware - PiFace

    I've never worked with PiFace so I don't know what your hookup options are to your ornament. I assume you have already made your electrical connections? Completed to the point where you can turn on a light if you run some basic blink script? There seems to

     

     

    Code - The Loop

    What code have you tried so far? Share it and we can help you more easily.

    Here is an example code that will look through your lighting combinations. This will go through each lighting combination and wait 1 second in between. Try running it and see how it works. You can modify the wait time as well.

     

    Hope this helps!

     

    J

     

    import time
    # Example of a script to cycle through and change light sequence
    
    
    # Every lighting combination can be summarized as a '1' for an on light and an '0' for an off light.
    # Those combinations are shown below.
    lights = ['10000','01000','00100','00010','00001','11100','01110','10110','11010','11001','01101','00111','10011','11111']
    
    
    # Define wait time for our function
    waittime = 1 # Number of seconds between light sequences, measured in seconds.
    
    
    # We want this script to run perpetually so we create a while True loop
    while True:
      # We iterate through each item in our list of light combinations, which is called 'lights'
      for index,item in enumerate(lights):
      # Putting a bunch of text print outs so you can see how the loop iterates
      print('We are now printing combination number',index+1,'in our light sequence')
      print('Light combination is',item)
    
      # Here is where you would send the data to the PiFace to control its lighting.
      print('If we send these commands to a lighting system \nlight 1 is',item[0],'light 2 is',item[1],'light 3 is',item[2],'light 4 is',item[3],'light 5 is',item[4],'\n')
      # Insert some lighting command here. Use the on/off data stored in the item variable to turn your lights on or off.
    
    
    
    
      # Now we use time command to put a delay in between lighting instruction
      time.sleep(waittime)
      print('Completed all sequences. repeating')

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer