Code Exchange
  • Technologies
  • More
Code Exchange
Forum How are flocks connecting there RPI with external world(Other embedded circuits)? any standards.. if not which 1 you will pick?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 55 subscribers
  • Views 3627 views
  • Users 0 members are here
  • 32bit
  • raspbpi
  • raspcontrol
  • Code Exchange
  • programming
  • embedded
  • raspberry_pi_rev_2
  • arm
  • arduino
  • atmel
Related

How are flocks connecting there RPI with external world(Other embedded circuits)? any standards.. if not which 1 you will pick?

shahbhaumik
shahbhaumik over 13 years ago

There are various option when it comes to connect RPI with external embedded boards. Currently many geeks are trying to interface various peripherals with RPI with the I/O header given. I feel there are following option one can go with.

 

1) Use I/O header.

Which i feel is good for prototyping but as we move do something that looks good this option is not what I feel is best, I hate all the wires that comes out of RPI and then loose connection and what not to take care of...

 

2) Use of USB port.

RPI is computer and you it can communicate to co-processor using its USB ports.I think this is very neat way to do things. For example if you are making a robot which has a microcontroller that has UART it can easily communicate with RPI above that you can reflash you microcontroller as per your application using RPI. I know there are no instruction or related work out there like this but soon i will be posting instruction to do this on my blog as well on code exchange.

 

 

Would like to now community views on same.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago +1
    Thus far I've been using the Adafruit Pi Cobbler Adafruit Pi Cobbler to interface the header with a breadboard and programming in Python using libraries like RPi.GPIO . I've really enjoyed Adafruit's tutorials…
  • morgaine
    morgaine over 13 years ago in reply to fustini +1
    Since you've already dealt with 1) Use I/O header , and 2) Use of USB port , I think I'll add the missing alternative, 3) Use of Ethernet . Some people consider USB a fixture and a sacred cow, but I've…
  • morgaine
    morgaine over 13 years ago in reply to gdstew +1
    On the issue of Ethernet complexity, I can't help you further since you refuse to use the engineering concept of dividing a communications stack into layers so that properties of single layers can be discused…
Parents
  • fustini
    0 fustini over 13 years ago

    Thus far I've been using the Adafruit Pi CobblerAdafruit Pi Cobbler to interface the header with a breadboard and programming in Python using libraries like RPi.GPIO.  I've really enjoyed Adafruit's tutorials: http://learn.adafruit.com/category/raspberry-pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to fustini

    Since you've already dealt with 1) Use I/O header, and 2) Use of USB port, I think I'll add the missing alternative, 3) Use of Ethernet.

     

    Some people consider USB a fixture and a sacred cow, but I've been of the opinion that it's a bit of a poor man's alternative to Ethernet ever since USB was released.  Maybe USB had a point in the very early days when Ethernet was still a bit bulky and costly, but that doesn't apply today.  Everything that USB does in 2012 could be done far more effectively and flexibly with Ethernet, and with IPv6 even more so because autoconfiguration makes IPv6 as plug'n'play as USB.

     

    What's more, with IP addresses being extremely plentiful under IPv6, you can easliy conceive of hundreds or millions of sensors connected by IP, and of course this is exactly what the Internet of Things is already engaged in doing.  And if your interest is in local communications only, and you have no interest in higher-level protocols or the Internet in your application, then raw Ethernet provides an extremely fast and efficient way of transferring data within a local set of boards or machines.

     

    All of which is a preamble to my recommendation:  "Think big, think ahead".  Why not make every sensor, actuator, slave and controller in your system networked, linked together by cheap Etherent switches, and even powered from Ethernet using PoE to eliminate power supplies?  All the bits you need are available, so it's more a case of thinking differently than doing research.

     

    Of course you'll still need the GPIO headers to connect the Pi to low level devices, but when it comes to connecting together such boards into a system, I really think Ethernet (and IPv6) is the way to go.  The very low cost of the Pi helps a lot of course.

     

    Once networked, you'll find your system's abilities expanding rapidly, because the net is a very synergistic place where everything piggybacks on everything else and new emergent phenomena appear every day.  I think you'd benefit from that.

     

    So would everybody else, but few people seem to realize it. image

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    ... and of course this is exactly what the Internet of Things is already engaged in doing...

    Personally, I think the "Internet of Things" (IoT) should be called the "Internet of Digital Things" (IoDiT).  I think the latter acronym -- with a small permutation -- captures the concept very nicely.

     

    I do like Ethernet, but it's costly, complex, and IMO overkill for applications that USB does well.  I rather like USB at the physical and packet layers.  I have yet to delve into USB software, which so far looks like Software Engineering with Cats.  Toot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I do like Ethernet, but it's costly, complex, and IMO overkill for applications that USB does well.

     

    It used to be costly, but it is no more.  As long as your project isn't literally counting pennies (and some really are, so fair enough there), the cost differences are minimal, and easily pay for themselves in extra functionality.

     

    I'm not an expert in USB so I can't compare its complexity properly with that of Ethernet, but Ethernet is extremely simple, and what little I do I know of USB suggests that it is extremely complex despite being so limited.  I think it had a role in its day, but frankly I don't understand why we're still using it when Ethernet is so much better.

     

    And finally, overkill ... well that's like saying that USB is overkill when we could be using the simpler RS232.  I don't think the "overkill" concept really means much in this context, but if we have to use the term then I'd say that USB is overkill when Ethernet does the job. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago in reply to morgaine

    Moraine said: and what little I do I know of USB suggests that it is extremely complex despite being so limited

     

    Yea you really should read up on the subject, otherwise your "logic" may be flawed.

     

    1) With USB you can guaranty the amount of bandwidth needed will be avaialable (within the amount available of course) which you can not do with Ethernet.

    2) With USB you can guaranty latency (at least to the millisecond, although this also depends on the processor of course) which you can not do with Ethernet.

    3) Most of the "complexity" is in the driver where it belongs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 13 years ago in reply to morgaine

    Moraine said: and what little I do I know of USB suggests that it is extremely complex despite being so limited

     

    Yea you really should read up on the subject, otherwise your "logic" may be flawed.

     

    1) With USB you can guaranty the amount of bandwidth needed will be avaialable (within the amount available of course) which you can not do with Ethernet.

    2) With USB you can guaranty latency (at least to the millisecond, although this also depends on the processor of course) which you can not do with Ethernet.

    3) Most of the "complexity" is in the driver where it belongs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 13 years ago in reply to gdstew

    Actually, Ethernet and IP has mechanisms for marking your hi-pri traffic.

    Latency can easily be sub-millisecond on same-network.

    However, often it is possible to design (depends on the use-case) so that you don't

    need high bandwidth or low latency.

    Personally I'm a fan of RS232-like asynch protocols and Ethernet.

    USB has its uses too of course.

    IoT will see a lot more IP being used, with varying physical layers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago in reply to shabaz

    shabaz,

     

    Yes but it can not and does not guaranty it. One problem with the USB latency/bandwidth guaranties is that on a

    given host to device interface you can only guaranty one or the other, not both at the same time.

     

    You can also use a USB interface exactly like you would with a RS-232RS-232 interface. I have a device I designed with

    a microprocessor that only has a async serial port. The serial port is connected to an FTDI-232BM serial to USB

    converter. It plugs into the host USB interface but the programming interface is just like any normal serial port. I

    did this for several reasons. The microprocessor I was using did not have a USB interface. The USB interface

    provides the power for the device, and by adding a RS232 level converter (on a header provided for this), it can

    be used with a normal serial port too, although it then needs and external power supply. The sofware to use the

    device is the same for both interfaces, only the /dev name is different depending on which one is being used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    Yea you really should read up on the subject, otherwise your "logic" may be flawed.

     

    1) With USB you can guaranty the amount of bandwidth needed will be avaialable (within the amount available of course) which you can not do with Ethernet.

    2) With USB you can guaranty latency (at least to the millisecond, although this also depends on the processor of course) which you can not do with Ethernet.

    3) Most of the "complexity" is in the driver where it belongs.

     

    Your points confirm what my limited knowledge of USB had suggested exactly.  USB has so much more built in that it is hugely more complex than Ethernet, which is just a very low level unverified frame transfer mechanism.

     

    So neither was my logic flawed nor were the observations that my minimal acquaintance had suggested flawed, you've proved that they were spot on.  In contrast, your conclusion about their comparative complexity is clearly incorrect by your own observations.

     

    Higher levels of protocol that ride on top of Ethernet are not Ethernet, and do not contribute to the complexity of Ethernet.  For what it's worth though, the complexity of upper layers is all in the kernel where it belongs and transparent to users and applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago in reply to morgaine

    No Morgaine you logic is terribly and obviously flawed. You don't have the easy programming interface to Ethernet you claim as its main

    advantage without the upper level protocols. That is after all exactly what they are for and why everybody uses them. Otherwise you will

    have to talk directly to the Ethernet driver at some slightly higher level of abstraction to remove hardware dependencies. This means that

    at least part of the "user" interface you will have to write will run in kernel space probably as a loadable module and have to send data

    back and forth between user and kernel space. Yea this is getting easier all the time (/sarcasm).

     

    With USB, all the complexity you fear is in the host kernel driver as it should be. You only have to deal with the "easy" API which is

    again, why such things exits. If you don't need all the complexity (guaranteed latency or bandwidth) or have a CPU that has trouble

    handling it, you can use a much less complicated host kernel driver for it and still have the "easy" upper level API to deal with. This

    is what USB OTG does. There are different, much, much less complex requirements for the device side driver. If you don't understand

    what that means read up on USB. I don't have a hundred pages to explain it to you. So logically speaking of course, you do requre

    knowledge of USB to make "logical" arguments, DUH.

     

    P.S. Still waiting on the "logical" scientifically based engineering explanation of your data 100% reliability (your exact  somewhat stilted

           phrasing) requirement for the Raspberry Pi, or in your belief in its current availability on any other computer on Earth for that matter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    USB has so much more built in that it is hugely more complex than Ethernet, which is just a very low level unverified [it is verified, but not corrected] frame transfer mechanism...

     

    Higher levels of protocol that ride on top of Ethernet are not Ethernet, and do not contribute to the complexity of Ethernet...

    USB does define the packet and software layers, so yes, if you ignore those parts of an Ethernet-based communctions stack that does give Ethernet an advantage.  So it seems to me that if you're going to make a fair comparison, you really need to do it layer by layer.  At the physical level, they're pretty similar complexity.  However, with Ethernet 100baseT you do have the complexity of MLT-3, and 1000baseT is loads of fun using all four pairs.  In contrast, I believe USB-3.0 just uses 8B10B coding.  You do have scrambling with both.  USB doesn't have to drive as far, so you can use lower-power drivers.  USB also gives you power for free, while PoE is an extra-cost option.  Ethernet Auto-MDIX is fun, something you don't need with USB since it's half duplex.  Let's ignore WiFi and Ethernet-level support for IEEE-1588 Precision Timing Protocol.

     

    The link layers are similar, with best effort data transfers.  However, USB does give you single-packet loss detection, so you don't need the higher-level protocol to handle it.  USB hubs are very simple devices, since the flow is always between host and device and you don't need to store much.  An Ethernet hub is likewise very simple, but nobody uses those nowadays.  Instead, you have Ethernet switches, which implement bridge functionality in hardware.  Bridge functionality is nasty, since the bridge has to learn the MAC addresses of frames coming in each port so it doesn't have to broadcast, and there's a limited amount of frame buffering in the switch, and you need to implement flow control, and you need to auto-negotiate to determine whether to implement flow control, and which speed to use, and whether you can do full duplex.

     

    And then you have Spanning Tree Protocol.  That's a fun algorithm.  There's a quote that reading the STP standard is a good cure for insomnia, and thinking about it can be an effective contraceptive as well.  If STP is too simple for you, how about Rapid STP?  Since USB is physically limited to tree interconnect, there's no STP.  Yes, if you're making an end device you don't need to worry about STP, but it's fair to compare USB tree enumeration with Ethernet STP as far as complexity is concerned.

     

    We're still at the link layer and haven't started sending any networking packets yet.

     

    I've done a lot of work with Ethernet hardware and software, and there's a lot of complexity there.  I haven't done actual implementation of USB, but I've read a lot of the USB 2.0 standard and IMO the USB physical and link layers are simpler.  Ethernet is a lot more versatile since it's peer-to-peer and can drive 100m, and higher performance since it's full duplex, supports multiple simultaneous data streams, and isn't polled.  But that comes with higher-cost components, more board area, and higher power budget.

     

    Like many tools in an engineer's bag of tricks, each has its advantages, disadvantages, and uses.

    JMO/YMMV

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    No Morgaine you logic is terribly and obviously flawed.

     

    Please stop attacking people and instead address the arguments they are making.  This isn't a debating chamber, it's an engineering forum.

     

    You don't have the easy programming interface to Ethernet you claim as its main

    advantage without the upper level protocols. That is after all exactly what they are for and why everybody uses them.

     

    That was not the claim.  I claimed that Ethernet was less complex than USB, which it is, as your own response proved, since you very nicely bullet-pointed all the things that USB has to do which the simple frame transfer mechansim of Ethernet does not have to do.

     

    The fact that almost nobody uses Ethernet alone does not say anything about the complexity of Ethernet alone.  If you want to discourse on the complexity of Ethernet then talk about Ethernet, don't talk about IP and TCP and HTTP and SOAP and Websocket and all the cloud protocols and still more that rides on top of Ethernet.  They are all completely irrelevant to the matter of whether Ethernet is complex or not.

     

    This is why engineers separate communications systems into layers, so that they can talk about one layer at a time sensibly.  Please do so, if you're an engineer.  And if you're not an engineer, that's fine too, but then sit back attentively and you'll see how engineers analyse things one piece at a time so that they can be understood easily.

     

    And the piece we're talking about at the moment is Ethernet.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    Morgaine Dinova wrote:

     

    USB has so much more built in that it is hugely more complex than Ethernet, which is just a very low level unverified [it is verified, but not corrected] frame transfer mechanism...

     

    Yes, sorry, I was less than fully precise there.  When I said unverified I had delivery verification in mind, since the sender doesn't know if the recipient receives a given Ethernet frame or not as ACKs are not part of the protocol.  Ethernet really is very basic, intentionally.  Each frame does however carry a 32-bit CRC (frame check sequence), so if the packet does actually arrive then its data integrity can be determined, which is the meaning you attached to my word "verified".  So it's a bit of both, integrity is verified but delivery is not.

     

    So it seems to me that if you're going to make a fair comparison, you really need to do it layer by layer.

     

    Yes indeed, that makes a lot of sense.

     

    At the physical level, they're pretty similar complexity.  However, with Ethernet 100baseT you do have the complexity of MLT-3, and 1000baseT is loads of fun using all four pairs.  In contrast, I believe USB-3.0 just uses 8B10B coding.  You do have scrambling with both.  USB doesn't have to drive as far, so you can use lower-power drivers.  USB also gives you power for free, while PoE is an extra-cost option.  Ethernet Auto-MDIX is fun, something you don't need with USB since it's half duplex.

     

    Pretty much balanced there, one physical layer has a few extra features in one area and the other has a few extra features in another area, none of which impose a major burden of complexity on their respective layer.

     

    The link layers are similar, with best effort data transfers.  However, USB does give you single-packet loss detection, so you don't need the higher-level protocol to handle it.  USB hubs are very simple devices, since the flow is always between host and device and you don't need to store much.  An Ethernet hub is likewise very simple, but nobody uses those nowadays.  Instead, you have Ethernet switches, which implement bridge functionality in hardware.  Bridge functionality is nasty, since the bridge has to learn the MAC addresses of frames coming in each port so it doesn't have to broadcast, and there's a limited amount of frame buffering in the switch, and you need to implement flow control, and you need to auto-negotiate to determine whether to implement flow control, and which speed to use, and whether you can do full duplex.

     

    And then you have Spanning Tree Protocol.  That's a fun algorithm.  There's a quote that reading the STP standard is a good cure for insomnia, and thinking about it can be an effective contraceptive as well.  If STP is too simple for you, how about Rapid STP?  Since USB is physically limited to tree interconnect, there's no STP.  Yes, if you're making an end device you don't need to worry about STP, but it's fair to compare USB tree enumeration with Ethernet STP as far as complexity is concerned.

     

    Although switches "live" at the link level, they're totally transparent in their operation and don't impact at all on the complexity of implementation nor the complexity of operation of the link layer's interface endpoints.  Two Ethernet interfaces talking to each other behave identically whether or not they are connected via a switch.  It's not like USB where you add a hub and suddenly the upstream endpoint gains a whole new level of operational complexity.

     

    So while I certainly don't dispute that switches are complex beasts to create, their link layer complexity is in a side lane of its own, not impacting on the complexity of the link layer between a pair of interfaces.  As for spanning tree ... there's room for a great book of the Soul of a New Machine type to be written around that subject.  It would be a mixture of success and calamity and insight and a serious rival to lay books on quantum mechanics. :-)

     

    We're still at the link layer and haven't started sending any networking packets yet.

     

    I've done a lot of work with Ethernet hardware and software, and there's a lot of complexity there.  I haven't done actual implementation of USB, but I've read a lot of the USB 2.0 standard and IMO the USB physical and link layers are simpler.  Ethernet is a lot more versatile since it's peer-to-peer and can drive 100m, and higher performance since it's full duplex, supports multiple simultaneous data streams, and isn't polled.  But that comes with higher-cost components, more board area, and higher power budget.

     

    Like many tools in an engineer's bag of tricks, each has its advantages, disadvantages, and uses.

    JMO/YMMV

     

    Sure, I agree there.  But the redux is that USB does a whole lot more, and that extra functionality not only gives USB extra operational complexity but those features also have to be implemented so there's more complexity in silicon as well.  To make a rather ugly analogy, Ethernet is like a RISC interconnect whereas USB is like a CISC one.  Like RISC, Ethernet is a pretty KISS approach almost entirely devoid of nice features, which have to be implemented at a higher level ("in the compiler", in this analogy) if your application needs them.

     

    But note that not all applications need those extra features, and when they don't then the barebones nature of Ethernet comes in very handy.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to morgaine

    It's worth pointing out here that this thread is about how to (quoting) "connect RPI with external embedded boards".  What prompted me to suggest Ethernet as a third option for Bhaumik Shah was that many simple sensors provide data that is naturally isochronous, and they often don't benefit from upper layer protocols at all.

     

    If you're measuring a fluctuating voltage or pressure or temperature then it usually matters little if one data point doesn't arrive because the next one will supercede it.  Retransmitting a datum because it didn't arrive the first time is often not only pointless but of negative value, because it's likely to arrive too late, and if the relevant time slot has passed then after processing it you'd have to discard it.  That would just consume resources for nil benefit.

     

    It's common to encounter this requirement in live media transport, but it's equally applicable to many low-level engineering communications.  Barebones Ethernet is a good match for this kind of application.

     

    PS. Additional benefit:  galvanic isolation, since Ethernet is magnetically coupled at both ends of a link.  This can be crucially important for some types of sensor network, especially if extending across more than one building.  Even if isolation is not a design requirement, it's standard in the Ethernet specification and hence your more expensive machines will be less at risk from problems occurring at remote sensors than they might otherwise be..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago in reply to morgaine

    Morgaine,

     

    I didn't attack you, I attacted your argument because it was and still is obviously flawed. I'll remind you about you attitude on

    attacking people/name calling the next time you use your favorite, Raspberry Pi fanbois.

     

    The complexity of Ethernet vs USB at the media or link level has little if anything to do with actually using them in the real

    world because it is hiden behind the hardware drivers and those protocol layers you speak of. Once again, that is exacty

    why the protocol layers exist. I have done a fair amount of Ethernet sockets programming using the TCP/IP and UDP/IP

    and have built my own Linux based Ethernet router so I am very familiar with how easy it is to use as well as the concept

    of protocol layers thank you. Communicating with any layer other that the one specifically provided for applications with

    either interface will require a complicated kernel level interface that will have to be written, tested, and debugged (in kernel

    space, lots o'fun) before it can be used.  As I previously said, and you clearly ignored, you do not have to implement any

    of the "complex" functions of the USB interface that you don't need when you talk to it at the same raw level as the

    Ethernet interface so you gain nothing there either. So why would anybody want to do all that low level programming to

    implement a raw Ethernet or USB interface when easy to use protocol stacks and application interfaces already exits

    for both interfaces ?

     

    While simple sensors may not themselves benefit from upper level protocols, as far as I know all of them that have an

    Ethernet interface support at least a limited TCP/IP, UDP/IP or even HTTP interface protocol. The ones that use USB

    interfaces can use application layer programming interfaces already available for Linux taking full advantage of all

    or none of the USB complexity they do or do not need. Not to mention that it is a lot easier to find programmers for

    application level interfaces than it is for intermediate protocol or raw level interfaces.

     

    And that is where your Ethernet vs. USB complexity sideshow comes crashing down. Welcome to the modern era of

    sensor interfaces and "easy programming". Just what the sensor vendors ordered.

     

    As to media layer electrical isolation, you can easily find USB equipment to do this too if you need it (Google it).

     

    P.S. Still waiting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to gdstew

    On the issue of Ethernet complexity, I can't help you further since you refuse to use the engineering concept of dividing a communications stack into layers so that properties of single layers can be discused separately.

     

    On sensor networks, you miss the point despite it having been outlined clearly.  Just because a facility like TCP or HTTP already exists doesn't mean that it's always good to use it.  Horses for courses.  As I pointed out already, a protocol that uses a retransmission mechanism is not only of no benefit in the transmission of isochronous data but can actually add a negative contribution.

     

    And finally, even a non-ACKed upper protocol like UDP adds overhead of around one order of magnitude compared to MAC-level communications, which means your isochronous sampling is limited to being an order of magnitude slower.  That may or may not be adequate, again it's horses for courses.  An engineer doesn't use just a single tool, but employs a large toolkit of solutions and chooses them appropriately to the problem in hand.

     

    You seem to want an all-in-one debate instead of an engineering analysis of pros and cons.  Not interested.