Code Exchange
  • Technologies
  • More
Code Exchange
Forum How are flocks connecting there RPI with external world(Other embedded circuits)? any standards.. if not which 1 you will pick?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 28 replies
  • Subscribers 55 subscribers
  • Views 3622 views
  • Users 0 members are here
  • 32bit
  • raspbpi
  • raspcontrol
  • Code Exchange
  • programming
  • embedded
  • raspberry_pi_rev_2
  • arm
  • arduino
  • atmel
Related

How are flocks connecting there RPI with external world(Other embedded circuits)? any standards.. if not which 1 you will pick?

shahbhaumik
shahbhaumik over 13 years ago

There are various option when it comes to connect RPI with external embedded boards. Currently many geeks are trying to interface various peripherals with RPI with the I/O header given. I feel there are following option one can go with.

 

1) Use I/O header.

Which i feel is good for prototyping but as we move do something that looks good this option is not what I feel is best, I hate all the wires that comes out of RPI and then loose connection and what not to take care of...

 

2) Use of USB port.

RPI is computer and you it can communicate to co-processor using its USB ports.I think this is very neat way to do things. For example if you are making a robot which has a microcontroller that has UART it can easily communicate with RPI above that you can reflash you microcontroller as per your application using RPI. I know there are no instruction or related work out there like this but soon i will be posting instruction to do this on my blog as well on code exchange.

 

 

Would like to now community views on same.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago +1
    Thus far I've been using the Adafruit Pi Cobbler Adafruit Pi Cobbler to interface the header with a breadboard and programming in Python using libraries like RPi.GPIO . I've really enjoyed Adafruit's tutorials…
  • morgaine
    morgaine over 13 years ago in reply to fustini +1
    Since you've already dealt with 1) Use I/O header , and 2) Use of USB port , I think I'll add the missing alternative, 3) Use of Ethernet . Some people consider USB a fixture and a sacred cow, but I've…
  • morgaine
    morgaine over 13 years ago in reply to gdstew +1
    On the issue of Ethernet complexity, I can't help you further since you refuse to use the engineering concept of dividing a communications stack into layers so that properties of single layers can be discused…
Parents
  • fustini
    0 fustini over 13 years ago

    Thus far I've been using the Adafruit Pi CobblerAdafruit Pi Cobbler to interface the header with a breadboard and programming in Python using libraries like RPi.GPIO.  I've really enjoyed Adafruit's tutorials: http://learn.adafruit.com/category/raspberry-pi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to fustini

    Since you've already dealt with 1) Use I/O header, and 2) Use of USB port, I think I'll add the missing alternative, 3) Use of Ethernet.

     

    Some people consider USB a fixture and a sacred cow, but I've been of the opinion that it's a bit of a poor man's alternative to Ethernet ever since USB was released.  Maybe USB had a point in the very early days when Ethernet was still a bit bulky and costly, but that doesn't apply today.  Everything that USB does in 2012 could be done far more effectively and flexibly with Ethernet, and with IPv6 even more so because autoconfiguration makes IPv6 as plug'n'play as USB.

     

    What's more, with IP addresses being extremely plentiful under IPv6, you can easliy conceive of hundreds or millions of sensors connected by IP, and of course this is exactly what the Internet of Things is already engaged in doing.  And if your interest is in local communications only, and you have no interest in higher-level protocols or the Internet in your application, then raw Ethernet provides an extremely fast and efficient way of transferring data within a local set of boards or machines.

     

    All of which is a preamble to my recommendation:  "Think big, think ahead".  Why not make every sensor, actuator, slave and controller in your system networked, linked together by cheap Etherent switches, and even powered from Ethernet using PoE to eliminate power supplies?  All the bits you need are available, so it's more a case of thinking differently than doing research.

     

    Of course you'll still need the GPIO headers to connect the Pi to low level devices, but when it comes to connecting together such boards into a system, I really think Ethernet (and IPv6) is the way to go.  The very low cost of the Pi helps a lot of course.

     

    Once networked, you'll find your system's abilities expanding rapidly, because the net is a very synergistic place where everything piggybacks on everything else and new emergent phenomena appear every day.  I think you'd benefit from that.

     

    So would everybody else, but few people seem to realize it. image

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    ... and of course this is exactly what the Internet of Things is already engaged in doing...

    Personally, I think the "Internet of Things" (IoT) should be called the "Internet of Digital Things" (IoDiT).  I think the latter acronym -- with a small permutation -- captures the concept very nicely.

     

    I do like Ethernet, but it's costly, complex, and IMO overkill for applications that USB does well.  I rather like USB at the physical and packet layers.  I have yet to delve into USB software, which so far looks like Software Engineering with Cats.  Toot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I do like Ethernet, but it's costly, complex, and IMO overkill for applications that USB does well.

     

    It used to be costly, but it is no more.  As long as your project isn't literally counting pennies (and some really are, so fair enough there), the cost differences are minimal, and easily pay for themselves in extra functionality.

     

    I'm not an expert in USB so I can't compare its complexity properly with that of Ethernet, but Ethernet is extremely simple, and what little I do I know of USB suggests that it is extremely complex despite being so limited.  I think it had a role in its day, but frankly I don't understand why we're still using it when Ethernet is so much better.

     

    And finally, overkill ... well that's like saying that USB is overkill when we could be using the simpler RS232.  I don't think the "overkill" concept really means much in this context, but if we have to use the term then I'd say that USB is overkill when Ethernet does the job. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago in reply to morgaine

    Moraine said: and what little I do I know of USB suggests that it is extremely complex despite being so limited

     

    Yea you really should read up on the subject, otherwise your "logic" may be flawed.

     

    1) With USB you can guaranty the amount of bandwidth needed will be avaialable (within the amount available of course) which you can not do with Ethernet.

    2) With USB you can guaranty latency (at least to the millisecond, although this also depends on the processor of course) which you can not do with Ethernet.

    3) Most of the "complexity" is in the driver where it belongs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to gdstew

    Actually, Ethernet and IP has mechanisms for marking your hi-pri traffic.

    Latency can easily be sub-millisecond on same-network.

    However, often it is possible to design (depends on the use-case) so that you don't

    need high bandwidth or low latency.

    Personally I'm a fan of RS232-like asynch protocols and Ethernet.

    USB has its uses too of course.

    IoT will see a lot more IP being used, with varying physical layers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago in reply to shabaz

    shabaz,

     

    Yes but it can not and does not guaranty it. One problem with the USB latency/bandwidth guaranties is that on a

    given host to device interface you can only guaranty one or the other, not both at the same time.

     

    You can also use a USB interface exactly like you would with a RS-232RS-232 interface. I have a device I designed with

    a microprocessor that only has a async serial port. The serial port is connected to an FTDI-232BM serial to USB

    converter. It plugs into the host USB interface but the programming interface is just like any normal serial port. I

    did this for several reasons. The microprocessor I was using did not have a USB interface. The USB interface

    provides the power for the device, and by adding a RS232 level converter (on a header provided for this), it can

    be used with a normal serial port too, although it then needs and external power supply. The sofware to use the

    device is the same for both interfaces, only the /dev name is different depending on which one is being used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • morgaine
    0 morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    Yea you really should read up on the subject, otherwise your "logic" may be flawed.

     

    1) With USB you can guaranty the amount of bandwidth needed will be avaialable (within the amount available of course) which you can not do with Ethernet.

    2) With USB you can guaranty latency (at least to the millisecond, although this also depends on the processor of course) which you can not do with Ethernet.

    3) Most of the "complexity" is in the driver where it belongs.

     

    Your points confirm what my limited knowledge of USB had suggested exactly.  USB has so much more built in that it is hugely more complex than Ethernet, which is just a very low level unverified frame transfer mechanism.

     

    So neither was my logic flawed nor were the observations that my minimal acquaintance had suggested flawed, you've proved that they were spot on.  In contrast, your conclusion about their comparative complexity is clearly incorrect by your own observations.

     

    Higher levels of protocol that ride on top of Ethernet are not Ethernet, and do not contribute to the complexity of Ethernet.  For what it's worth though, the complexity of upper layers is all in the kernel where it belongs and transparent to users and applications.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 13 years ago in reply to morgaine

    No Morgaine you logic is terribly and obviously flawed. You don't have the easy programming interface to Ethernet you claim as its main

    advantage without the upper level protocols. That is after all exactly what they are for and why everybody uses them. Otherwise you will

    have to talk directly to the Ethernet driver at some slightly higher level of abstraction to remove hardware dependencies. This means that

    at least part of the "user" interface you will have to write will run in kernel space probably as a loadable module and have to send data

    back and forth between user and kernel space. Yea this is getting easier all the time (/sarcasm).

     

    With USB, all the complexity you fear is in the host kernel driver as it should be. You only have to deal with the "easy" API which is

    again, why such things exits. If you don't need all the complexity (guaranteed latency or bandwidth) or have a CPU that has trouble

    handling it, you can use a much less complicated host kernel driver for it and still have the "easy" upper level API to deal with. This

    is what USB OTG does. There are different, much, much less complex requirements for the device side driver. If you don't understand

    what that means read up on USB. I don't have a hundred pages to explain it to you. So logically speaking of course, you do requre

    knowledge of USB to make "logical" arguments, DUH.

     

    P.S. Still waiting on the "logical" scientifically based engineering explanation of your data 100% reliability (your exact  somewhat stilted

           phrasing) requirement for the Raspberry Pi, or in your belief in its current availability on any other computer on Earth for that matter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 13 years ago in reply to morgaine

    No Morgaine you logic is terribly and obviously flawed. You don't have the easy programming interface to Ethernet you claim as its main

    advantage without the upper level protocols. That is after all exactly what they are for and why everybody uses them. Otherwise you will

    have to talk directly to the Ethernet driver at some slightly higher level of abstraction to remove hardware dependencies. This means that

    at least part of the "user" interface you will have to write will run in kernel space probably as a loadable module and have to send data

    back and forth between user and kernel space. Yea this is getting easier all the time (/sarcasm).

     

    With USB, all the complexity you fear is in the host kernel driver as it should be. You only have to deal with the "easy" API which is

    again, why such things exits. If you don't need all the complexity (guaranteed latency or bandwidth) or have a CPU that has trouble

    handling it, you can use a much less complicated host kernel driver for it and still have the "easy" upper level API to deal with. This

    is what USB OTG does. There are different, much, much less complex requirements for the device side driver. If you don't understand

    what that means read up on USB. I don't have a hundred pages to explain it to you. So logically speaking of course, you do requre

    knowledge of USB to make "logical" arguments, DUH.

     

    P.S. Still waiting on the "logical" scientifically based engineering explanation of your data 100% reliability (your exact  somewhat stilted

           phrasing) requirement for the Raspberry Pi, or in your belief in its current availability on any other computer on Earth for that matter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • morgaine
    0 morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    No Morgaine you logic is terribly and obviously flawed.

     

    Please stop attacking people and instead address the arguments they are making.  This isn't a debating chamber, it's an engineering forum.

     

    You don't have the easy programming interface to Ethernet you claim as its main

    advantage without the upper level protocols. That is after all exactly what they are for and why everybody uses them.

     

    That was not the claim.  I claimed that Ethernet was less complex than USB, which it is, as your own response proved, since you very nicely bullet-pointed all the things that USB has to do which the simple frame transfer mechansim of Ethernet does not have to do.

     

    The fact that almost nobody uses Ethernet alone does not say anything about the complexity of Ethernet alone.  If you want to discourse on the complexity of Ethernet then talk about Ethernet, don't talk about IP and TCP and HTTP and SOAP and Websocket and all the cloud protocols and still more that rides on top of Ethernet.  They are all completely irrelevant to the matter of whether Ethernet is complex or not.

     

    This is why engineers separate communications systems into layers, so that they can talk about one layer at a time sensibly.  Please do so, if you're an engineer.  And if you're not an engineer, that's fine too, but then sit back attentively and you'll see how engineers analyse things one piece at a time so that they can be understood easily.

     

    And the piece we're talking about at the moment is Ethernet.

     

    Morgaine.