Code Exchange
  • Technologies
  • More
Code Exchange
Forum Interfacing of SHT11 with PIC24f16KA102
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Code Exchange to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 2 answers
  • Subscribers 50 subscribers
  • Views 3311 views
  • Users 0 members are here
Related

Interfacing of SHT11 with PIC24f16KA102

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I have written the c code for I2C for interfacing the SHT11(temp sensor) and PIC24F16KA102. but i m not getting the acknowledge from the SHT11 when i m writing through pic.  i m pasting my code here. plz let me know where i m doing wrong if possible. thanks

 

#include <stdint.h>

#include <xc.h>

#include "main.h"

 

#include <p24Fxxxx.h>

// ICD Pin Placement Select (EMUC/EMUD share PGC3/PGD3)

//_FICD(ICS_PGx1)

/*

* File:   main.c

* Author: jalpa

*

* Created on 7 February, 2014, 10:11 AM

*/

/*******************************************************************************************************************/

//Include section

 

/*******************************************************************************************************************/

#include "p24F16KA102.h"

 

#include "spi.h"

#include "i2c.h"

#include <timer.h>

 

 

 

/*******************************************************************************************************************/

//Define section

/*******************************************************************************************************************/

// for input use  PORTBbits.RB7  notation and for output pin use LATBbits.LATB2.

//#define CE LATBbits.LATB2    //pin-6  // CE output pin, PORTB bit 2

 

 

//#define SDA_pin LATBbits.LATB9    //pin-22// Clock output pin, PORTB bit 11

//#define SCL_pin LATBbits.LATB8

//

//#define SDA_dir TRISBbits.TRISB9

//#define SCL_dir TRISBbits.TRISB8

 

/*******************************************************************************************************************/

 

//Declaration of variable

/*******************************************************************************************************************/

unsigned char msb;

unsigned char lsb;

unsigned char status;

 

/*******************************************************************************************************************/

//Declaration of functions

 

/*******************************************************************************************************************/

void i2c_init();

void reset_i2c_bus();

void delay_us(unsigned short us);

void i2c_start();

void i2c_restart();

char i2c_send_byte(int data);

char i2c_read_byte();

 

 

//#define SCK_dir TRISBbits.TRISB8

 

 

 

/*******************************************************************************************************************/

//Main function

/*******************************************************************************************************************/

 

void main(void)

{

 

 

 

   // AD1PCFGbits.PCFG0=1;

   // AD1PCFGbits.PCFG1=1;

 

   AD1PCFG =0XFF;

   //SCK_dir=0;

  

   i2c_init();

   i2c_start();

   delay_us(2000);

   status = i2c_send_byte(0x03);

   delay_us(10000);

   msb= i2c_read_byte();

   lsb= i2c_read_byte();

   reset_i2c_bus();

 

 

 

   

 

}

 

 

 

 

 

void i2c_init()

{

    int temp;

    I2C1BRG = 157;

    I2C1CONbits.I2CEN = 0;

    I2C1CONbits.DISSLW = 1;

    I2C1CONbits.I2CEN= 1;

    temp = I2C1RCV;

    reset_i2c_bus();

 

}

 

void reset_i2c_bus()  // reset is used before and after a packet i sent through the bus (release both sda and scl)

{

 

    int x=0;

 

    I2C1CONbits.PEN= 1;

 

    while(I2C1CONbits.PEN)

    {

 

        delay_us(1);

        x++;

        if(x>20) break;

 

    }

 

    I2C1CONbits.RCEN=0;

    IFS1bits.MI2C1IF=0;

    I2C1STATbits.IWCOL=0;

    I2C1STATbits.BCL=0;

 

    delay_us(10);

   

}

 

void i2c_start(void)

{

   int x = 0;

   I2C1CONbits.ACKDT = 0;    //Reset any previous Ack

   delay_us(10);

   I2C1CONbits.SEN = 1;    //Initiate Start condition

   Nop();

 

   //the hardware will automatically clear Start Bit

   //wait for automatic clear before proceding

   while (I2C1CONbits.SEN)

   {

      delay_us(1);

      x++;

      if (x > 20)

      break;

   }

    delay_us(2);

}

 

 

void i2c_restart(void)

{

   int x = 0;

 

   I2C1CONbits.RSEN = 1;    //Initiate restart condition

   Nop();

 

   //the hardware will automatically clear restart bit

   //wait for automatic clear before proceding

   while (I2C1CONbits.RSEN)

   {

      delay_us(1);

      x++;

      if (x > 20)    break;

   }

 

   delay_us(2);

}

 

 

char i2c_send_byte(int data)

{

   int i;

 

   while (I2C1STATbits.TBF) { }

   IFS1bits.MI2C1IF = 0; // Clear Interrupt

   I2C1TRN = data; // load the outgoing data byte

 

   // wait for transmission

   for (i=0; i<500; i++)

   {

      if (!I2C1STATbits.TRSTAT) break;

      delay_us(1);

 

      }

      if (i == 500) {

      return(1);

   }

 

   // Check for NO_ACK from slave, abort if not found

   if (I2C1STATbits.ACKSTAT == 1)

   {

      reset_i2c_bus();   //error

      return(1);

   }

 

   delay_us(2);

   return(0);

}

 

char i2c_read_byte(void)    //does not reset bus!!!

{

   int i = 0;

   char data = 0;

 

   //set I2C module to receive

   I2C1CONbits.RCEN = 1;

 

   //if no response, break

   while (!I2C1STATbits.RBF)

   {

      i++;

      if (i > 2000) break;

   }

 

   //get data from I2CRCV register

   data = I2C1RCV;

 

   //set ACK to high

   I2C1CONbits.ACKEN = 1;

 

   //wait before exiting

   delay_us(10);

 

   //return data

   return data;

}

 

 

 

void delay_us(unsigned short us)

{

  unsigned short i;

 

  // TIMER1 Period = PR1 x 2 x Tosc x Prescale second

  // TIMER1 Period = 145 x 2 x 1/32000000 x 1 = 9 us // practically coming 12us

 

  PR1=145;                      // Maximum Counter

  T1CON=0x0000;            // TIMER1 Off, Prescale 1:1 using the internal clock

  for (i=0; i < us;i++) {

    TMR1=0;                     // Reset TIMER1 Counter

    IFS0bits.T1IF=0;            // Clear TIMER1 Interrupt Flag

    T1CONbits.TON=1;            // Turn On TIMER1

    while(IFS0bits.T1IF != 1);  // Wait until TMR1 > PR1 (Overflow)

    T1CONbits.TON=0;            // Turn Off TIMER1

  }

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to gihu +1
    Hi, thanks Actually i checked the the clock configuration earlier through as u said by LED blinking Code. and for FRCPLL and keeping CLKDIV=0x0000; i m getting Fcy=16MHz. I have checked it by putting different…
Parents
  • gihu
    0 gihu over 12 years ago

    Hi jalpa,

     

    I suppose that you are using MPLAB IDE plus XC16 complier, rigth?

    In your code you:

    #include "i2c.h",

     

    but you never use it, you are using own function declared and coded in your main.c, right?

    If you have chosen the PIC when create the project, you do not need to:

    #include <p24Fxxxx.h>

    After includes and defines, configuration bits are missing, (the configuration bits MPLAB utility is very usefull!!).

     

    I recommend you using the functions in i2c.h, like OpenI2C1(), CloseI2C1(), MasterWriteI2C1(), StartI2C1(), StopI2C1(), etc... the function to use will depend on the configuration of the bus when OpenI2C.

     

    I hope that helps,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to gihu

    thanks for your reply. For configuration i have kept file so thats why is not included in this code. I will try the functions suggested by you, which are in built.  can u tell me what is the difference between hardware spi and software spi?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 12 years ago in reply to e14 Contributor

    Normally, you use I2C by soft when you do not have a dedicated hardware for I2C, mainly when you use software to emulate such a dedicated hardware, the CPU has to deal with all the delay, timings, pooling, checking flags, whereas if you use dedicated hardware (with interruptions), CPU has just to configure the hardware just once, and let the hardware deals with most of this work, making lighter the workload of the CPU.

     

    I see you try to use a the dedicated registers and flags, so better use the functions given by XC.

     

    If you configure the hardware, and when write, you don't receive the slave ACK, check you have configured correctly the address mode and the SCL speed of the I2C, maybe the sensor is not receiving correctly what it is expecting.

     

    Hope that helps,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gihu
    0 gihu over 12 years ago in reply to e14 Contributor

    Normally, you use I2C by soft when you do not have a dedicated hardware for I2C, mainly when you use software to emulate such a dedicated hardware, the CPU has to deal with all the delay, timings, pooling, checking flags, whereas if you use dedicated hardware (with interruptions), CPU has just to configure the hardware just once, and let the hardware deals with most of this work, making lighter the workload of the CPU.

     

    I see you try to use a the dedicated registers and flags, so better use the functions given by XC.

     

    If you configure the hardware, and when write, you don't receive the slave ACK, check you have configured correctly the address mode and the SCL speed of the I2C, maybe the sensor is not receiving correctly what it is expecting.

     

    Hope that helps,

    Miguel