Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum Identifying a Connector or at least Manufacturer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 127 subscribers
  • Views 1866 views
  • Users 0 members are here
  • connector
  • nes
  • nintendo
  • unknown
Related

Identifying a Connector or at least Manufacturer

e14 Contributor
e14 Contributor over 10 years ago

I am looking to build a board that will be installed in an original NES. With the right connectors I will be able to build this such that no changes are needed to the console in order to add a small feature, but I need to find the existing connectors in order to source compatible new ones. Luckily, one of the connectors I want to use was identifiable(after a lot of searching/learning) as one of the JST variations: all the measurements match the datasheets nicely, and so do the visuals.

 

The other connector is more of a problem: P6. It is used to connect to the power/reset/LED board mounted to the front of the case, and I cannot figure out who even makes it. Pictures of the connector and logo are below.

 

I've tried asking this in the NES hardware forums online, but no luck yet.

 

I'm also open to more suggestions on where to look.

 

Info I have:

- 5 pins - keyed with pin 1 at 1.5 times other pitch

- pitch from pin 1 to pin 2 = 7.5mm

- pitch for all other pins = 5 mm

- connector is between 6 mm and 6.5 mm high

- connector is between 27.3 mm and 27.7 mm wide

- connector is about 4.2 mm deep

- pins are about 1.1 mm square

- blue( a lighter blue, but as with anything like this, it varies a bit between batches and with age )

(measurements are approximate, my digital calipers are a bit cheap, sometimes randomly adding exactly 1/5th of an inch to measurements - these are double and sanity checked)

 

There is no manufacturer name on either part, just a single letter('P') and a circular symbol that kinda looks like a 6 sided star, divided into 6 segments in a ring. This symbol is also found on one of my NES systems on the power and reset switches, still no company name. Other NES have Mitsumi switches, but they don't seem to be the same company. This would have been manufactured in the millions in the 80's, so there must be a datasheet somewhere.

 

Let me know if any other information will help.

 

Image of the logo: https://goo.gl/photos/Gc2213oZm1ZmzDyz6

Image of connector: https://goo.gl/photos/kNJjqzAKBSNs338Y7

Left is pin 1.

 

Thanks for any help or direction.

G42

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +1
    Looks like a job for a 3D printer...
Parents
  • dougw
    0 dougw over 10 years ago

    Looks like a job for a 3D printer...

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to dougw

    Now that's something for me to acquire. I do wonder if I could find one that can do the shape well though. Some of the walls involved at 0.75mm, I might see if I can find out if there are printers that could do that. I'm still hoping to identify a compatible pre-existing one(Molex has something close) and save me a lot of work for a toy project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to dougw

    Now that's something for me to acquire. I do wonder if I could find one that can do the shape well though. Some of the walls involved at 0.75mm, I might see if I can find out if there are printers that could do that. I'm still hoping to identify a compatible pre-existing one(Molex has something close) and save me a lot of work for a toy project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 10 years ago in reply to e14 Contributor

    To get the odd spacing you can pull one pin out of the Molex and drill a new hole for it - make sure the hole is very tight fit.