Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum from usb to wireless
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 128 subscribers
  • Views 882 views
  • Users 0 members are here
  • usb
  • wireless
Related

from usb to wireless

e14 Contributor
e14 Contributor over 16 years ago
Hello,

 

I have a data logger connected to a PC via USB. I would like to turn this connection into a wireless one: I mean to connect the USB port of the data logger to a wireless transmitter, whose receptor will be connected to the PC via USB, bearing in mind that I will have approximately 100 meters between the transmitter and the receptor and that the rate of exchanged data is very low.

How could I success in doing that at a very low  cost and easily?

 

Best,

 

E. Vial

  • Sign in to reply
  • Cancel
  • suresh
    0 suresh over 16 years ago

    Bluetooth is used most of the forms of communication like data logger. Bluetooth data logger takes data from an ADC via MCU and then Bluetooth link to PC for collecting the data. Bluetooth is not sufficient for your application and to achieve 100 mtr distance definitely you need to go with wi-fi or zigbee.

    we have solution for your application which can achieve indoor -100mtr distance with Zigbee, please follow the link below.

    The solution by MaxStream with ZigBeeTm/802.15.4 OEM RF Modules.

    http://www.newark.com/maxstream/xb24-dks/development-kit-with-modules/dp/42M0971

     

     

    Attachments:
    imageZigbee module.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago

    Hello

     

    With LM Technologies Ltd Bluetooth you have two solutions:

    1: if your datalogger has an RS232 port you can use our LM048 Bluetooth Adapter http://www.lm-technologies.com/business/bluetooth-adapters/LM048/rs232-cable-replacement on the datalogger and a USB adapter on the PC http://www.lm-technologies.com/business/bluetooth-adapters/LM540/bluetooth-usb-adapter-class-1

     

    2: if your datalogger has a USB port then LM060 convertor http://www.lm-technologies.com/business/accessories/LM060/rs232-to-usb-adapter and then LM048 http://www.lm-technologies.com/business/bluetooth-adapters/LM048/rs232-cable-replacement

     

    With USB adapters you need to load the drivers from a download or CD. Our LM048 Adapters can be configured on a PC and then connected to your datalogger. Where your datalogger has USB port only using the LM060 convertor allows the Bluetooth connection without any modification to your datalogger application.

     

    Our Bluetooth Adapters have a range of up to 100m. If you need more than 100m you can change the antenna  http://www.lm-technologies.com/business/antennaon on our LM058 http://www.lm-technologies.com/business/bluetooth-adapters/LM058/rs232-cable-replacement---external-antenna and LM540 http://www.lm-technologies.com/business/bluetooth-adapters/LM540/bluetooth-usb-adapter-class-1

     

    kind regards

     

    Hazel Doughty

    LM Technologies Ltd

    hazel@lm-technologies.com