Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum PWM high current signals with low currents signals in the same cable
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 128 subscribers
  • Views 327 views
  • Users 0 members are here
  • connectors
  • connector
  • ethernet
Related

PWM high current signals with low currents signals in the same cable

Catwell
Catwell over 16 years ago
I have 8 PWM controlled motor driver wires conducting up to 3A each, 3 wires from a rotary speed sensor at 5V 100mA, and 2 wires from Active Low switches at 5V. A total of 13 wires. I would like to have them all in the same cable going from a control box to a machine, no longer than 6 feet.

The 1st concern is interference from the motor drive wires on the other five, mA conducting, wires. Would shielding work or twisted pair work to isolate the drive signals? Or should I keep the two groups separate?

My 2nd concern is the actual cable. I would like a cable that is inexpensive and already assembled. Currently, I use a 8 pin CPC connector for the motors and an cat5 connection for the other wires. But, for the motors, I have to solder every pin on the CPC plugs. I'm tired of doing that over and over, and I'm tired of the solder fumes. So with all 13 wires solution, I would need 2 plug receptacles and a cable with matching plugs on either end. It would be nice if wiring the receptacles was easy, or even if they were pre-wired.

Any suggestions would be greatly appreciated.

Cabe
  • Sign in to reply
  • Cancel
  • enrico.migchels
    0 enrico.migchels over 16 years ago

    Hi Cabe,

     

    My suggestion is: Keep the Motor drive power separated from the remaining circuits. Due to the PWM currents you will have a very noisy ground. It is best to have a motor_ground and sensor/switch_ground. If you want to force the current back through a predefined path you could use a common mode choke on the DC-output. The value of such a coil is in the range of 220uH (thick copper wire on HF toriod).

     

    Best regards, Enrico Migchels