Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum 4-pin speaker connector.. how best to hook up to a single speaker
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 127 subscribers
  • Views 3792 views
  • Users 0 members are here
Related

4-pin speaker connector.. how best to hook up to a single speaker

Matt
Matt over 4 years ago

I'm working on a retro project where I'm fitting this 7" LCD screen to a cool-looking film editor built in the 1970s, that looks like it's from the TV show Severance Slight smile

I'd like to hook it up to a single 1" speaker.

There's a 4-pin speaker connector on the screen's main board;

image

image

On the board they're labelled as R1 R2 L1 L2.

Am I correct in assuming that I can take a generic 4-pin lead with 1.25mm spacing like this, and simply combine wires R1+L1, and R2+L2, and wire those direct into the mono 1" speaker?

Thanks in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • Matt
    Matt over 4 years ago in reply to shabaz +4
    Thanks Shabaz! The old film editor is very basic, so just full of mirrors & cogs.. no electronics apart from a small bulb Good call about the laptop speakers! I'll have a look at one where I've already…
  • shabaz
    shabaz over 4 years ago +2 verified
    Hi Matt, Nice project! It looks like your LCD board is using the audio chip shown below. I can't tell which specific 4-pin lead will fit, but even if you get it wrong, you could just tack wires to…
  • Matt
    Matt over 4 years ago +1
    If you're interested, this is the film editor I'm retrofitting the screen into;
Parents
  • shabaz
    +1 shabaz over 4 years ago

    Hi Matt,

    Nice project!

    It looks like your LCD board is using the audio chip shown below. I can't tell which specific 4-pin lead will fit, but even if you get it wrong, you could just tack wires to the pins although admittedly that's awkward when they are small.

    Anyway, if you have just a single mono speaker, then you can wire it to either pins 1 and 2, or pins 3 and 4, but it's not good to parallel them. There's no harm if one pair of wires is left disconnected, and nothing will sound weird if the input is mono, or if there is not much difference in the stereo signals. The other option of course is to wire two speakers, but that depends if you have two, and if you have the space for them. By the way, from AliExpress it is possible to get speaker modules (presumably from old laptops or LCD TVs) that consist of the speaker already in a plastic enclosure, that can provide more bass than a single speaker. If it is possible to remove the old speaker and retrofit a laptop speaker, then it may provide better sound quality than the original : ) Some are sold in pairs with a 4-pin connector, although it's possible the connector will be different. Some of the speakers are compact/slim, so two might fit the space you have.

    image

    image

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • shabaz
    +1 shabaz over 4 years ago

    Hi Matt,

    Nice project!

    It looks like your LCD board is using the audio chip shown below. I can't tell which specific 4-pin lead will fit, but even if you get it wrong, you could just tack wires to the pins although admittedly that's awkward when they are small.

    Anyway, if you have just a single mono speaker, then you can wire it to either pins 1 and 2, or pins 3 and 4, but it's not good to parallel them. There's no harm if one pair of wires is left disconnected, and nothing will sound weird if the input is mono, or if there is not much difference in the stereo signals. The other option of course is to wire two speakers, but that depends if you have two, and if you have the space for them. By the way, from AliExpress it is possible to get speaker modules (presumably from old laptops or LCD TVs) that consist of the speaker already in a plastic enclosure, that can provide more bass than a single speaker. If it is possible to remove the old speaker and retrofit a laptop speaker, then it may provide better sound quality than the original : ) Some are sold in pairs with a 4-pin connector, although it's possible the connector will be different. Some of the speakers are compact/slim, so two might fit the space you have.

    image

    image

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Matt
    0 Matt over 4 years ago in reply to shabaz

    Thanks Shabaz!

    The old film editor is very basic, so just full of mirrors & cogs.. no electronics apart from a small bulb Slight smile

    Good call about the laptop speakers! I'll have a look at one where I've already removed the screen & see if I can salvage speakers from it (assuming they'll fit where I want them).

    I'm putting together a short video series on how I've modded it, so will report back when I've finished that so you can take a proper look at how it went.

    • Cancel
    • Vote Up +4 Vote Down