Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum Seeking Your Interest in Receiving Solderless Compression Mounted RF Connectors to Experiment With
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 126 subscribers
  • Views 5785 views
  • Users 0 members are here
  • sv microwave
  • rf connectors
  • community poll
  • solderless compression mounted connectors
Related

Seeking Your Interest in Receiving Solderless Compression Mounted RF Connectors to Experiment With

rscasny
rscasny over 3 years ago

imageI have been in conversation with one of our suppliers who makes solderless compression-mounted RF connectors. They say these connectors are desirable for their fast and easy installation compared to standard soldered connectors. They are rugged and durable, and can be customized for the PCB footprint. While they aren't the solution for every situation, they are used for applications such as RF test and measurement boards; High Speed Digital component test equipment; and stripline, microstrip and coplanar waveguide PCB launch connectors.

Here's some documentation on these connectors:

www.svmicrowave.com/.../Solderless_Compression_Mount_Study.pdf
www.svmicrowave.com/.../LiteTouch_Solderless_PCB_Connectors_Application_Note.pdf
www.svmicrowave.com/.../Solderless_PCB_Compression_Mount_Connectors_Application_Note.pdf
www.svmicrowave.com/solderless-pcb-edge-launch
https://svmicrowave.com/high-speed-solderless-pcb-connectors

What we would like you to do

We would like to send a few members some of these connectors to experiment with informally and write a blog about their thoughts and testing of them. The blog would be something like this one: click here to view.

Here are some of the types of solderless compression mounted RF connectors we would give you:

image image image image
SF2921-61507 RF / Coaxial Connector, PCB SMD, SMA Coaxial, Straight Flanged Jack, Compression, 50 ohm  SF2921-61507 SF1521-60061 RF COAXIAL, 2.92MM JACK, 50 OHM, PANEL  SF1521-60061 SF3321-60040 RF / Coaxial Connector, 1.85mm Coaxial, Edge Launch Jack, Board Edge / End Launch, 50 ohm   SF3321-60040 SF1521-60013 RF / Coaxial Connector, 2.92mm Connector, Straight Jack, 50 ohm, Beryllium Copper  SF1521-60013

**Participants will receive a giveaway prize that needs to be determined. 

  • Sign in to reply
  • Cancel

Top Replies

  • rsjawale24
    rsjawale24 over 3 years ago +4
    The compression mount type SMAs are quite popular in mmWave microwave circuits. I have specialised in antennas and I have been using the normal edge mount SMAs from Wurth or Molex that work upto 18 GHz…
  • rscasny
    rscasny over 3 years ago +3
    Hi all, I wanted to touch with anyone interested in participating in this little project. Since we haven't really done anything (that I can recall) on solderless compression connectors, I'm interested…
  • shabaz
    shabaz over 3 years ago +2
    Thanks Jan Cumps I didn't see this. I'll write up a mini-proposal and send it across to see if it is of interest. I can think of several applications where it could be very useful.
Parents
  • rsjawale24
    rsjawale24 over 3 years ago

    The compression mount type SMAs are quite popular in mmWave microwave circuits. I have specialised in antennas and I have been using the normal edge mount SMAs from Wurth or Molex that work upto 18 GHz only. Given below are two of my published works on frequency reconfigurable antennas. You can see the soldered SMAs to the antenna feed.

    imageimage

    imageimage

    For higher frequencies like 26-28GHz, the compression mount connectors (2.92 mm/K type) are used. I'm surprised to see the specs of the above conncetors, they work from DC all the way upto 67 GHz! I was familiar with the ones that work till 40 GHz.
    While I can still blog about them, but I have limited resources and cannot test the connectors for more than 20GHz as the VNA I have access to works till 20 GHz only.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsjawale24
    rsjawale24 over 3 years ago

    The compression mount type SMAs are quite popular in mmWave microwave circuits. I have specialised in antennas and I have been using the normal edge mount SMAs from Wurth or Molex that work upto 18 GHz only. Given below are two of my published works on frequency reconfigurable antennas. You can see the soldered SMAs to the antenna feed.

    imageimage

    imageimage

    For higher frequencies like 26-28GHz, the compression mount connectors (2.92 mm/K type) are used. I'm surprised to see the specs of the above conncetors, they work from DC all the way upto 67 GHz! I was familiar with the ones that work till 40 GHz.
    While I can still blog about them, but I have limited resources and cannot test the connectors for more than 20GHz as the VNA I have access to works till 20 GHz only.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • rsjawale24
    rsjawale24 over 3 years ago in reply to rsjawale24

    Had to change my vote at the last minute. Unfortunately, I'm busy with two back to back conferences in December. I'm going to present paper on a similar design as above.. reconfigurable antenna...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 3 years ago in reply to rsjawale24

    That's too bad. But I fully understand. Have a successful conference presentation. 

    Randall

    -element14 Team