Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum Would You Like To Test Out a Magnetic, Rotatable, IP67-rated Connector?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 127 subscribers
  • Views 5848 views
  • Users 0 members are here
  • IP67-rated Connector?
  • Would You Like To Test Out a Magnetic
  • Rotatable
Related

Would You Like To Test Out a Magnetic, Rotatable, IP67-rated Connector?

rscasny
rscasny over 3 years ago

I have been talking with a roadtest sponsor who is interested in having a product roadtested. It's a magnetic connector that can be disconnected quickly or used in an area where accidental damage is likely. These magnetic connectors are rated current of 5A at 30V AC/DC. The unique design also allows the connector to rotate a full 360 degrees without loss of the electrical connection. While the panel mount connector and cable connectors are individually IP67 rated, due to the design of the magnetic connector the connection itself is not waterproof.

Here's some info about the product

image

For More Info

image

Datasheet

Poll Questions



  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago in reply to kmikemoo +3
    Finding a part to "fill a need" is a process that could probably be scientifically studied. The process I go through varies but it is something like: what do I imagine is the ideal part to fill this…
  • Jan Cumps
    Jan Cumps over 3 years ago +2
    This is a great solution for those cases where connectors (or wires) are regularly ripped out of the enclosure. You may not be able to prevent the break, but it doesn't cause physical damage.
  • kmikemoo
    kmikemoo over 3 years ago +2
    I really like that the other end is already in a cable form. I could put this to use now. The ability to quickly disconnect a circuit without destroying something... If it doesn't make it to Roadtest…
Parents
  • kmikemoo
    kmikemoo over 3 years ago

    I really like that the other end is already in a cable form.  I could put this to use now.  The ability to quickly disconnect a circuit without destroying something... 

    If it doesn't make it to Roadtest or Design Challenge, it's on the list of potential projects.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kmikemoo
    kmikemoo over 3 years ago

    I really like that the other end is already in a cable form.  I could put this to use now.  The ability to quickly disconnect a circuit without destroying something... 

    If it doesn't make it to Roadtest or Design Challenge, it's on the list of potential projects.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to kmikemoo

    There seems to be a straight plug and one with 90° angle, according to the data sheet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to Jan Cumps

    Jan Cumps  I saw that. Grinning  Which one to use?  I'd probably start out with the straight one and make the panel connector into an in-line connection.  5A is respectable.  I would probably use the 90 degree on on a battery maintainer connection to a vehicle or trailer brake battery system.  The "rotatable" part is also interesting.  I'll have to ponder this more. Laughing