Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum Would You Like To Test Out a Magnetic, Rotatable, IP67-rated Connector?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 127 subscribers
  • Views 5848 views
  • Users 0 members are here
  • IP67-rated Connector?
  • Would You Like To Test Out a Magnetic
  • Rotatable
Related

Would You Like To Test Out a Magnetic, Rotatable, IP67-rated Connector?

rscasny
rscasny over 3 years ago

I have been talking with a roadtest sponsor who is interested in having a product roadtested. It's a magnetic connector that can be disconnected quickly or used in an area where accidental damage is likely. These magnetic connectors are rated current of 5A at 30V AC/DC. The unique design also allows the connector to rotate a full 360 degrees without loss of the electrical connection. While the panel mount connector and cable connectors are individually IP67 rated, due to the design of the magnetic connector the connection itself is not waterproof.

Here's some info about the product

image

For More Info

image

Datasheet

Poll Questions



  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago in reply to kmikemoo +3
    Finding a part to "fill a need" is a process that could probably be scientifically studied. The process I go through varies but it is something like: what do I imagine is the ideal part to fill this…
  • Jan Cumps
    Jan Cumps over 3 years ago +2
    This is a great solution for those cases where connectors (or wires) are regularly ripped out of the enclosure. You may not be able to prevent the break, but it doesn't cause physical damage.
  • kmikemoo
    kmikemoo over 3 years ago +2
    I really like that the other end is already in a cable form. I could put this to use now. The ability to quickly disconnect a circuit without destroying something... If it doesn't make it to Roadtest…
Parents
  • Fred27
    Fred27 over 3 years ago

    It's an interesting product - and one that could fairly easily be tested without needing anything to go with it.

    I can't immediately think of anything that might require it, but it seems like the sort of product that would suddenly find itself a perfect fit for something. I can imagine myself working on some random project in the future and realising that it would be useful. It's the sort of thing that might sit in your toolbox for ages until one day you go "Aha! I have just the thing for that! Where did I put it?"

    I wonder if it would be worth having a pool of useful components like this that members could request when working on a Project14 entry? Rather than trying for find a way to use it, just wait until it jumps out at you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago in reply to Fred27

    Fred27  "Jumps out at you" is my entire project plan!  I'd like to say that I subscribe to the "See a need. Fill a need." philosophy (Bigweld from the movie Robots) but it's more like just chasing the newest bright shiny thing. LaughingThumbsup  It's my version of ADD - Adult Distractability Disorder.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to kmikemoo

    Finding a part to "fill a need" is a process that could probably be scientifically studied. The process I go through varies but it is  something like:

    • what do I imagine is the ideal part to fill this need?
    • what do I think I have that comes closest to this ideal part? (I often cannot remember everything I have - so)
    • rummage around several possible storage locations to see if I actually have something that I remember or something else that might fit the bill
    • give up and order something
    • suddenly realize I was looking in the wrong place and find something suitable
    • when the now un-needed part comes in, squirrel it away somewhere where I am never going to forget it
    • and then promptly forget all about it
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 3 years ago in reply to kmikemoo

    Finding a part to "fill a need" is a process that could probably be scientifically studied. The process I go through varies but it is  something like:

    • what do I imagine is the ideal part to fill this need?
    • what do I think I have that comes closest to this ideal part? (I often cannot remember everything I have - so)
    • rummage around several possible storage locations to see if I actually have something that I remember or something else that might fit the bill
    • give up and order something
    • suddenly realize I was looking in the wrong place and find something suitable
    • when the now un-needed part comes in, squirrel it away somewhere where I am never going to forget it
    • and then promptly forget all about it
    • Cancel
    • Vote Up +3 Vote Down