Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Forum How can i test RS-485
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 43 replies
  • Subscribers 126 subscribers
  • Views 14463 views
  • Users 0 members are here
  • connector
  • wiring
  • communication
Related

How can i test RS-485

Dsoky
Dsoky over 3 years ago

Hello, i am looking for a way to test MAX-485 , i do not have any idea how to do it , anyone can help me?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 3 years ago in reply to Dsoky +2
    Perhaps Jan Axelson's book 'Serial Port Complete' might help you ? http://janaxelson.com/spc.htm It covers the basics of serial communications, covers working with RS485 networks, and includes some…
  • KennyMillar
    KennyMillar over 3 years ago in reply to Dsoky +2
    Yeah no problem, here it is: https://www.analog.com/media/jp/technical-documentation/data-sheets/1111.pdf If you have any questions please feel free to ask - I use these chips in loads of things. …
  • Dsoky
    Dsoky over 3 years ago in reply to KennyMillar +2
    Ok good stuff i found that module https://handsontec.com/index.php/product/ft232r-usb-to-serialttl-converter-module/ will that work ?
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    Perhaps something like this tutorial showing two MAX485 modules to connect two Arduinos together may help?

    https://microcontrollerslab.com/rs485-serial-communication-arduino-tutorial/

    If you are using two USB to RS485 convertors, then you wouldn't need the MAX485 IC unless you wanted to add a third node such as an Arduino onto the bus, in which case you would attach the DI and RO pins to the Arduino's serial GPIO pins. You also need to connect the DE and RE enable pins to a GPIO port to be able to toggle the MAX485 driver between transmit and receive states.

    Alternatively, you could use one USB to RS485 convertor connected to the PC and a MAX485 connected to an Arduino and send data from the SSCOM terminal application to the Arduino.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Dsoky
    Dsoky over 3 years ago in reply to beacon_dave

    good idea but with that way i only tested the transmitting part, i mean i tested the MAX485 as a transmitter , how to test it as a receiver?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to Dsoky

    In the linked tutorial, one RS485 module is transmitting and one is receiving so you are testing both transmit and receive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 3 years ago in reply to Dsoky

    In the linked tutorial, one RS485 module is transmitting and one is receiving so you are testing both transmit and receive.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Dsoky
    Dsoky over 3 years ago in reply to beacon_dave

    I understand but these are complex steps for testing i hope i find easier solutions without the need of arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to Dsoky

    Perhaps Jan Axelson's book 'Serial Port Complete' might help you ?

    http://janaxelson.com/spc.htm 

    It covers the basics of serial communications, covers working with RS485 networks, and includes some programming.

    Another useful reference might be this e-Book 'A Practical Guide to Using RS-422 and RS-485 Serial Interfaces'

    https://advantech-bb.com/wp-content/uploads/2014/12/RS-422-RS-485-eBook.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Dsoky
    Dsoky over 3 years ago in reply to beacon_dave

    Thanks a lot!.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to Dsoky

    There is an example of a USB <-> RS485 schematic here which may be of interest:

    http://www.rs485.com/pdffiles/converters/USBA4revB.pdf

    It includes additional logic to automatically enable DE / disable RE on data transmission. It's one of the approaches outlined in Jan's book linked previously.