Connector Technology & Design
  • Technologies
  • More
Connector Technology & Design
Polls Poll: How Significant is Single Pair Ethernet Technology to Engineers and the Industry?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Connector Technology & Design to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 16 May 2020 1:39 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:59 PM
  • Views 2165 views
  • Likes 2 likes
  • Comments 5 comments
Related
Recommended

Poll: How Significant is Single Pair Ethernet Technology to Engineers and the Industry?

Ethernet has been the go-to communication and network protocol in LAN applications for decades It enables the seamless data transmission via TCP/IP. But Ethernet is evolving from the 4- and 8-wire cabling systems to simpler two-wire cabling, called Single Pair Ethernet technology.

 

Poll Question: How Significant is Single Pair Ethernet Technology to engineers and the industry?

  • community survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mp2100
    mp2100 over 6 years ago +2
    I‘m looking forward to seeing this get rolled out. For a lot of uses, the SPE at 10 Mbps is ’good enough’. I don’t need Gbps for everything. I like the idea of the 1000 meter range of it, for use in sensor…
  • DAB
    DAB over 6 years ago +1
    Ethernet was always expected to expand beyond the initial implementation both for more complex and more simple connections. The initial design envisioned tapping into small computers at low data rates…
  • frostybeard
    frostybeard over 6 years ago +1
    In automotive, this is the only kind of ethernet you find - the two-wire twisted pair. They want things to be light and robust in cars. The connectors are not the standard ethernet connectors, but something…
Parents
  • kmikemoo
    kmikemoo over 6 years ago

    I agree with mp2100 that single pair Ethernet will displace profibus and fieldbus - and LONWorks and BACNet.  We will probably still keep their networks as they can be integrated into the larger system, but bandwidth considerations and security should keep them separated - at least for a while.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kmikemoo
    kmikemoo over 6 years ago

    I agree with mp2100 that single pair Ethernet will displace profibus and fieldbus - and LONWorks and BACNet.  We will probably still keep their networks as they can be integrated into the larger system, but bandwidth considerations and security should keep them separated - at least for a while.