Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog C++ library for ST Teseo GPS - pt. 10: 3.0 release - stable
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 9 Feb 2025 9:35 PM Date Created
  • Views 1249 views
  • Likes 6 likes
  • Comments 4 comments
  • raspberry
  • pico
  • c++26
  • nmea
  • c++23
  • Teseo
  • gps
  • teseo_c++
Related
Recommended

C++ library for ST Teseo GPS - pt. 10: 3.0 release - stable

Jan Cumps
Jan Cumps
9 Feb 2025

The Teseo-LIV3 GPS module (as used in shabaz ' GPS / Galileo / BeiDou / GLONASS receiver) talks UART and I2C. I developed an OO driver and parser for it.
The Raspberry Pico port of that library is now ready for release 3.0.

GitHub 3.0 release with binaries

Main changes:

  • the libraries are now implemented as C++ modules

Check the release notes via the link above, for a full list of changes

This version of the project requires CMake 3.28, GCC 14 and a build system that can manage modules. Ninja works.

Summary of Pico connections

Pico resources used only if you use I2C:

  • I2C0
  • SDA: GP16 (Pico I2C0 SDA)
  • SCL:  GP17 (Pico I2C0 SCL)
  • baud: 100 * 1000

for I2C, SDA connects to SDA and SCL to SCL. The PCB that I use has the pull-ups for I2C.

Pico resources used only if you use UART:

  • UART1
  • TX: GP4 (Pico UART1 RX)
  • RX:  GP5 (Pico UART1 Tx)
  • baud: 9600
  • UART1 RX interrupt

for UART, RX connects to TX and vice versa

Pico common resources:

  • RESET: GP18 (optional)
  • 5V: VBUS
  • 0V: GND

image
image: how to hook up the Teseo PCB to a Pico.

visit the github repository (git clone https://github.com/jancumps/pico_gps_teseo.git --recursive)
view the online documentation
Link to all posts.

  • Sign in to reply
Parents
  • shabaz
    shabaz over 1 year ago

    Nice to see this port of your code to Pi!

    I was thinking, that maybe the noise from the Pi might mess up the sensitive GPS receivers. Did it need any careful positioning/separation from the Pi? Or it just works?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to shabaz

    It's for Pico. I don't have a Pi that uses the new GPIO api yet..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    Ah sorry. It was late, brain was not working : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 1 year ago in reply to Jan Cumps

    Ah sorry. It was late, brain was not working : (