Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog C++ library for ST Teseo GPS - pt. 7: 1.0 release with NMEA parser - stable
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 8 Aug 2024 2:01 PM Date Created
  • Views 1245 views
  • Likes 5 likes
  • Comments 4 comments
  • raspberry
  • pico
  • rp2040
  • c++23
  • Teseo
  • OO
  • c++
  • teseo_c++
Related
Recommended

C++ library for ST Teseo GPS - pt. 7: 1.0 release with NMEA parser - stable

Jan Cumps
Jan Cumps
8 Aug 2024

The Teseo-LIV3 GPS module (as used in shabaz ' GPS / Galileo / BeiDou / GLONASS receiver) talks UART and I2C. I developed an OO driver and parser for it.
The Raspberry Pico port is now ready for a stable release.

GitHub Release 1.0, with binaries.

Overview:

  • driver library for Teseo GPS (device independent)
  • parser library for NMEA messages (device independent)
  • UART and I2C implementation for Raspberry Pico / RP2040
  • Teseo driver example (device independent, compiled for Pico)
  • NMEA parser and Teseo driver example (device independent, compiled for Pico)
  • I2C and UART binaries for both examples, ready to drop-and-run on your RP2040

Pico resources used only if you use I2C:

  • I2C0
  • SDA: GP16 (Pico I2C0 SDA)
  • SCL:  GP17 (Pico I2C0 SCL)
  • baud: 100 * 1000

for I2C, SDA connects to SDA and SCL to SCL. The PCB that I use has the pull-ups for I2C.

Pico resources used only if you use UART:

  • UART1
  • TX: GP4 (Pico UART1 RX)
  • RX:  GP5 (Pico UART1 Tx)
  • baud: 9600
  • UART1 RX interrupt

for UART, RX connects to TX and vice versa

Pico common resources:

  • RESET: GP18 (optional)
  • 5V: VBUS
  • 0V: GND

image
image: how to hook up the Teseo PCB to a Pico.

Dependency between examples, libraries and Pico / RP2040 port:

image

Api changes since previous version:

  • the NMEA parser api is new functionality
  • Teseo lib: the command / validation pair changed.
    pair.second is no longer representing the validation line (the NMEA command itself has enough info).
    new use: nmea_rr teseo::gll("$PSTMNMEAREQUEST,100000,0\n\r", "GLL,");
    The first string, the NMEA command, is unchanged.
    The second "check" string now represents the signature of a NMEA reply (and is used for that). 
    Code now uses the first string a command, and as validator for the closing validation line.

Example changes:

  • new example to showcase the Teseo GPS communication lib, together with the NMEA parser lib

Infrastructure changes

  • default build generates binaries for each example, in I2C and UART variant
  • Pico C/C++ SDK compatible
  • GitHub action scripts to validate build and create nightly releases
  • Teseo and NMEA lib are subprojects that can be used in isolation
  • Pico dependent code moved out of examples, into port/pico directory
  • Pico I2C reader is way better and resource-friendlier in this version

Other:

  • requires a C++23 capable toolchain. Developed and tested on GCC 13.3.1
  • tested with Pico C/C++ SDK 1.5.1 and 2.0.0

Development examples

For the full source code of the parser example I review here, check the documentation.

Typical query - response - parse code example - query that returns a single reply:

teseo::teseo gps;
std::string reply;
bool valid; // intentionally uninitialised

// 

nmea::gll o; // NMEA GLL object
valid = gps.ask_gll(reply); // ask Teseo GPS library for GLL data
if (valid) {
    valid = nmea::gll::from_data(reply, o); // fill NMEA GLL object with the reply attributes
}

debugger view after the GLL object is built up:

image

Using the object in your code (print example snippet):

printf("lat: %f, lon: %f.", 
    o.lat, o.lon);

GLL source: gps. lat: 50.863354 lon: 4.376334, time: 11:00:32.000.

Typical query - response - parse code example - query that returns a multiple replies:

teseo::teseo gps;
std::vector<std::string> replies(NMEA_MAX_REPLIES); 
// vector size is a suggestion. STL will allocate at least NMEA_MAX_REPLIES
uint count; // intentionally uninitialised
bool valid; // intentionally uninitialised

// ...

valid = gps.ask_gsv(replies, count);
if (!valid) { return; }
for(auto r : std::ranges::subrange(replies.begin(), replies.begin() + count)) {
	nmea::gsv o;
    valid = nmea::gsv::from_data(r, o);
    
    // .. either use the object, or store it in a container for later use.
}

debugger view:

image

Using the object in your code (example where the retrieved objects are directly used for printing, not stored for later use):

	for(auto r : std::ranges::subrange(replies.begin(), replies.begin() + count)) {
		nmea::gsv o;
	    valid = nmea::gsv::from_data(r, o);
        printf("GSV source: ");
        print_talker(o.source);
        printf(".\r\n");
	    for(const auto s : o.sats) {
            printf("sat prn: %i, elev: %i, azim: %i, snr: %i.\r\n", 
                s.prn, s.elev, s.azim, s.snr);
	    }
	}

GSV source: gps.
sat prn: 3, elev: 84, azim: 344, snr: 21.
sat prn: 2, elev: 48, azim: 135, snr: 27.
sat prn: 17, elev: 48, azim: 271, snr: 25.
sat prn: 4, elev: 43, azim: 182, snr: 43.
GSV source: gps.
sat prn: 19, elev: 36, azim: 303, snr: 14.
sat prn: 21, elev: 32, azim: 133, snr: 21.
sat prn: 28, elev: 20, azim: 56, snr: 0.
sat prn: 31, elev: 20, azim: 92, snr: 0.
GSV source: gps.
sat prn: 6, elev: 16, azim: 304, snr: 0.
sat prn: 9, elev: 13, azim: 204, snr: 37.
sat prn: 49, elev: 31, azim: 179, snr: 41.
sat prn: 0, elev: 0, azim: 0, snr: 0.
GSV source: glonass.
sat prn: 84, elev: 77, azim: 311, snr: 0.
sat prn: 69, elev: 67, azim: 220, snr: 25.
sat prn: 68, elev: 56, azim: 41, snr: 25.
sat prn: 83, elev: 34, azim: 145, snr: 22.
GSV source: glonass.
sat prn: 85, elev: 20, azim: 323, snr: 0.
sat prn: 85, elev: 20, azim: 323, snr: 0.
sat prn: 77, elev: 9, azim: 34, snr: 0.
sat prn: 76, elev: 10, azim: 352, snr: 23.
GSV source: glonass.
sat prn: 67, elev: 8, azim: 41, snr: 0.
sat prn: 0, elev: 0, azim: 0, snr: 0.
sat prn: 0, elev: 0, azim: 0, snr: 0.
sat prn: 0, elev: 0, azim: 0, snr: 0.

visit the github repository (git clone https://github.com/jancumps/pico_gps_teseo.git)
view the online documentation
Link to all posts.

  • Sign in to reply
Parents
  • shabaz
    shabaz over 2 years ago

    This is awesome! Fantastic work. ST engineers should be taking a leaf out of your book (and also taking on board how difficult they made it with the I2C). Glad you've managed to tame it all.

    Also, it's interesting just how much one learns about the planet when experimenting with GPS and reading around it. It had never occurred to me before, that (say) the length of a earth-rotational "day" isn't 24 hours, it varies by a lot over the space of a year! And learning how oceans clump in areas on the planet, due to different densities, making it quite a challenge for GPS to report altitudes with a reference to (say) sea level. And learning how Christopher Columbus was not a nice person. But noticed those sea anomalies!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 2 years ago

    This is awesome! Fantastic work. ST engineers should be taking a leaf out of your book (and also taking on board how difficult they made it with the I2C). Glad you've managed to tame it all.

    Also, it's interesting just how much one learns about the planet when experimenting with GPS and reading around it. It had never occurred to me before, that (say) the length of a earth-rotational "day" isn't 24 hours, it varies by a lot over the space of a year! And learning how oceans clump in areas on the planet, due to different densities, making it quite a challenge for GPS to report altitudes with a reference to (say) sea level. And learning how Christopher Columbus was not a nice person. But noticed those sea anomalies!