Products
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
Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Cheap debugger ($6) for EasyL1105 MSPM0 board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 7 Sep 2025 1:27 PM Date Created
  • Views 1674 views
  • Likes 7 likes
  • Comments 9 comments
  • xds110
  • MSPM0L1105
  • MSPM0
  • easyL1105
  • texas instruments
  • launchpad
  • ti
Related
Recommended

Cheap debugger ($6) for EasyL1105 MSPM0 board

Jan Cumps
Jan Cumps
7 Sep 2025
Cheap debugger ($6) for EasyL1105 MSPM0 board

 shabaz designed a development kit for the recent Texas Instruments MSPM0 microcontroller series. 
In this post, I show how to use a LaunchPad as debugger for that board. Complexity: low.

image
(post that introduces the kit)

 Required hardware and software

  • EasyL1105 kit, with headers soldered to the programmer interface J5
  • an IDE that supports XDS110 debugging. I use ccstudio 20
  • A LaunchPad with XDS110 debugger on board (cheapest: LP-MSPM0C1104, $5.99 from TI store).
  • USB cable to connect LaunchPad to PC
  • 7 patch wires to connect EasyL1105 signals to LaunchPad

I used an MSP432 LaunchPad for this blog. As long as your LaunchPad has XDS110 on board, and it's accessible, it 'll work

Functionality

  • programmer
  • debugger
  • COM port passthrough
  • power

Connections

Remove all jumpers from the EasyL1105. And all (at least the debugger) jumpers of your LaunchPad.

Then connect the two, using patch wires:

image

EasyL1105 LaunchPad
J5.1 GND GND
J5.2 RST RST
J5.3 SWCLK TCK
J5.4 SWDIO TMS
J5.5 3V3 3V3
J3.2 UART0_RXD RXD*
J3.4 UART0_TXD TXD*

*on the LaunchPad jumpers, the TXd and RXd are labeled for the controller side signal. So no Rx/Tx crossing.

On the cheap LP-MSPM0C1104, here are those signals:

image

On the MSP432 LP that I'm using, it's very similar. The table above will guide you through the setup.

image

Double check, then connect the LaunchPad USB to your PC.

Start debugging in ccstudio

Click on your MSPM01105 project. Then call menu Run -> Debug Project (your project name). If this is your first debug attempt, ccstudio will show a debug configuration screen.

On the Basic tab, select debugger XDS110. The MSPM01105 controller should already be correctly selected.

On the advanced tab, select on the root node of the tree. Take over the settings from the image below:

image

If you haven't used your LaunchPad for ages, ccstudio may upgrade its debugger firmware. After that, you should be in business.

Use UART

To connect to the MSPM0 UART, open a serial console via View -> Console -> Serial Console. Open the COM port representing the passthrough (the one named XDS110 Class Application/User UART in your Windows device manager).

Most SDK examples use 9600 baud, 8, N 1.

Happy debugging.

CCS project used in this post: uart_rw_multibyte_fifo_poll_gcc_EasyL1105_20250907.zip

Related posts

  • Sign in to reply
  • Jan Cumps
    Jan Cumps 3 months ago

    You can also do the opposite of what's described in this post: program the LaunchPad with an external debugger.

    Several of the MSPM0 LaunchPads have 2 ARM 10-pin JTAG connectors. One so that you can use the LaunchPad to program other devices.
    The other one allows to connect an external debugger. In the photo below, I use a TI XDS110 debug probe.

    image

    In both uses cases, you have to remove the debug bridge jumpers in the middle of the board, to break the connection between the on-board debugger and the MSPM0.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps 11 months ago

    TI has a Launchpad version of the debugger: LP-XDS110. Or the LP-XDS110ET if you want EnergyTrace Both are lot cheaper than the XDS110 proper.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago

    I corrected UART wiring. Because on a LaunchPad, the jumpers are labeled for the "controller side" signal, don't cross  RXd/TXd.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 1 year ago in reply to Jan Cumps

    Hmm, I have an extended MSP430 development board that might be usable.

    I will have to do some research on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to DAB

    It won't work with an MSP430 board. They have an MSP-FET (flash-emulation-tool) debugger. It doesn't work on ARM controllers.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>