Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Click boards -- The Biggest Add-on Board Collection in the World
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bhfletcher
  • Date Created: 1 Dec 2020 12:36 AM Date Created
  • Views 3941 views
  • Likes 5 likes
  • Comments 4 comments
  • ultra96-v2
  • raspberry compatibility
  • click board
  • click mezzanine
  • mikroelektronika
  • mikroe
  • arduino shield
  • ultra96
  • sphere
  • maaxboard
  • arduino
  • raspberry pi hat
Related
Recommended

Click boards -- The Biggest Add-on Board Collection in the World

bhfletcher
bhfletcher
1 Dec 2020

If you've never heard or used a Click board, now is a great time to check them out.

Click Boards from MikroElektronica

 

MikroElektronika invented the Click boards and the mikroBUS standard to which they fit. MikroElektronika makes the claim, "The Biggest Add-on Collection in the World," and I think they are correct. As of today, November 30th 2020, I can see 974 items on their https://www.mikroe.com/click  landing page, including Sensors, Displays, Wireless transceivers, Motor control, Connection ports, Encoders, speech recognition, thunder detection, and fingerprint scanning.

image

 

mikroBUS

At the heart of the Click technology is the mikroBUS -- a 12-pin, dual-row standard that includes SPI, I2C,  and UART protocols, along with an Analog input and PWM output. Voltage sources of 5V and 3.3V are both accessible on the mikroBUS.

image

96Boards Mezzanine / Ultra96-V2

On the Avnet Ultra96-V1 or Ultra96-V2, you can adapt the 96Boards Low-speed Expansion to two mikroBUS sites using the Click Mezzanine. You can purchase the Click Mezzanine either by itself (AES-ACC-U96-ME-MEZ) or in a bundle (AES-ACC-U96-ME-SK) that includes the mezzanine plus 3 Click boards (USB UART with Microchip MCP2221, 2x16 Character LCD with Microchip controller, and 6DoF inertial measurement unit with ST Micro LSM6DSL).

 

For more information about the Starter Kit, see this page:

96Boards Click Mezzanine Starter Kit

 

For an example project using the Starter Kit, see:

https://www.hackster.io/pablotrujillojuan/manage-usb-i2c-uart-click-board-from-petalinux-in-ultra96-6fa7cf

 

image

Buy 96Boards Click Mezzanine Starter KitBuy 96Boards Click Mezzanine Starter Kit

Buy 96Boards Click MezzanineBuy 96Boards Click Mezzanine

Buy Ultra96-V2Buy Ultra96-V2

Buy Ultra96-V2 I-gradeBuy Ultra96-V2 I-grade

 

Sphere

The Azure sphere MT3620 Starter Kit has native mikroBUS sites on-board. You can read more about some of the example designs for Sphere with Click here:

Using MikroE Click BoardsTm with Microsoft Sphere

Azure Sphere and Click Stepper2 Motor Control

 

Buy Azure Sphere Starter KitBuy Azure Sphere Starter Kit

 

Arduino

Any board that has an Arduino UNO or MEGA Shield interfaces can also be adapted to mikroBUS sockets, which opens up a couple other Xilinx-based boards, like MiniZed and MicroZed with the Arduino Carrier Card. Of course, a number of Arduino type boards are also compatible with these shields as well.

image

Buy Arduino UNO Click ShieldBuy Arduino UNO Click Shield

Buy Arduino MEGA Click ShieldBuy Arduino MEGA Click Shield

Buy MiniZedBuy MiniZed

Buy MicroZed Arduino Carrier CardBuy MicroZed Arduino Carrier Card

 

Raspberry Pi / MaaXBoard

MikroElektronika also offers an adapter for a Raspberry Pi Hat, which is also compatible with the Avnet MaaXBoard. Check out this blog using MaaXBoard, the Click Pi Hat, and Azure:

Sending Data to Azure with MaaXBoard

image

 

Buy Raspberry Pi Click HatBuy Raspberry Pi Click Hat

Buy MaaXBoardBuy MaaXBoard

 

If you're looking to quickly prototype something with your favorite development, it is definitely worth exploring mikroBUS compatibility and if you can use Click boards for your testing. Like I said at the start, it is "The Biggest Add-on Board Collection in the World!"

  • Sign in to reply

Top Comments

  • bhfletcher
    bhfletcher over 5 years ago in reply to gam3t3ch +1
    Definitely not phasing out Raspberry Pi. In fact, there is a Pi Hat Click adapter as well. I just got some additional information this morning, so I will update the blog with the additional info supporting…
Parents
  • 14rhb
    14rhb over 5 years ago

    974 !  I think that should cover just about everything I can imagine/build as well as many things I haven't already thought of. I've collected a few PMoD as the are useful when experimenting with the Digilent dev boards however I think I'll have to get a few of these - I recall a ST Nucleo boards having slots for the Mikrobus. I'll see if there is a nice starter kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • 14rhb
    14rhb over 5 years ago

    974 !  I think that should cover just about everything I can imagine/build as well as many things I haven't already thought of. I've collected a few PMoD as the are useful when experimenting with the Digilent dev boards however I think I'll have to get a few of these - I recall a ST Nucleo boards having slots for the Mikrobus. I'll see if there is a nice starter kit.