Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Blog Renesas Solution Starter Kit for RX23E-A - break out TIMER signals
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 27 Sep 2024 8:49 AM Date Created
  • Views 901 views
  • Likes 5 likes
  • Comments 1 comment
  • RX23e-a
  • renesas
  • d2a28d6e-11d8-11ee-be56-0242ac120002
Related
Recommended

Renesas Solution Starter Kit for RX23E-A - break out TIMER signals

Jan Cumps
Jan Cumps
27 Sep 2024

I'm trying to generate a complementary PWM wave, with dead time, with a timer of  a RX23E-A microcontroller. This signal will later be used to create an excitor signal for precision measurements.

I have an evaluation board from Road test: Renesas Solution Starter Kit for RX23E-A. It has options for USB, CAN and RS-485/profibus. Out of box, it doesn't expose a timer. But it has the capabilities to do so. This blog shows a few modifications I did to get at 4 signals of timer MTU2a (Multi-function timerpulse unit 2).

This post is similar to  Renesas Solution Starter Kit for RX23E-A - break out the SPI signals , but for a different peripheral, and a different connector. Mainly for my own documentation, if I want to revert later.

The application note for this kit shows what I can get at without bodge wires. The connector J2 exposes a number of PWM lines. Including ones for channel MTU3 of the MTU2a peripheral. But one of them is connected to the timer and profibus ICs. So I need to do just a little change.

image

image

On the PCB, I need to mount J2, and remove R89. The resistor is tiny. Luckily, there is a lot of empty space around it. It's easy to remove.

image

It turned out to be very easy. I used a hot air pencil this time, and blew R89 off its pads.
J2 is a standard pin header. Again, there was enough room to solder it in without difficulties.
I taped the resistor on the piece of paper that already had the ones for my SPI mod, and put it back inside the kit's box. In case I want to restore it to its original configuration.

Here's the result:

image

  • Sign in to reply
Parents
  • Jan Cumps
    Jan Cumps over 2 years ago

    I've got a complementary PWM working. Not with dead band yet, but it's a start:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 2 years ago

    I've got a complementary PWM working. Not with dead band yet, but it's a start: