Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
DSP Forum Algo for rms computation?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 166 subscribers
  • Views 3111 views
  • Users 0 members are here
Related

Algo for rms computation?

ggabe
ggabe over 3 years ago

I’m entertaining a true rms computation on MSPM0G3507 for the 10Hz…100KHz range. 

The MCU is limited to 32K RAM, so I’d change the sampling frequency if I can determine the signal is periodic and in the lower frequency range.

Is there any algorithm that aims capture N periods of a periodic signal? 

Should I be better of by going into frequency domain with a proper window function, and possibly trying multiple sampling rates to choose the proper range?

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 3 years ago +1
    What's wrong with: sample (at 500kHz) s square (at 500kHz) sq = s * s mean (at 500kHz) m = m + ( (sq - m) / Ki) square root (at read out rate) rms = m ^ 0.5 Division by a constant can be done…
  • ggabe
    ggabe over 3 years ago in reply to scottiebabe +1
    Yes, it is interesting. TI is selling the EVB for $16 direct. The part is very much a new item, TI is not sampling it yet. The accelerator is cool, but not as advanced as the MSP430's LEA. The benefit…
  • ggabe
    ggabe over 3 years ago in reply to michaelkellett +1
    I think the algorithm with Ki used to be referred as exponential decay averaging. The alternative, the moving averaging has a sensitivity when the weight of the partial periods start to influence the average…
Parents
  • shabaz
    shabaz over 3 years ago

    It sounds like you're trying to measure frequency, although I wasn't sure why. All the decent methods I can think of for measuring frequency would take time to compute : ( For instance by first getting the highest amplitude frequency bucket, and then sweeping inside that bucket using an algorithm.

    Unrelated, I was thinking that it could be possible to make a simple true RMS meter (nowhere near your desired spec) by using a cheap DSP module. There's a basic example here (Example 7):

     Wave Miner: 10 Experiments with a Pi Digital Signal Processor (DSP) 

    It could be completely standalone with that chip incidentally, if the web interface were replaced with a panel meter or moving-coil meter (i.e. all the code residing in the DSP chip). Admittedly very crude, but maybe interesting for those who don't have such a feature in their multimeter.

    Also, the measurement bandwidth could be selected by buttons instead of the web interface too (not sure of the use-case, I only did that feature because it was easy in the DSP).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    It sounds like you're trying to measure frequency, although I wasn't sure why. All the decent methods I can think of for measuring frequency would take time to compute : ( For instance by first getting the highest amplitude frequency bucket, and then sweeping inside that bucket using an algorithm.

    Unrelated, I was thinking that it could be possible to make a simple true RMS meter (nowhere near your desired spec) by using a cheap DSP module. There's a basic example here (Example 7):

     Wave Miner: 10 Experiments with a Pi Digital Signal Processor (DSP) 

    It could be completely standalone with that chip incidentally, if the web interface were replaced with a panel meter or moving-coil meter (i.e. all the code residing in the DSP chip). Admittedly very crude, but maybe interesting for those who don't have such a feature in their multimeter.

    Also, the measurement bandwidth could be selected by buttons instead of the web interface too (not sure of the use-case, I only did that feature because it was easy in the DSP).