Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Interfacing RFID with Freedom board KL-25Z
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 504 subscribers
  • Views 1033 views
  • Users 0 members are here
  • interfacing
  • freescale
  • rfid
  • embedded
  • arm
  • kl-25z
  • module
Related

Interfacing RFID with Freedom board KL-25Z

e14 Contributor
e14 Contributor over 11 years ago

Can someone explain how to interface the rfid module with the freedom board kl-25z.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor +1
    what to use to level shift from 5V to 3.3V? Apart from searching using google, you could use two resistors as a voltage divider. It appears from the datasheet that its just Tx from the chip. The output…
  • gadget.iom
    gadget.iom over 11 years ago in reply to e14 Contributor +1
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    The 16 pin DIP component looks like a MAX232 chip. If you look at the datasheet for that component you will see a T1 in Connection (possibly pin 11).

     

    If you pull out the IC and push a prototyping wire into the socket at that pin, you can connect the other end to your MCU. The communication should then take place at TTL level.

     

    You will also need to level-shift the 5v on the rfid board to 3.3v for your Freescale board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to gadget.iom

    Thank you for the help. Could you also mention what to use to level shift from 5V to 3.3V?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor

    what to use to level shift from 5V to 3.3V?

    Apart from searching using google, you could use two resistors as a voltage divider.

    It appears from the datasheet that its just Tx from the chip.

     

    The output from the MAX232 is RS232 levels so you need to ditch that.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 11 years ago in reply to e14 Contributor

    what to use to level shift from 5V to 3.3V?

    Apart from searching using google, you could use two resistors as a voltage divider.

    It appears from the datasheet that its just Tx from the chip.

     

    The output from the MAX232 is RS232 levels so you need to ditch that.

     

     

    Mark