Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum advice on arm cortex-m embedded hardware
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 505 subscribers
  • Views 1320 views
  • Users 0 members are here
  • recommendations
  • board
  • cortex-m4
  • embedded
  • development
  • arm
Related

advice on arm cortex-m embedded hardware

amrrahmy
amrrahmy over 10 years ago

hello,

I would like to start programming arm cortex-m microcontrollers. the problem I am currently facing is that there is a sea of development boards or prototyping boards with cortex m3 or m4.

 

preferably,

  • I would like the option to program in just C, instead of relying on Arduino libraries for example
  • I would like the option of USB HID and USB host
  • I would like the the microcontroller to be cortex-m4

 

Can someone recommend small development boards?

 

update:

  • by program in C, I meant to say, I would like to use a Linux distribution and use a gnu arm tool-chain/library/compiler to compile, debug, ...etc. I don't want to switch IDEs, and I would like not to rely on Arduino libraries.
  • And I would like the board to be small in size (arduino nano, micro, teensy form factors)
  • It would be easier for me to get a small teensy or an mbed board or an atmel development board(unless element14 has international shipping at a reasonable price?), if there is an option to program in entirely in C.

 

Message was edited by: Amr Rahmy

  • Sign in to reply
  • Cancel

Top Replies

  • bovrchevr
    bovrchevr over 7 years ago +3 suggested
    The new Teensy 3.5 and 3.6 seem to be pretty good from a hardware point of view, and are fairly cheap. However, a platform such as the Mbed has a much larger support and resource base behind it.
  • gihu
    gihu over 10 years ago +2 suggested
    Hi, ST has several nice discovery board for different arm cortex m. There are several IDE that you can use, even I think that now true studio from atollic is free. Cypress has the CY8CKIT-059 CY8CKIT-059…
  • kas.lewis
    kas.lewis over 10 years ago +2 suggested
    TI has their boards with very good support and an IDE that is ready to use CCS. The boards can be found here. There are some under each category (MSP432, CC3200-LAUNCHXL , Tiva C Boards, etc. I hope that…
Parents
  • gihu
    0 gihu over 10 years ago

    Hi,

     

    ST has several nice discovery board for different arm cortex m. There are several IDE that you can use, even I think that now true studio from atollic is free.

    Cypress has the  CY8CKIT-059CY8CKIT-059 is M3(not M4 but Cypress has the Psoc creator a powerfull software for their silicon and you do not really need to worry much about the internal architecture of the core

    Some other boards exits, but these ones are the ones I personally like.

     

    Hope that helps,

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gihu
    0 gihu over 10 years ago

    Hi,

     

    ST has several nice discovery board for different arm cortex m. There are several IDE that you can use, even I think that now true studio from atollic is free.

    Cypress has the  CY8CKIT-059CY8CKIT-059 is M3(not M4 but Cypress has the Psoc creator a powerfull software for their silicon and you do not really need to worry much about the internal architecture of the core

    Some other boards exits, but these ones are the ones I personally like.

     

    Hope that helps,

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer