Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum advice on arm cortex-m embedded hardware
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 505 subscribers
  • Views 1322 views
  • Users 0 members are here
  • recommendations
  • board
  • cortex-m4
  • embedded
  • development
  • arm
Related

advice on arm cortex-m embedded hardware

amrrahmy
amrrahmy over 10 years ago

hello,

I would like to start programming arm cortex-m microcontrollers. the problem I am currently facing is that there is a sea of development boards or prototyping boards with cortex m3 or m4.

 

preferably,

  • I would like the option to program in just C, instead of relying on Arduino libraries for example
  • I would like the option of USB HID and USB host
  • I would like the the microcontroller to be cortex-m4

 

Can someone recommend small development boards?

 

update:

  • by program in C, I meant to say, I would like to use a Linux distribution and use a gnu arm tool-chain/library/compiler to compile, debug, ...etc. I don't want to switch IDEs, and I would like not to rely on Arduino libraries.
  • And I would like the board to be small in size (arduino nano, micro, teensy form factors)
  • It would be easier for me to get a small teensy or an mbed board or an atmel development board(unless element14 has international shipping at a reasonable price?), if there is an option to program in entirely in C.

 

Message was edited by: Amr Rahmy

  • Sign in to reply
  • Cancel

Top Replies

  • bovrchevr
    bovrchevr over 7 years ago +3 suggested
    The new Teensy 3.5 and 3.6 seem to be pretty good from a hardware point of view, and are fairly cheap. However, a platform such as the Mbed has a much larger support and resource base behind it.
  • gihu
    gihu over 10 years ago +2 suggested
    Hi, ST has several nice discovery board for different arm cortex m. There are several IDE that you can use, even I think that now true studio from atollic is free. Cypress has the CY8CKIT-059 CY8CKIT-059…
  • kas.lewis
    kas.lewis over 10 years ago +2 suggested
    TI has their boards with very good support and an IDE that is ready to use CCS. The boards can be found here. There are some under each category (MSP432, CC3200-LAUNCHXL , Tiva C Boards, etc. I hope that…
Parents
  • kas.lewis
    0 kas.lewis over 10 years ago

    TI has their boards with very good support and an IDE that is ready to use CCS. The boards can be found here. There are some under each category (MSP432, CC3200-LAUNCHXL, Tiva C Boards, etc. I hope that helps. Quick and easy to use with LOTS of demo code.

     

    Kas

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 10 years ago

    TI has their boards with very good support and an IDE that is ready to use CCS. The boards can be found here. There are some under each category (MSP432, CC3200-LAUNCHXL, Tiva C Boards, etc. I hope that helps. Quick and easy to use with LOTS of demo code.

     

    Kas

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer