Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Embedded WiFi recommendations?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 34 replies
  • Answers 2 answers
  • Subscribers 505 subscribers
  • Views 5031 views
  • Users 0 members are here
  • wifi
  • 802.11
  • embedded
  • microcontroller
  • wireless
  • arduino
Related

Embedded WiFi recommendations?

fustini
fustini over 15 years ago

Howdy,

 

I was wondering if anyone might have recommendations for WiFi modules for a low-end embedded system.  I'm primarily thinking of Arduino so a simple interface to the radio would be ideal (not USB).

 

Thanks,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • PBrunner
    PBrunner over 15 years ago in reply to e14 Contributor +1 suggested
    You are perfectly right Julian Freescale has actually 3 different Wifi modules based on 3 different chipsets from 3 different suppliers( http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=0152106740AFE4…
  • e14 Contributor
    e14 Contributor over 14 years ago +1
    There is also TI CC3000 which is a UART-to-WIFI module, probably a more compact solution with respect to the MCW1001A+MRF24WB0Mx couple. Although I've used the Microchip's one in a dev-kit of theirs and…
  • Funklord
    Funklord over 14 years ago +1
    The Microchip MRF24WBOMx modules are great, especially due to the low price, and existing code for 8bit PIC, AVR and Arduino etc. I'm successfully using it with an ATMEGA168 (or better) and WPA2/AES encryption…
  • ssilberhorn
    0 ssilberhorn over 14 years ago in reply to e14 Contributor

    Yes some great modules already available via www.ti.com/simplelink or checkout the Ultimate RoadTest and read about the guys experience with the WiFi CC3000+MSP430FRAM KitCC3000+MSP430FRAM Kit

     

    http://www.element14.com/community/groups/ultimate-road-test

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Funklord
    0 Funklord over 14 years ago

    The Microchip MRF24WBOMx modules are great, especially due to the low price, and existing code for 8bit PIC, AVR and Arduino etc.

    I'm successfully using it with an ATMEGA168 (or better) and WPA2/AES encryption.

    You do NOT need MCW1001A or any other chip to control it, an 8bit micro with around 6k flash to spare is enough.

     

    They can be gotten for around 17eur/each @100pcs here:

    http://se.mouser.com/Search/Refine.aspx?Keyword=mrf24wbom

    Although they are probably cheaper from microchip direct.

     

    I believe the original designer is Gainspan, but I'm not sure.

     

    A while ago, I had a few small breakout boards fabricated for connecting a MRF24WBOMx to SPI with a single 9 pin 2.54mm header... interrupts (optional) and such are broken out.

    If anyone is interested, I have a few extra boards I could send.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Funklord

    Hi Funklord, could you spare a bit more details on the software side of these project of yours?

    How did you get to use an MRF24WB0M with only 6KB of code? Even more on platforms different from microchip?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Funklord
    0 Funklord over 14 years ago in reply to e14 Contributor

    I've hooked up the MRF24WB0M like this: http://store.weburban.com/store-weburban/wifi.html

    It's compatible with WiShield and some other Wifi libs for Arduino.

     

    git clone git://github.com/asynclabs/WiShield.git

     

    Info about WiShield and its' lib:

    http://asynclabs.com/wiki/index.php?title=AsyncLabsWiki

     

    I just tested compiling the web server example for atmega328, which showed Binary sketch size: 10996 bytes

    Obviously text parsing (http) bloats the code tremendously, so, not recommended on an 8bit micro, unless you like to waste memory ;P

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to Funklord

    Thanks for the tip.  I'm going to be returning to my wifi project in a little bit with the aim of building about 10 devices which display calendar meeting status on an LCD.  I'll be looking to make a design with minimal cost so the WiFly shield I had been using is definitely out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robotonics
    0 robotonics over 14 years ago

    I have finally managed to get the PIC24EP512GU810-I/PFPIC24EP512GU810-I/PF Starter kit + MRF24WB0MA to run the demo web page, and so far have just toggled led's and buttons on the board.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to robotonics

    Great to see.  I think I'll probably go with that WiFi module, but it'll will be a tough decision to go AVR or PIC when I start working on my wifi project again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MicrochipRTCfr
    0 MicrochipRTCfr over 14 years ago in reply to fustini

    Hi,

     

    Thanks to the recent acquisition of RovingNetworks by Microchip, there are plenty of new 802.11B/G WiFi modules, adapters and developers kits which can be also used for embedded low power WiFi applications : http://www.rovingnetworks.com/products/Wi_Fi_Products

    The modules will become easier to source on a worldwide basis in the next months through the larger global sales network from Microchip.

     

     

    The modules are UART / SPI based. Any microcontroller can control them easily as the TCP/IP stack run on the WiFi module itself ;=)


    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robotonics
    0 robotonics over 14 years ago in reply to MicrochipRTCfr

    Thanks for that! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fustini
    0 fustini over 14 years ago in reply to MicrochipRTCfr

    Yeah, I'd seen a headline for that - very interesting.  I have actually been using RN-131C which is on SparkFun's WiFly Arduino shield.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>