Embedded and Microcontrollers
  • Technologies
  • More
Embedded and Microcontrollers
Embedded Forum Freescale Kinetis software & mbed.org compiler
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Embedded and Microcontrollers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 503 subscribers
  • Views 2155 views
  • Users 0 members are here
  • kinetis
  • mbed
  • k64f
  • ksdk
Related

Freescale Kinetis software & mbed.org compiler

e14 Contributor
e14 Contributor over 11 years ago

Has anyone any experience (successful preferably) at exporting code from mbed to Kinetis SDK?

I have been playing with a FRDM K64F board and found it much easier to create code using the mbed compiler.

However debugging is a complete mystery to me ( other than printf statements)

The learning curve for KDSK etc is extreemly steep.

My main misfortune is to use WIN8.1

secondly to choose a recently released mbed device where most documentation is for something else!

So a few pointers would be gratefully received.

georgemm101

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to clem57 +1
    I was actually able to do this for the FRDM-K64F last week. I took one of the basic pre-built examples in mbed.org and brought it into Kinetis Design Studio, and could successfully compile and debug. I…
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 11 years ago +1
    Hi guys This discussion should be probably moved to the dedicated place in Design Center for the Freedom Development Platform HERE as the informations will be useful for other Freedom and mbed users Thank…
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor +1
    That's why I wait for others to cross the frontier! Clem
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    In mbed, right click on your project and select "Export Program..."

    image

     

    Then in the dialog box that comes up, select the Kinetis Design Studio toolchain under "Export Toolchain:" and then click on the Export button. You could of course also select the other available toolchains like Keil or IAR.

    image

     

    The website will think for a while and then give you a zip file to download. Unzip it, and import it into KDS like normal (see here for an example: [FRDM-K64F + Kinetis Design Studio (KDS) + Software Dev Kit (SDK)] Tutorial: Toggling an RGB LED without Processor expert).

     

    It'll compile and there are OpenOCD/CMSIS-DAP debug configurations already prepopulated to easily start debugging via the OpenSDAv2 circuit on the board.

     

    Inside that zip directory you can also find the KSDK HAL code at \<project_name>\mbed\TARGET_K64F\TARGET_Freescale\TARGET_KPSDK_MCUS\TARGET_KPSDK_CODE

    This obviously is only true for devices supported by KSDK and mbed enabled, so the FRDM-K64F and FRDM-K22F

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks Anthony I will give it a go later.

     

    George

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    As with everything to do with kinetis, its the detail that counts!

    Importing the project is half the battle. I was unable to do any debugging until the Segger openSDA Bootloader was installed in the K64F Board ( not the mbed version).

    I never finished debugging, for that matter i never really stated as i got distracted by KDS V2.0 being released.

    So now I am back at square one.image

    KDS2 .0 is another story, typical of the lack of attention to detail by Freescale.

    Do they do Quality at Freescale?

    Does anybody check the release before it goes out?

    I guess we have to install the KDSK again! what else is missing?

    I have spent weeks struggling with the beta version, and 1.1.1, so now its start over............

    I am rapidly loosing the will to live.....

    Is there a product that works first time

    george

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    That's why I wait for others to cross the frontier!image

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi george,

    You have to install the KSDK eclipse plugin first. That plugin is what tells KDS (and other eclipse based tools) about Kinetis SDK.  Instructions are in Section 4.4.1 of the C:\Freescale\KSDK_1.0.0\doc\Kinetis SDK K64 User's Guide.pdf

     

      Then when using the new project wizard, you also have to make sure you're selecting a device/board supported by Kinetis SDK.

     

      You don't have to re-install KSDK. Hope that helps.

     

    -Anthony

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi george,

    You have to install the KSDK eclipse plugin first. That plugin is what tells KDS (and other eclipse based tools) about Kinetis SDK.  Instructions are in Section 4.4.1 of the C:\Freescale\KSDK_1.0.0\doc\Kinetis SDK K64 User's Guide.pdf

     

      Then when using the new project wizard, you also have to make sure you're selecting a device/board supported by Kinetis SDK.

     

      You don't have to re-install KSDK. Hope that helps.

     

    -Anthony

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer