Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Blog Repairing a CQ-VX5500 CD/MD Car Stereo
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 28 Aug 2022 3:55 PM Date Created
  • Views 10070 views
  • Likes 9 likes
  • Comments 11 comments
  • audio
  • CQ-VX5500
  • car stereo
  • panasonic
  • repair
  • automotive
Related
Recommended

Repairing a CQ-VX5500 CD/MD Car Stereo

shabaz
shabaz
28 Aug 2022

Introduction

I was recently given a car stereo to fix, and it's possibly the most good-looking piece of equipment I've seen in a long while!

I figured I would document the repair project a bit, since there's not a lot of information on the Internet about it, and it's sometimes nice to see device internals.

The video shows the stereo.. the owner clearly has good music taste, the Django Unchained music CD was already inside:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This model was released around 2001 in Japan, and cost about $760 USD when new. There is a D-suffix and a K-suffix version (the D-suffix version is silver).

The MiniDisc Wiki has a bit of information on it.

Connections

The diagram here shows the pinout.

image

The connectors and cables were dirty/greasy as expected, and had bad connections. I replaced with Molex Mini-Fit Jr (reviewed here) since I had the crimp tool for that, and they are nice connectors for this application.

image

The vehicle uses an ISO 10487 connector and so I attached the mating Mini-Fit Jr connectors to that too. I also made up some test cables so that I could attach a power supply and a speaker or speaker simulator.

image

The new connectors did the trick, and the system pretty much worked apart from the MiniDisc player.

MiniDisc Player

The MiniDisc player doesn't function but it may be a fault with the disc I was using. If you've never seen a MiniDisc before, they are really tiny, in my opinion near-ideal storage medium for music before Flash memory became cheaper.

image

Although the mechanism works, I reckon the optical components of the MiniDisc player may have dust on them, since the stereo had some dirt inside. I blasted with some canned air, but didn't take this mechanism further apart. Hardly anyone uses MiniDisc anymore so I don't think it's worth the repair effort.

image

Japanese FM Band

A more severe issue is that the unit is a grey import, and doesn't support UK FM operation. The tuner is set to the Japanese frequencies. Taking a peek at the circuit board shows the FM synthesiser (Sanyo LC72135), main microcontroller (the NEC chip visible in the photo below), and the FM tuner module (the long metal can partially visible on the right side edge of the photo). 

image

There are a bunch of resistor positions that perhaps may select the region, and you can see a bit of flux on the photo where I attempted to solder resistors. Unfortunately I didn't figure it out; with all resistor combinations that I tried, the frequency band did not change. There is a pinhole reset button on the front panel of the car stereo, and I pressed that each time I made a resistor change, but it only seems to reset the device without wiping its configuration.

I suspected that the resistors to change were those that were 0805-sized rather than 0603-sized.

I don't have a schematic, but the ElectroTanya website offered a service manual for the CQ-TX5500, so I looked at that instead. I experimented with the resistors highlighted here:

image

A bit more of the schematic from that CQ-TX5500 model (click to zoom):

image

The configuration is likely stored in the FRAM chip visible to the right of the NEC microcontroller chip. I could desolder it and extract the contents, but there's only finite time to try to repair this car stereo, and I didn't do this. Even if I succeeded in changing the band in this manner, it still may not work if the VCO connected to the synthesizer chip needs adjustment/component changes. For now, if the owner wishes to use the FM band in the UK, there is the possibility to purchase a cheap band converter device that connects to the antenna socket (the wrong frequency will be displayed however). It's an ugly solution, but it is a solution.

Summary

With a bit of clean-up the car stereo functions adequately. It's a 20-year old car stereo but there's plenty of life in it, it is well made. I just wish Panasonic had published some information to help change the FM band, but it is pretty normal for manufacturers not to do that, since it affects their sales arrangements in different regions. I still need to give it a proper listen, but it sounds great, and looks awesome. This will be returned to the owner soon.

Thanks for reading!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 4 years ago +1
    Very nice. I miss the days when things were built to last. I have a Sony CD/Cassette tape player I bought about 25 years ago. Still works and sounds great.
Parents
  • Gough Lui
    Gough Lui over 4 years ago

    That looks like a stereo that Techmoan (YouTube) would approve of, especially given those prominent analog VU meters!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Gough Lui
    Gough Lui over 4 years ago

    That looks like a stereo that Techmoan (YouTube) would approve of, especially given those prominent analog VU meters!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 4 years ago in reply to Gough Lui

    Hehe love Techmoan!