Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Blog Repairing a CQ-VX5500 CD/MD Car Stereo
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 28 Aug 2022 3:55 PM Date Created
  • Views 8234 views
  • Likes 9 likes
  • Comments 11 comments
  • audio
  • CQ-VX5500
  • car stereo
  • panasonic
  • repair
  • automotive
Related
Recommended

Repairing a CQ-VX5500 CD/MD Car Stereo

shabaz
shabaz
28 Aug 2022

Introduction

I was recently given a car stereo to fix, and it's possibly the most good-looking piece of equipment I've seen in a long while!

I figured I would document the repair project a bit, since there's not a lot of information on the Internet about it, and it's sometimes nice to see device internals.

The video shows the stereo.. the owner clearly has good music taste, the Django Unchained music CD was already inside:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

This model was released around 2001 in Japan, and cost about $760 USD when new. There is a D-suffix and a K-suffix version (the D-suffix version is silver).

The MiniDisc Wiki has a bit of information on it.

Connections

The diagram here shows the pinout.

image

The connectors and cables were dirty/greasy as expected, and had bad connections. I replaced with Molex Mini-Fit Jr (reviewed here) since I had the crimp tool for that, and they are nice connectors for this application.

image

The vehicle uses an ISO 10487 connector and so I attached the mating Mini-Fit Jr connectors to that too. I also made up some test cables so that I could attach a power supply and a speaker or speaker simulator.

image

The new connectors did the trick, and the system pretty much worked apart from the MiniDisc player.

MiniDisc Player

The MiniDisc player doesn't function but it may be a fault with the disc I was using. If you've never seen a MiniDisc before, they are really tiny, in my opinion near-ideal storage medium for music before Flash memory became cheaper.

image

Although the mechanism works, I reckon the optical components of the MiniDisc player may have dust on them, since the stereo had some dirt inside. I blasted with some canned air, but didn't take this mechanism further apart. Hardly anyone uses MiniDisc anymore so I don't think it's worth the repair effort.

image

Japanese FM Band

A more severe issue is that the unit is a grey import, and doesn't support UK FM operation. The tuner is set to the Japanese frequencies. Taking a peek at the circuit board shows the FM synthesiser (Sanyo LC72135), main microcontroller (the NEC chip visible in the photo below), and the FM tuner module (the long metal can partially visible on the right side edge of the photo). 

image

There are a bunch of resistor positions that perhaps may select the region, and you can see a bit of flux on the photo where I attempted to solder resistors. Unfortunately I didn't figure it out; with all resistor combinations that I tried, the frequency band did not change. There is a pinhole reset button on the front panel of the car stereo, and I pressed that each time I made a resistor change, but it only seems to reset the device without wiping its configuration.

I suspected that the resistors to change were those that were 0805-sized rather than 0603-sized.

I don't have a schematic, but the ElectroTanya website offered a service manual for the CQ-TX5500, so I looked at that instead. I experimented with the resistors highlighted here:

image

A bit more of the schematic from that CQ-TX5500 model (click to zoom):

image

The configuration is likely stored in the FRAM chip visible to the right of the NEC microcontroller chip. I could desolder it and extract the contents, but there's only finite time to try to repair this car stereo, and I didn't do this. Even if I succeeded in changing the band in this manner, it still may not work if the VCO connected to the synthesizer chip needs adjustment/component changes. For now, if the owner wishes to use the FM band in the UK, there is the possibility to purchase a cheap band converter device that connects to the antenna socket (the wrong frequency will be displayed however). It's an ugly solution, but it is a solution.

Summary

With a bit of clean-up the car stereo functions adequately. It's a 20-year old car stereo but there's plenty of life in it, it is well made. I just wish Panasonic had published some information to help change the FM band, but it is pretty normal for manufacturers not to do that, since it affects their sales arrangements in different regions. I still need to give it a proper listen, but it sounds great, and looks awesome. This will be returned to the owner soon.

Thanks for reading!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 3 years ago +1
    Very nice. I miss the days when things were built to last. I have a Sony CD/Cassette tape player I bought about 25 years ago. Still works and sounds great.
  • Akentphoto
    Akentphoto over 1 year ago

    Hopefully you can be a life saver,

    I recently installed one of these decks and the CD player was working great.  I then decided to try a MD that I verified before inserting. It accepted the disk then promptly switched to no disk inserted.  After going through the manual it says it is suppose to automatically eject for pretty much any reason.  Apart from that contact the store you purchased from. Same goes for the CD player. Apart from that contact the store you purchased from. Great.  Fast forward a few weeks of the CD player working and it suddenly did the same thing.  

    My main question is if you might have discovered or have photos of a way to manually eject either of the disks without removal?  Some players back in the day had that slot for a paper clip to push it out...?  My worry is the Lazer died and that is why it's not seeing the disk at all.  The  I'm also not getting any errors so I'm a little confused.  Worst case scenario I can use a phone or portable MD player but I was really enjoying going through old CDs...

    Thank you in advance if you have any insights!

    Ps I got bit hard by the old Lumix M43 system.  The GM1 is such good travel camera!  Too bad the secret is already out and prices are double or more compared to 4 years ago...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 3 years ago

    Very nice.

    I miss the days when things were built to last.

    I have a Sony CD/Cassette tape player I bought about 25 years ago. Still works and sounds great.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Gough Lui

    Hehe love Techmoan!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    That looks like a stereo that Techmoan (YouTube) would approve of, especially given those prominent analog VU meters!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 3 years ago in reply to Jan Cumps

    I do agree with you.  I may have poorly expressed my opinion.  I too have been a vintage audio fan.  My last turntable was a very nice Bang & Olufsen, teamed up with some nice Kenwood components and JBL studio speakers.  I broke into audio through building a high school radio station studio and through touring many professional studios (also hanging around with some serious audiophiles).  I dreamed of a tube based amplifier (McIntosh) but could afford the Kenwood.

    When I moved in with my wife (many years later), a wall full of stereo was too much, so I sold it Frowning2

    My recent search for a car stereo was an exercise in futility.  The brands that I used to consider as great were now so so (Alpine for example).  The process was so frustrating that I just gave up and am suffering with a messed up stock Toyota Prius stereo that routinely looses its mind leaving most of the controls useless.  I am sure my frustrations are caused by a lack of current knowledge of stereos and stereo manufactures

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>