Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Want to replace resistors myself, but need an advice
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 311 subscribers
  • Views 3894 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Want to replace resistors myself, but need an advice

vladnech
vladnech over 5 years ago

Hi guys

 

It has been a long time since I soldered something, but with COVID-19 decided to dust off my knowledge about electronics.

My air-fryer Philips XXL (5 years old) stopped to switched on (after I felt the smell of something burnt out).

I found resistors got burnt - see pictures

.

I need your help what Om and W value of those ones?

Looks like they have 4 bands: Orange, Black, Black, Gold, which is 30 Om.

Not sure whether it is correct. Plus, not sure how to find W.

 

Thanks in advance for your help,

Vlad

Attachments:
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago +4
    Hi Vlad, I agree with Jan that the black capacitor near the transformer looks like it has over heated and is probably damaged. If you have a meter it would not hurt to measure the resistance of the heat…
  • dougw
    dougw over 5 years ago +3
    The power rating can usually be deduced from the physical size. These look to be about 1W. but I'm not sure from the picture exactly how big they are. . They don't look burned enough to be smelling burnt…
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to vladnech +3
    L1 is an inductor. It indeed looks like there's a blowhole in the IC. For the glue-like compound: has something melted above the IC and dripped down on the IC?
Parents
  • jw0752
    jw0752 over 5 years ago

    Hi Vlad,

     

    I agree with Jan that the black capacitor near the transformer looks like it has over heated and is probably damaged. If you have a meter it would not hurt to measure the resistance of the heat damaged resistors before you try to remove them. I have seen where a color band will change from a color to black when heated to an extreme. Based on the physical size of the resistors relative to the other components my guess would be that they are 1/2 Watt. With the damage to the capacitor and the resistors be aware that they may be symptoms of a failure and not the actual failure itself. There is a reddish brown cylinder on the board near the white relay. I would like to know what the markings on it are. I was trying to imagine what would cause resistors and a capacitor to over heat and what comes to mind is the failure of a rectifier. This would allow AC to be applied to the DC side of the circuit and short out the capacitor which in turn would cause a higher current and over heat the resistors. Of course this is speculation based on insufficient information so it is only one idea. In any case I would look at all the components whether they have visible damage or not before reapplying power.

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 5 years ago

    Hi Vlad,

     

    I agree with Jan that the black capacitor near the transformer looks like it has over heated and is probably damaged. If you have a meter it would not hurt to measure the resistance of the heat damaged resistors before you try to remove them. I have seen where a color band will change from a color to black when heated to an extreme. Based on the physical size of the resistors relative to the other components my guess would be that they are 1/2 Watt. With the damage to the capacitor and the resistors be aware that they may be symptoms of a failure and not the actual failure itself. There is a reddish brown cylinder on the board near the white relay. I would like to know what the markings on it are. I was trying to imagine what would cause resistors and a capacitor to over heat and what comes to mind is the failure of a rectifier. This would allow AC to be applied to the DC side of the circuit and short out the capacitor which in turn would cause a higher current and over heat the resistors. Of course this is speculation based on insufficient information so it is only one idea. In any case I would look at all the components whether they have visible damage or not before reapplying power.

     

    John

    • Cancel
    • Vote Up +4 Vote Down