Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Colorsound Power Boost - Another issue!!!
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 317 subscribers
  • Views 6521 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Colorsound Power Boost - Another issue!!!

Andy Betts
Andy Betts over 5 years ago

Hi guys,

 

Been a long time since I posted here and i have another issue for you that hopefully you might be able to help with.

 

I've just recently built another Power boost pedal for a client. I etched the board myself using the photo resist method, it came out not too bad save for a couple of areas where the tracks were broke. i patched them up with copper tape that has conductive adhesive. I've checked for continuity and all is fine where the patches are. Here are the pictures of the board and also for reference the schematic.

 

 

image

 

imageimage

 

I've built a few of these now and have had no issues with the circuit or builds until now. I built this one, wired it to my test rig and there is no sound at all.... it's totally dead as if it's not in the circuit at all. I've checked for voltage on input and it's ok. I've checked for continuity in the circuit and it seems ok. i don't know what the voltages should be in the various sections of the circuit so haven't checked them. I've gone basic and checked the input and output wires for breaks and they're ok. I've also checked the test rig with a known good circuit and it's OK.

 

i think there might be a duff component but not sure on first steps to troubleshoot.... Any help will be greatly received.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago in reply to Andy Betts +3
    What value is the blue bodied resistor - it looks like 1.8M brown grey green - if its meant to be 180k that would explain things. I could be being misled by pictures. MK
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to geralds +3
    geralds wrote: ... Tip: use your finger as a signal injector. - You are a 60Hz (in AUT I'm a 50Hz sender ) sender "brummmmmm.....!!!""", so you can check the signal with a signal follower (mini-amp with…
  • Andy Betts
    Andy Betts over 5 years ago +3
    I've taken a higher res photo of the board.... this is how it stand now after reflowing the 3k9 resistor and bridging the break in the track on the Q3 base
Parents
  • Andy Betts
    Andy Betts over 5 years ago

    I've taken a higher res photo of the board.... this is how it stand now after reflowing the 3k9 resistor and bridging the break in the track on the Q3 base

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 5 years ago in reply to Andy Betts

    image

    The Q3, is this transistor broken? It seems that there is a burned hole.

    What's the name of the 3 transistors?

    The PCB, hm.... are the pots on an fixed place, or can you rearrange all parts on the board?

    Because it is better, if you makes a smaller board with optimized track wiring.

    Also the parts, for such tone control preamp they are a bit big.

    How look the other boards, which are working right? Are they with the same layout?

     

    Tip:

    You can check the basic functionality of the transistor with an Ohm-Meter.

    For an NPN: plus (red pin of the meter)  to B and minus to C or E, and the Ohm are low; or minus to B and plus to C or E, and the Ohm are high (MOhm or more).

    For an PNP: minus to B and plus to C or E, the Ohms are low.

    If you check E to C, a good transistor has an "endless" Ohm (GOhm), otherwise the diodes in the tr. were melted.

    Or you can also check the tr. with an diode-meter, or you have a transistortesting on your multimeter.

    Gerald

    ---

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 5 years ago in reply to Andy Betts

    image

    The Q3, is this transistor broken? It seems that there is a burned hole.

    What's the name of the 3 transistors?

    The PCB, hm.... are the pots on an fixed place, or can you rearrange all parts on the board?

    Because it is better, if you makes a smaller board with optimized track wiring.

    Also the parts, for such tone control preamp they are a bit big.

    How look the other boards, which are working right? Are they with the same layout?

     

    Tip:

    You can check the basic functionality of the transistor with an Ohm-Meter.

    For an NPN: plus (red pin of the meter)  to B and minus to C or E, and the Ohm are low; or minus to B and plus to C or E, and the Ohm are high (MOhm or more).

    For an PNP: minus to B and plus to C or E, the Ohms are low.

    If you check E to C, a good transistor has an "endless" Ohm (GOhm), otherwise the diodes in the tr. were melted.

    Or you can also check the tr. with an diode-meter, or you have a transistortesting on your multimeter.

    Gerald

    ---