Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum How do you connect LED's in parallel?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 324 subscribers
  • Views 3474 views
  • Users 0 members are here
  • electronic circuit design
  • led array
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

How do you connect LED's in parallel?

colporteur
colporteur over 5 years ago

I have a need to connect a number of LED's in parallel. Can someone share their insight into why an additional resistor is required for the LED's of different colour in parallel to light?

 

The LED's in circuit A lights with no issues. In circuit B, only the Red LED lights. Circuit C lights both LED's but requires the extra resistor to achieve the success.

 

My formal electronics training occurred when vacuum tubes were still common in electronics. My understanding would be voltage drops. The Green LED requires a higher voltage drop to light than a Red LED. Circuit B doesn't light because the Red LED lights with it's voltage drop not being sufficient for Green to light.

 

I appreciate this is a pretty simplistic circuit. I find for myself exploring the basics refreshes the knowledge retained in my magnetic core memory:)

image

  • Sign in to reply
  • Cancel

Top Replies

  • geralds
    geralds over 5 years ago +3
    Hi, this is just a basic calculation. The datasheet describes more details. Best Regards Gerald ---
  • neilk
    neilk over 5 years ago in reply to colporteur +3
    Sean, have a look here (sorry about the length of the URL): https://reviseomatic.org/help/e-diodes/Diodes%20Light%20Emitting.php#:~:text=LEDs%20emit%20light%2C%20only%20when%20they%20are%20forward%20biased…
  • colporteur
    colporteur over 5 years ago in reply to neilk +3
    Thanks for the resource link. I wish I was sitting across the table at coffee break with a napkin to better generate an understanding.
Parents
  • geralds
    geralds over 5 years ago

    Hi,

    this is just a basic calculation. The datasheet describes more details.

    image

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 5 years ago

    Hi,

    this is just a basic calculation. The datasheet describes more details.

    image

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 5 years ago in reply to geralds

    That is where the waters get muddy.

    image

     

    You would think the Green would work and the Red not when they are in series without the resistor. That is not the case. I can't work out the voltage divider to arrive at the bias voltage on the device.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 5 years ago in reply to colporteur

    Sean, have a look here (sorry about the length of the URL):

     

    https://reviseomatic.org/help/e-diodes/Diodes%20Light%20Emitting.php#:~:text=LEDs%20emit%20light%2C%20only%20when%20they%20are%20forward%20biased.&text=Typical%20LEDs%20have%20about%202,colour%20and%20type%20of%20LED).

     

    Includes forward bias voltages for all colours and says "LEDs in parallel - bad idea; LEDs in series - OK"

     

    Neil

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to neilk

    Thanks for the resource link.

     

    I wish I was sitting across the table at coffee break with a napkin to better generate an understanding.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 5 years ago in reply to colporteur

    The point is what Mr Kirchhoff once said.

    The sum of the incoming currents is the sum of the outgoing currents.

    For the thought with the LED wiring:

    An LED is a diode, that's it.

    In one direction it is a wire, in the other direction an "insulator".

     

    If a network (Kirchhoff) now divides the LED currents, and each LED has a different differential resistance,

    then a different current flows through the respective LED due to the exemplar-specific voltage drop,

    which can overload this relevant LED.

    So there will be more current flowing through a low voltage drop LED.

    -> An (the) other LED, which is still under the drop voltage (U_LED_forward) will not work until the voltage will go higher over this forward voltage of that LED.

     

    !! You can't see it optically (except with a measuring device), but the LED gets hot. !!

     

    You could also operate an LED without a protective resistor, but that only works when the "knee" changes,

    when the reverse voltage U_LED_forward is switched to the conductive state.

    And exactly THERE must the current be limited exactly.

    The diode, followed by the LED, is a current-operated component.

    There can also draw µA through the LED, but you cannot see this, but this current can heat the LED.

     

    There are also LEDs with 3V or more U_LED_forward.

     

    Therefore, for a given stable voltage, the series resistor is calculated taking into account the voltage drop from the

    diode and the temperatures (ta tc) so that the parameters are never exceeded during operation.

    So you can NOT excessively increase a voltage in the direction of current flow.

    The data sheet of the LED usually states from which current a defined suitable light output (100% desired) is achieved,

    and this is used as a parameter.

    Then there are tolerances, such as 100% + or - light output at temperatures, current limits, etc., without having to cool the diode or LED.

     

    !! So a separation the two, or more LEDs "parallel" is necessary.

    !! Each LED needs a separate resistor, if you use a parallel circuit.

     

    As Neil said, in serial, this is possible. But how high you want going with the supply voltage?

    If you have 12V, hm.... no  many LEDs you can use, and 1 resistor for the current flow is will be enough.

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down