Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help -> generate 0 - 50mV dc with arduino
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 315 subscribers
  • Views 2503 views
  • Users 0 members are here
  • arduino mega 2560
  • spi
  • 50mv output
  • dc
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help -> generate 0 - 50mV dc with arduino

phoenixcomm
phoenixcomm over 4 years ago

Is there a way I can generate 0 to 50mV for a meter (dc most likely) from an Arduino Mega?? Any thoughts would be appreciated.

I need two of the sources. so the cheaper the better.

~~Cris

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago in reply to dougw +6
    The capacitor value may not be ideal. The time constant of the RC filter is 10us as drawn. With a PWM frequency of 64kHz (about as fast as an Arduino can go) this will make a lot of ripple. The ripple…
  • dougw
    dougw over 4 years ago +5
    The analogWrite instruction uses PWM and a resistor and capacitor on the pin to generate an analog voltage: https://www.instructables.com/Arduino-RC-Circuit-PWM-to-analog-DC/ The Mega can have 14 PWM pins…
  • Andrew J
    Andrew J over 4 years ago +5
    You're probably aware of this Chris, but it may be worth stating anyway. An IO pin is absolute maximum 40mA but recommended at 20mA. Additionally, there is an overall maximum current draw across all pins…
Parents
  • shabaz
    shabaz over 4 years ago

    Hi Cris,

     

    I just remembered I had to drive a meter with Arduino too a while back, although I used an Arduino Micro, maybe the ideas are similar with Arduino Mega).

    The info is here:

    Sensirion Gas/Temp/Humidity Sensor Kit - Review

    image

     

    The code is here:

    https://github.com/shabaz123/FeelWellMeter/blob/master/env-sensor.ino

    I don't remember it in any detail, but line 23 in the code there defines the constant 'meter' to be pin PB5, where the meter is wired as can be seen in the diagram above.

    image

     

    Lines 339-344 set up the PWM mode, and this may change on Arduino Mega.

    image

    Then, whenever the meter reading needs to change, then 'meter' is just set to a different value.

    For example, to make the needle swing to maximum, then wait three seconds, then swing to minimum, the following code is used (max and mmin can be calculated or just try any values for experimentally determining them, in my case they were 100 and 3500 respectively, for the 100uA meter):

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz

    shabaz looks very straight forward I shall give it a try. From what I am seeing for my 50mv meter all I will have to do double R1 to about 95 ohms.

    Thank you immensely.

    ~~ Cris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to phoenixcomm

    shabaz I also looked at your stuff on git hub.  nice work. You don't mind if I borrow some of it. And of course, I will give affirmations. in each function.

    ~~Cris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to phoenixcomm

    shabaz I also looked at your stuff on git hub.  nice work. You don't mind if I borrow some of it. And of course, I will give affirmations. in each function.

    ~~Cris

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 4 years ago in reply to phoenixcomm

    Hi Cris,

     

    Great, I hope it helps! Feel free to use any code, and looking forward to hear how it goes!