Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Have a question about ADCs or DACs? Ask our Expert, Nick Gray
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 118 replies
  • Subscribers 345 subscribers
  • Views 17209 views
  • Users 0 members are here
  • expert
  • nick_gray
  • power
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Have a question about ADCs or DACs? Ask our Expert, Nick Gray

ChristyZ
ChristyZ over 16 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Question about Communications in the element14 Community Wireless Communications Technology group. You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


Nick Gray

 

Nicholas Gray

Nicholas has worked in the Semiconductor industry for over 30 years and has authored a number of published articles about data converters (ADCs and DACs) and signal integrity issues.

 

  • Sign in to reply
  • Cancel

Top Replies

  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor +1
    Hi, Ben, A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable…
  • nickgray
    nickgray over 14 years ago in reply to YT2095 +1
    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then…
  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor

    Hi Mukund,

     

    I am not sure just what you want to do. I know you want to convert the radio waves coming from your mobile phone, but I do not know what you want to do with the energy once you "convert" it. If you want to decode the information coming from it, you really need the equivalent of a mobile system base station, which is a LOT of circuitry. The information transmitted in addition to the voice or text information includes a lot of things, including information needed to know when to change receive and transmit frequencies when the mobile phone leave one cell area and enters another.

     

    If you mean convert it to electrical energy for general use, like replacing a battery or something, than that is not practical because it the energe generated is so small that it is almost completely useless.

     

    If you mean something besides one of these, please explain just what you want to do and ask again.

     

    Nick Gray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to nickgray

    Hi Nick

     

    I would like your help with the selection of a suitable ADC IC for a sensor product I am working on.

     

    I  need to accurately read (16 bit), the analog output of 2, 5 volt hall  effect sensors, the output of which swings from 0.5 to 4.5 volts. The  output of the sensors changes very slowly over time so I don't need  anything fast. I can allow up to about 2 seconds for the conversion. My  device wakes up every hour, reads the sensors, stores the result and  then goes back to sleep.

     

    I'm  using a PIC18F46J11 as my controller which runs at 3.3 volts but I also  have a 5 volt supply on the board to power the 2 hall sensors. I'm  using SPI for interfacing to all the other components so the ADC also  needs to be SPI.

     

    Ideally  the ADC would be able to interface directly to the pic with 3.3v SPI  lines, but the analog side to be able to cope with the 5 volt input of  the sensors.

     

    I know there are various types of ADC but I'm not sure which would be most suitable for this application.

     

    Many thanks, Ben Harker

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • RWM
    RWM over 14 years ago in reply to e14 Contributor

    For example ADS1146 and similar:

    http://www.ti.com/product/ads1146

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hello Nick;
    i'm using a current DAC from analog devices (AD5428) that did not work for me, 
    http://www.analog.com/en/digital-to-analog-converters/da-converters/ad5428/products/product.html
    i select DAC A and i put a load on Iout A but the potential is always zero, i doubt about using an amplifier before connecting the load directly to the IoutA, but i get nothing also, my ad5428 is mounted on a breadboard, and there is time diagram that i follow by using switch,
    thanks in advance

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor

    Hi, Ben,
    A couple of ADCs that should do well in your application with Hall Effect sensors are the ADS1146 and the ADS1255, both from Texas Instruments. I am sure that other suppliers probably have suitable devices as well. However, I think that it would be much less expensive and use less board area if you combined the PIC and ADC in a single package by using one of the CY8C34 family of Programmable System-on-Chip (PSoC) devices from Cypress Semiconductor. Digi-Key shows pricing at less than half of the price they show for the ADS1146 or the ADS1255, in addition to the board area and inventory cost savings. The PSoC devices can operate from supply voltages of 1.7V to 5.5V and have separate analog and digital supplies. The analog supply must be equat to or greater than the digital supply, so operating the digital at 3.3V and the analog at 5V is absolutely no problem.

    The PSoC can be shut down to consume almost no power when not needed. It has an 8051 core, up to 64k of Flash memory, up to 8k of RAM, have SPI, I2C, USB and CAN interfaces, have a Delta Sigma ADC that can be programmed for resolutions of 12 to 20 bits, has timers, counters, PWM, four DACs (voltage or current output), four op-amps, four voltage comparators, sample-and-hold, temperature sensor, programmable analog blocks that can be used to build any number of analog functions, LCD direct drive circuit, CapSense inputs, up/down mixer and just about anything else you need for mixed signal systems. The PSoC Creator software allows you to configure your PSoC just the way you want to without worrying about how to make your custom internal connections. Create your schematic in the PSoC Creator software, then tell the software to configure your device. This is really a fast, easy way to go.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 14 years ago in reply to e14 Contributor
    Without more circuit information it is difficult to know the exact nature of the problem. However, it does seem as though you have a low value resistive load at the output. Considering that the DAC as constructed per Figure 37 of the data sheet, we find that, with a load resistor between the output and some voltage Vterm, the general form of the output is:

     

              Vout = Vterm + [ (Vref – Vterm) * Load R ] /(Rdac + Load R)

     

    where Vterm is as described above, Vref is the DAC reference voltage, Load R is the resistance of your load and Rdac is a nominal 10k, with minimum and maximum of 8k and 12k, as described in the data sheet page 16. The above formula is valid for any value of Vterm between 0V (ground) and the DAC supply voltage.

     

    The probable reasons you are seeing no output include the following:

      Your load resistance is very low, Vterm is 0V and you are measuring the voltage output to ground or output to Vterm
      Vterm is the same as Vref and you are measuring a voltage across the load or the current through the load

     

    Please know that the output voltage of this type of DAC should always be maintained at 0V to get accurate current output, which is why all of the applications in the data sheet show the use of op-amps as current-to-voltage converters.

     

    I suggest that you look at the AD5410 to source a current. It has output current ranges of 0 to 20mA, 0 to 24mA and 4 to 20mA.

     

    If you want to sink a current, I suggest you try the DAC-08. It can sink up to 4mA as long as its output is always at least 5V above its negative supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • YT2095
    YT2095 over 14 years ago

    Hi,

    I`m after an 8 bit A to D converter that will run up to a couple of MHz (but nothing past 4Mhz as it would be a waste).

    I`v already got the Audio A to Ds working well for my computer, but whilst experimenting with them to get it running smoothly, I couldn`t help but wonder what would happen if I attatched my Long-Wire antenna to the input, and surprisingly there Was radio of sorts present.

    needless to say that prompted a few ideas image

    my D to A is near infinate speed as it`s a homemade R2R, so that side is fine, but now I want something that`s a Single channel, 8 bit, really fast conversion time, A to D.

    the voltage rails aren`t a problem as I`v been forced to use a PC PSU for 5V current reasons, so have all the available +/- 12 and 5v stuff ready and waiting.

    I have a ZN425E-8 here, but feel certain there are likely to be Other chips out there that will out perform this, so to save me reading Tons of data sheets, does any particular chip spring to mind?

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 14 years ago in reply to YT2095

    The reason that you picked up radio signals when connecting a long wire antenna to the input is because the ADC had an input bandwidth that could pick up those signals. The sampling action of the ADC then aliased the input signal, converting the RF signal to the audio band as the signal was digitized. You can “tune” in different stations by adjusting the ADC clock frequency. If the ADC input bandwidth is too high, you may sometimes pick up two adjacent radio stations at the same time, although one or both of them may be a little distorted.

     

    Most ADCs today have a serial output. This allows them to be in a much smaller package with fewer pins, reducing their cost. Because you have used the ZN425E8, I am assuming that you want the ease of use of a parallel output ADC and will not consider serial output devices.

     

    There seems to be a gap in ADC speeds between 1 Msps (megasamples per second) and 10 Msps, with not many products available in that range. However, all ADCs can operate a little faster than their specified maximum speed, but their performance may suffer if you try to operate them too much faster than their rated speed. On the other hand, high speed converters may not work well at very low speeds. The general solution to this type of problem is to use a high speed converter and just lot look at all the samples if you do not want data a high rates. For example, If you want data at 2 Msps and can not find a suitable converter at that speed, get a converter specified at 15 or 20 Msps, operate it at 16 Msps and look at every 8th output. This gives you a used data rate of 16 Msps / 8 = 2 Msps. Don’t consider the use of a super fast ADC as a waste. The prices of these things are about the same as slower devices. Here are some suggested ADCs The first is from Analog Devices, the others are from TI / National Semiconductor.

     

    AD7822, 2 Msps
    ADC1173CIMTC/NOPBADC1173CIMTC/NOPB, 15 Msps
    ADC1175, 20 Msps
    ADC08351, 42 Msps
    TLV5535, 35 Msps
    TLC5540, 40 Msps
    ADS830EADS830E, 60 Msps

     

    Nick Gray

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • YT2095
    YT2095 over 14 years ago in reply to nickgray

    That`s fantastic, Thanks!

    currently I`m using a Z80 at 8.192 MHz, but hope to upgrade to a 10 MHz version soon, so any even multiple of that would be great, and who knows, since the entire CPU card is replacable, using a Fast A to D would make it somewhat "Future proof".

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nickgray
    nickgray over 14 years ago in reply to YT2095

    I am happy that I could help. My best to you.

     

    Nick Gray

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>