Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Generally, how are capacitors picked? (Applies to radio, MCU's, digital, analog)
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 320 subscribers
  • Views 624 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Generally, how are capacitors picked? (Applies to radio, MCU's, digital, analog)

Former Member
Former Member over 12 years ago

Sorry if this post is out of line, I'm pretty new to Element14 and I'm not fully oriented with the site yet, meaning I also don't know how many times someone may have asked this same exact question. Please bear with me, though.

 

 

I have been trying to learn about capacitors, and I know that their function is to store energy, but what I don't understand is how this applies to electronic circuits. When it is used in digital circuits, what's the point of putting it where it is? What is the function of caps in radio circuits or small DC motor circuits? I understand a little bit of that, but what bugs me the most is how people know what farad, material and voltage to use!! I looked around all over the internet but I couldn't find an explanation that I could understand. Would someone care to point me toward where I can be enlightened about capacitors, their specific purposes and how to determine what kind?

 

Thank you,

-Tom

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 12 years ago +1
    Hi Thomas, They store a certain amount of charge when you stick a voltage across them, but that is much like describing a glass window as "made of silicon dioxide", which while true at a high level, doesn…
  • johnbeetem
    johnbeetem over 12 years ago +1
    My expertise is digital, where capacitors are mostly used for bypass. The purpose of a bypass capacitor is to keep the supply voltage for an IC constant. The problem with most digital ICs is that the amount…
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    My expertise is digital, where capacitors are mostly used for bypass.  The purpose of a bypass capacitor is to keep the supply voltage for an IC constant.  The problem with most digital ICs is that the amount of current they need can change very rapidly, especially if multiple inputs change at the same time.  For example, if 32 IC outputs all switch from 0V to 3.3V simultaneously, the IC needs to get a bunch of charge from somewhere quickly.  Now it could try to get the charge from the power supply, but it's far enough away that it will take a while to get the current to the IC.  Meanwhile, the IC will pull charge from whatever is near, which causes the supply voltage of the IC to dip.  If it dips too much, it will malfunction.

     

    So what the bypass capacitor does is provide a reservoir of charge right next to the IC power pin so that it provides the charge and minimizes the dip in supply voltage.  To calculate the amount of capacitance you need, you add up the amounts of charge needed to change the outputs.  Usually nobody bothers with the calculations and instead uses 0.1 uF or 0.01 uF capacitors everywhere.  Parts with lots of voltage supply pins (usually called Vcc or Vdd) often tell you in the data sheet what values are recommended, e.g., 0.1 uF ceramic cap for each Vdd plus an additional 10 uF bulk capacitor.  Also, many manufacturers provide a reference design board or schematic and encourage you to copy the capacitor values from that board.

     

    One thing you have to be careful about with capacitors is that they don't just have capacitance: they also have resistance and inductance.  Typically those little 0603 SMT 0.01 uF ceramic caps have very little inductance so they make the best bypass.  However, they can't store much charge so you add larger 10 uF multi-layer ceramic caps to provide a second reservoir.

     

    There are also large electrolytic capacitors.  They're slow, but can store a lot of charge... unless they get too warm and the electrolyte boils off making them useless.  This happens a lot with cheap PC motherboards.

     

    Capacitors also have a working voltage.  You usually want to have twice the highest voltage you expect to get good margin.  Higher voltage capacitors are physically larger, and may have more inductance.

     

    Analog capacitors are a huge subject which I know very little about.  If I need to do something analog, I try to copy the reference design exactly, including the same types and values of capacitors.  I leave the differences between polyester and mica and paper to others.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 12 years ago

    My expertise is digital, where capacitors are mostly used for bypass.  The purpose of a bypass capacitor is to keep the supply voltage for an IC constant.  The problem with most digital ICs is that the amount of current they need can change very rapidly, especially if multiple inputs change at the same time.  For example, if 32 IC outputs all switch from 0V to 3.3V simultaneously, the IC needs to get a bunch of charge from somewhere quickly.  Now it could try to get the charge from the power supply, but it's far enough away that it will take a while to get the current to the IC.  Meanwhile, the IC will pull charge from whatever is near, which causes the supply voltage of the IC to dip.  If it dips too much, it will malfunction.

     

    So what the bypass capacitor does is provide a reservoir of charge right next to the IC power pin so that it provides the charge and minimizes the dip in supply voltage.  To calculate the amount of capacitance you need, you add up the amounts of charge needed to change the outputs.  Usually nobody bothers with the calculations and instead uses 0.1 uF or 0.01 uF capacitors everywhere.  Parts with lots of voltage supply pins (usually called Vcc or Vdd) often tell you in the data sheet what values are recommended, e.g., 0.1 uF ceramic cap for each Vdd plus an additional 10 uF bulk capacitor.  Also, many manufacturers provide a reference design board or schematic and encourage you to copy the capacitor values from that board.

     

    One thing you have to be careful about with capacitors is that they don't just have capacitance: they also have resistance and inductance.  Typically those little 0603 SMT 0.01 uF ceramic caps have very little inductance so they make the best bypass.  However, they can't store much charge so you add larger 10 uF multi-layer ceramic caps to provide a second reservoir.

     

    There are also large electrolytic capacitors.  They're slow, but can store a lot of charge... unless they get too warm and the electrolyte boils off making them useless.  This happens a lot with cheap PC motherboards.

     

    Capacitors also have a working voltage.  You usually want to have twice the highest voltage you expect to get good margin.  Higher voltage capacitors are physically larger, and may have more inductance.

     

    Analog capacitors are a huge subject which I know very little about.  If I need to do something analog, I try to copy the reference design exactly, including the same types and values of capacitors.  I leave the differences between polyester and mica and paper to others.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jvdberg@ieee.org
    jvdberg@ieee.org over 12 years ago in reply to johnbeetem

    In his explanation John Beeten wrote about changing the output Voltage of an integrated circuit. The inputs of the circuits connected  to those outputs are the real need for a decoupling capacitor. The output of a C-mos digital circuit acts as a switch, connecting the output pin to the supply pin or to ground. The load is mostly capacitive. With fast components,  the inductance of the trace to the supply cannot be neglected. A capacitor close to the supply pins of the driving IC will charge the load when the output goes from low ho high. Without this capacitor, the supply Voltage at the driving IC will drop when the polarity of the output changes. If this IC is a gate, this will cause a delay. If this IC is a counter or a memory, the drop in supply Voltage can cause loss of the content stored in the IC. The value of the decoupling capacitor must be more than 10 times the input capacity of the inputs, connected to the outputs of the IC. In general ceramic capacitors with a value of 0.1 μF are used for this purpose. Capacitors also have inductance.  Larger capacitors have larger inductance, as a result if their mechanical size and construction. Properties of a capacitor are not only value and maximum Voltage. Inductance, current rating, ESR(Equivalent Series Resistance), accuracy and stability are sometimes important. For critical decoupling over a wide frequency area, often several capacitors with different type and value are used in parallel. For example  a 0.1 μF ceramic capacitor, a 1 μF polyester capacitor and a 1000 μF electrolytic capacitor. For decoupling purposes, accuracy and stability are not important. In tuned circuits and timing systems they are. In switched mode power supplies some capacitors must handle high currents at the switching frequency. Here a low ESR is important. J. van den Berg