Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help with embedded PI
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 316 subscribers
  • Views 1014 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help with embedded PI

Former Member
Former Member over 12 years ago

I purchased this screen which I told was compatible with the Raspberry pi (model B) after getting it home I soon realized I was ripped off and the seller was long gone!

this is not the seller but it is the same thing (SEEED 2.8" STUDIO Touch Shield 2770070)

http://www.ebay.com/itm/SEEED-2-8-STUDIO-Touch-Shield-2770070-/231017330268?pt=Educational_Toys_US&hash=item35c9b4b65c

 

So thinking i'm stuck with a screen I want to work with a raspberry Pi and some research, Someone from customer service at coocox told me that the Embedded PI would be my answer to having the shield work with the raspberry pi, soon after unboxing the embedded pi I realized I bit off way more then I could chew, not to mention I see no instructions that work online to set up the embedded pi or anyone even trying to get the 2 to work together!

Is there anyone out there with the knowledge I need to get these 2 working, even if i lose something like the touchscreen and can only use it as a screen. Anything to get these working!!!

 

also...

following instructions from this link....

http://www.coocox.org/forum/topic.php?id=3497

I get to this line

gcc –mcpu=cortex-m3 –mthumb –Wall –g –O0 –nostartfiles –I. –c led.c –o led.o

I get this error.... please help

image


  • Sign in to reply
  • Cancel
Parents
  • packetgeek
    packetgeek over 12 years ago

    The first two errors cause me to believe that you used the copy & paste function, from your web browser, into a text editor (it's happened to me a couple (hundred) times).  Take a close look at the lines gcc is complaining about (in your case, it looks like line 14 in led.c).  Sometimes spaces, tabs, double-quotes, or other special characters don't get translated properly (your browser is likely using a ISO-8859 character set, while gcc is expecting flat ASCII).

     

    Hint: \207 is the double-quote, \303 is a tilde (in extended ASCII).  Edit the complained-about file and re-type the characters in the complained-about lines.

     

    Additional reading: http://www.ic.unicamp.br/~stolfi/EXPORT/www/ISO-8859-1-Encoding.html

     

    Hope this helps.

     

    - Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to packetgeek

    No matter how many time i try and change encodeing over to iso-8859-1 and copy the items while viewing the page through midora and then save the file with the encoding for iso-8859-1 i get an error depending where i get the info from or the file saves in which i get a whole boat load of problems with line 14 instead of the couple, why is it that I seem to be the only one having this issue?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 12 years ago in reply to packetgeek

    No matter how many time i try and change encodeing over to iso-8859-1 and copy the items while viewing the page through midora and then save the file with the encoding for iso-8859-1 i get an error depending where i get the info from or the file saves in which i get a whole boat load of problems with line 14 instead of the couple, why is it that I seem to be the only one having this issue?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 12 years ago in reply to Former Member

    Lets just make this really simple before continuing, Do you have a embedded Pi and if so is it the correct card to have to get a 2.8 inch touch shield to work with or do i need something like the alamode?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to Former Member

    Paul,

       I don't know if embedded Pi is what you need, but I think I can help with led.c.

    Assuming you have done the "wget" and "tar" commands to download and unpack the tools,

    you should see a directory "EmbeddedPi", with a subdirectory "example".  In that subdirectory,

    there is led.c, which is exactly the same as the one you were trying to copy/paste.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to Former Member

    Correct i made it myself, thus same error is popping up

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to Former Member

    Paul,

      I'm not sure if I understand you, but you don't need to make led.c yourself,

    you can just use the one that comes with the download, which should compile fine.

    So if you have overwritten led.c with a version that doesn't compile, you should be able

    to delete the EmbeddedPi directory and rerun the tar command to recreate it.