Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Beginner here. Designed a PC Arcade Controller, trying to figure out how to make it work.
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 26 replies
  • Answers 10 answers
  • Subscribers 319 subscribers
  • Views 4837 views
  • Users 0 members are here
  • custom arcade stick
  • teensy
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Beginner here. Designed a PC Arcade Controller, trying to figure out how to make it work.

lyndan
lyndan over 8 years ago

Over the past month or so I've been working on a design for my ideal PC game controller and I'm getting closer to figuring it all out.. And I was wondering if I could run it by the experts here for some help in understanding it all.

Here is the latest version of my design!

image

 

It started as my ideal handheld controller and evolved into an arcade stick. The stick I plan to build has two analog sticks; the leftmost analog stick being Ultimarc's Ultrastik 360 (or U360) and the rightmost being a thumbstick. Also on my design are 12 pushbuttons.

So I've been doing a lot of searching and learning about interfaces and such, but I still feel very in the dark. At this point, I believe it's a Teensy board that I'll need in order to convert these signals to digital so my PC can recognize my arcade controller as a HID. So as far as I understand, the voltage of the Interface I use will need to support the highest voltage of any of my switches, right? The U360 has it's own interface that you can hook to buttons and plug and play, but it only supports eight buttons, and my project incorporates 12 plus an additional analog stick. The U360 can also work in output mode, with 2 of it's eight pins outputting raw analog signal. Also note the stick can output digital 100% signals, but that is not what I want to use. I need the analog signals.

Here's the info on the U360: http://www.ultimarc.com/ultrastik_inst.html

So it shows the pin for powering the U360 is 5V.

Sorry for getting off topic a bit, but it says on the raw analog signals "not used at present".. Does this mean I wouldn't be able to use it? I contacted Andy at Ultimarc and he said it can output raw analog, but he seemed to want me to also buy his I-PAC for my extra buttons, which doesn't support analog, and just make my project act as two separate devices: one for the ultrastick and one for the buttons. That still doesn't let me use my extra analog stick and is too... messy for what I want. I want it to be clean and simple.

 

Anyway, as far as I can understand, I'll need a Teensy board that can power 5V, connect the two raw analog pins of the U360 to the Teensy's analog inputs and it should work fine, right?

Here is the analog stick from Adafruit I plan to pair with it: https://www.adafruit.com/product/512  "Usable with any voltage up to 5V, 2 analog outputs. 1 milliamp draw when used with 5V"

So the two analog sticks would take up four analog pins on a board, right? Then all that's left are the buttons which I can't find the voltage for.. it doesn't say on any of the sites for ordering them. I guess that's not something you have to worry about?

With all this information, if you notice something I'm missing, please let me know.

 

I guess the main questions I'm asking are: is this going to work with this U360 analog stick wired to a Teensy board, and which board should I buy for this project?

Thank you so much for your time.

  • Sign in to reply
  • Cancel

Top Replies

  • jeremy.f.medlin
    jeremy.f.medlin over 8 years ago in reply to lyndan +2 suggested
    Maybe this will help. Arduino is on the left. Each one of those lines represents a wire going somewhere. That +5V which is your power rail will connect to one side of your switch. Then an input pin wire…
  • Sean_Miller
    Sean_Miller over 8 years ago +1 suggested
    Good discussion. Your thumbstick is probably just two mechanically driven potentiometers that center on Vcc/2. So, not counting power and ground, you will consume two pins per stick. Get you the prototyping…
  • jeremy.f.medlin
    jeremy.f.medlin over 8 years ago in reply to lyndan +1 suggested
    Ah okay! Yep, definitely a way to get the joystick info. Hall effect sensors use voltage to determine direction, so you would read the voltage at the pins in order to find the direction and distance the…
Parents
  • jeremy.f.medlin
    0 jeremy.f.medlin over 8 years ago

    An Arduino input at it's very basic level can either sense when voltage is being applied to the pin (true or on) or when there is no voltage on the pin (false or off.)

     

    Without getting too complex, you can either have example 1, which is a joystick connected to its own chip that will output a number that arduino will read (then you can read that value and say okay, that value means forward, left, backward, right etc.) Or you can, example 2, have a joystick where when you push up, it pushes the "up" button and the arduino reads that as a voltage on the pin it's connected to.

     

    In the second example, that joystick is more like a stick connected to a gamepad. Thus you treat each axis like it's two buttons. On the y-axis you have up and down button. On the x-axis you have left and right button. 4 buttons total.

     

    It can get more complicated for sure, and a lot of joysticks don't work as simply as I described, but for your first Arduino project, keep it simple! It's just as important to limit how much you have to do on your first project so that you can at least have something you can test rather than chasing the perfect gamepad setup on your first try!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jeremy.f.medlin
    0 jeremy.f.medlin over 8 years ago

    An Arduino input at it's very basic level can either sense when voltage is being applied to the pin (true or on) or when there is no voltage on the pin (false or off.)

     

    Without getting too complex, you can either have example 1, which is a joystick connected to its own chip that will output a number that arduino will read (then you can read that value and say okay, that value means forward, left, backward, right etc.) Or you can, example 2, have a joystick where when you push up, it pushes the "up" button and the arduino reads that as a voltage on the pin it's connected to.

     

    In the second example, that joystick is more like a stick connected to a gamepad. Thus you treat each axis like it's two buttons. On the y-axis you have up and down button. On the x-axis you have left and right button. 4 buttons total.

     

    It can get more complicated for sure, and a lot of joysticks don't work as simply as I described, but for your first Arduino project, keep it simple! It's just as important to limit how much you have to do on your first project so that you can at least have something you can test rather than chasing the perfect gamepad setup on your first try!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • lyndan
    0 lyndan over 8 years ago in reply to jeremy.f.medlin

    Ohhh no, I'm not using a switch joystick. The Joystick and the thumbstick are both analog.