Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Apollo 13 inside my car !  or how to get lower AMP for a heater ?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 4 answers
  • Subscribers 339 subscribers
  • Views 2024 views
  • Users 0 members are here
  • heater
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Apollo 13 inside my car !  or how to get lower AMP for a heater ?

redgreenblue
redgreenblue over 8 years ago

Hi,

 

I'm having a problem with my car heater, which is completly dead. Yep houston we have a problem, winter is incredibly hard this year.  it's over -20 celcuis outside most of the time. While I wait for better weather to fix the radiator and not freeze my fingers till they droped,  I figure I can use for a while a small heater that could use the lighter switch.

 

The lighter switch is 12 volt @ 15 amps, which give me 180 watts.

I baught a pretty nice ceramic heater that use 120 volt @ 2.1 amps, which need 250 watts.

 

I know with a lower AMP the heater will generate less heat but on the other hand this is way better than having -15 cold inside the car, which would probably feel like being inside apollo 13 with no heat...

 

The heater is pretty simple, it use the AC to power the heater and use DC to power a fan.

The thing I'm not use to is to modify and work with AC.

So here plenty of pics that show how it's build and specs.

 

I'm wondering

 

1- does I need to modify the 3 ways switch  (off, lower, high)

or

2-I need to change the step down transformer on the circuit.

 

 

Thanks guys !

Attachments:
image
image
image
image
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +2 suggested
    Hi redgreenblue, What you are trying to do will be difficult as you are fighting design. Since the heater is designed for 120 VAC @ 2.1 Amps this means that the effective resistance of the heater element…
  • jw0752
    jw0752 over 8 years ago in reply to redgreenblue +1 suggested
    Hi Sorry I didn't look at the pictures before I wrote the first time. I have looked now and so I hopefully won't have a red face this time. The heater actually has (2) heaters that can be hooked up together…
  • jw0752
    jw0752 over 8 years ago +1 suggested
    I will bother you one more time. You mentioned that the heater is at 460 Watts when it is on high in the last posting. At 460 watts the heater would draw about 40 amps from the 12 volts. This would also…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi redgreenblue,

     

    What you are trying to do will be difficult as you are fighting design. Since the heater is designed for 120 VAC @ 2.1 Amps this means that the effective resistance of the heater element is 57 Ohms. If you take a 57 ohm heater and power it with 12 volts we will have a current of 210 mA or just under a quarter of an Amp. This translates to 2.5 watts which will not provide any usable heat. One option would be to use an inverter but unfortunately this would demand at least 25 Amps from your 12 volt system. While you could wire the inverter directly to the battery and use it only when the car is running you would have the expense of an inverter. If you take any of these suggestion make sure you leave some tolerance . For example for a 250 Watt heater you would want an inverter that can handle 300 or 350 Watts as a safety factor. The motor is another question. If it is an induction motor then it must have AC to operate. Some of the better inverters will run an induction motor. You mentioned that the motor was DC. You may want to check and verify this as it is unusual for the manufacturers to put additional expense into these small heaters. If they have AC voltage available for the heater element they likely are also using the same for the motor.

     

    Correction: I was too quick. Your motor is 12 volts. That leaves you with only the problem of how to convert a 120 volt heating element to a 12 volt one.

     

    It may be better to just buy a heater that is designed for 12 volts. Here is a small 600 BTU/Hr 12 volt 15 Amp model that mounts on a visor.

     

    https://www.walmart.com/ip/Roadworthy-THR6000C-12-Volt-Auto-Heater/47651732

     

    In my opinion the cost to use an inverter to run the small AC heater would be impractical. Converting the AC heater for use in the car will be impractical also.  Sorry.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago

    Hi redgreenblue,

     

    What you are trying to do will be difficult as you are fighting design. Since the heater is designed for 120 VAC @ 2.1 Amps this means that the effective resistance of the heater element is 57 Ohms. If you take a 57 ohm heater and power it with 12 volts we will have a current of 210 mA or just under a quarter of an Amp. This translates to 2.5 watts which will not provide any usable heat. One option would be to use an inverter but unfortunately this would demand at least 25 Amps from your 12 volt system. While you could wire the inverter directly to the battery and use it only when the car is running you would have the expense of an inverter. If you take any of these suggestion make sure you leave some tolerance . For example for a 250 Watt heater you would want an inverter that can handle 300 or 350 Watts as a safety factor. The motor is another question. If it is an induction motor then it must have AC to operate. Some of the better inverters will run an induction motor. You mentioned that the motor was DC. You may want to check and verify this as it is unusual for the manufacturers to put additional expense into these small heaters. If they have AC voltage available for the heater element they likely are also using the same for the motor.

     

    Correction: I was too quick. Your motor is 12 volts. That leaves you with only the problem of how to convert a 120 volt heating element to a 12 volt one.

     

    It may be better to just buy a heater that is designed for 12 volts. Here is a small 600 BTU/Hr 12 volt 15 Amp model that mounts on a visor.

     

    https://www.walmart.com/ip/Roadworthy-THR6000C-12-Volt-Auto-Heater/47651732

     

    In my opinion the cost to use an inverter to run the small AC heater would be impractical. Converting the AC heater for use in the car will be impractical also.  Sorry.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer