Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Apollo 13 inside my car !  or how to get lower AMP for a heater ?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 4 answers
  • Subscribers 339 subscribers
  • Views 2023 views
  • Users 0 members are here
  • heater
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Apollo 13 inside my car !  or how to get lower AMP for a heater ?

redgreenblue
redgreenblue over 8 years ago

Hi,

 

I'm having a problem with my car heater, which is completly dead. Yep houston we have a problem, winter is incredibly hard this year.  it's over -20 celcuis outside most of the time. While I wait for better weather to fix the radiator and not freeze my fingers till they droped,  I figure I can use for a while a small heater that could use the lighter switch.

 

The lighter switch is 12 volt @ 15 amps, which give me 180 watts.

I baught a pretty nice ceramic heater that use 120 volt @ 2.1 amps, which need 250 watts.

 

I know with a lower AMP the heater will generate less heat but on the other hand this is way better than having -15 cold inside the car, which would probably feel like being inside apollo 13 with no heat...

 

The heater is pretty simple, it use the AC to power the heater and use DC to power a fan.

The thing I'm not use to is to modify and work with AC.

So here plenty of pics that show how it's build and specs.

 

I'm wondering

 

1- does I need to modify the 3 ways switch  (off, lower, high)

or

2-I need to change the step down transformer on the circuit.

 

 

Thanks guys !

Attachments:
image
image
image
image
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +2 suggested
    Hi redgreenblue, What you are trying to do will be difficult as you are fighting design. Since the heater is designed for 120 VAC @ 2.1 Amps this means that the effective resistance of the heater element…
  • jw0752
    jw0752 over 8 years ago in reply to redgreenblue +1 suggested
    Hi Sorry I didn't look at the pictures before I wrote the first time. I have looked now and so I hopefully won't have a red face this time. The heater actually has (2) heaters that can be hooked up together…
  • jw0752
    jw0752 over 8 years ago +1 suggested
    I will bother you one more time. You mentioned that the heater is at 460 Watts when it is on high in the last posting. At 460 watts the heater would draw about 40 amps from the 12 volts. This would also…
Parents
  • redgreenblue
    0 redgreenblue over 8 years ago

    Hi,

     

    thanks for the advices.

     

    Before buying this heater I actually bought the same 12 volt 15 amp model you send. Unfortunatly that thing does not give heat as it should but the main problem is it stop to work after 2 times, so my opinion is this is not a reliable solution. You can also check on youtube you'll see that most peoples who also baught this kind of small heater didn't have what they expected. I don't want to be rude, it's simply did not convinced me. Been on the problem for a while now.... so I kinda look everywhere for solutions.

     

    I've already got the inverter, it's a 400 watt. I purchased this one becuz it's the closest to 250 watt so the less expensive...for the needs.

    Also I changed the fuse on the lighter port from my car to 30 amp expecting to be letting more AMP to the lighter but it didn't.

     

    Anyway, so I got 2 choices now, according to what you said

    Hook the inverter directly to the car battery or buy another battery that I'll use only for that.

     

    Still I wonder why the 'switch is able to make the heater go from 250 watt at 'LOW' and then to 460 watt at 'HIGH'" I don't know if you seen the pictures but I'm wondering if the switch is responsable for the 'AMP' switch or only the 'voltage ?

     

     

    thanks John !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • redgreenblue
    0 redgreenblue over 8 years ago

    Hi,

     

    thanks for the advices.

     

    Before buying this heater I actually bought the same 12 volt 15 amp model you send. Unfortunatly that thing does not give heat as it should but the main problem is it stop to work after 2 times, so my opinion is this is not a reliable solution. You can also check on youtube you'll see that most peoples who also baught this kind of small heater didn't have what they expected. I don't want to be rude, it's simply did not convinced me. Been on the problem for a while now.... so I kinda look everywhere for solutions.

     

    I've already got the inverter, it's a 400 watt. I purchased this one becuz it's the closest to 250 watt so the less expensive...for the needs.

    Also I changed the fuse on the lighter port from my car to 30 amp expecting to be letting more AMP to the lighter but it didn't.

     

    Anyway, so I got 2 choices now, according to what you said

    Hook the inverter directly to the car battery or buy another battery that I'll use only for that.

     

    Still I wonder why the 'switch is able to make the heater go from 250 watt at 'LOW' and then to 460 watt at 'HIGH'" I don't know if you seen the pictures but I'm wondering if the switch is responsable for the 'AMP' switch or only the 'voltage ?

     

     

    thanks John !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to redgreenblue

    Hi Sorry

     

    I didn't look at the pictures before I wrote the first time. I have looked now and so I hopefully won't have a red face this time. The heater actually has (2) heaters that can be hooked up together to create the high and only one to create the low. From what I can see each heater is designed to handle 120 volts and put out 1/2 of the max output of the heater. Your inverter should work with this unit but it may have to have heavier wires running to the battery. If you put in a bigger fuse but don't change the wires the wires could over heat and start a car fire. Based on your original 250 watt rating of the heater I would expect the inverter to draw 25 Amps when it is running the heater. If you have the inverter inside the car you will at least capture what ever heat it is also producing.

    I am sorry that the visor heater didn't work. unfortunately there is a lot of poor quality stuff out there.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer