Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Apollo 13 inside my car !  or how to get lower AMP for a heater ?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 4 answers
  • Subscribers 339 subscribers
  • Views 2020 views
  • Users 0 members are here
  • heater
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Apollo 13 inside my car !  or how to get lower AMP for a heater ?

redgreenblue
redgreenblue over 8 years ago

Hi,

 

I'm having a problem with my car heater, which is completly dead. Yep houston we have a problem, winter is incredibly hard this year.  it's over -20 celcuis outside most of the time. While I wait for better weather to fix the radiator and not freeze my fingers till they droped,  I figure I can use for a while a small heater that could use the lighter switch.

 

The lighter switch is 12 volt @ 15 amps, which give me 180 watts.

I baught a pretty nice ceramic heater that use 120 volt @ 2.1 amps, which need 250 watts.

 

I know with a lower AMP the heater will generate less heat but on the other hand this is way better than having -15 cold inside the car, which would probably feel like being inside apollo 13 with no heat...

 

The heater is pretty simple, it use the AC to power the heater and use DC to power a fan.

The thing I'm not use to is to modify and work with AC.

So here plenty of pics that show how it's build and specs.

 

I'm wondering

 

1- does I need to modify the 3 ways switch  (off, lower, high)

or

2-I need to change the step down transformer on the circuit.

 

 

Thanks guys !

Attachments:
image
image
image
image
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +2 suggested
    Hi redgreenblue, What you are trying to do will be difficult as you are fighting design. Since the heater is designed for 120 VAC @ 2.1 Amps this means that the effective resistance of the heater element…
  • jw0752
    jw0752 over 8 years ago in reply to redgreenblue +1 suggested
    Hi Sorry I didn't look at the pictures before I wrote the first time. I have looked now and so I hopefully won't have a red face this time. The heater actually has (2) heaters that can be hooked up together…
  • jw0752
    jw0752 over 8 years ago +1 suggested
    I will bother you one more time. You mentioned that the heater is at 460 Watts when it is on high in the last posting. At 460 watts the heater would draw about 40 amps from the 12 volts. This would also…
Parents
  • jw0752
    0 jw0752 over 8 years ago

    I will bother you one more time. You mentioned that the heater is at 460 Watts when it is on high in the last posting. At 460 watts the heater would draw about 40 amps from the 12 volts. This would also exceed the rating of the inverter. If an inverter detects an over load of this nature most will just shut down and refuse to work. You had a question about Amps and volts. In your case you  have 12 volts. Depending on the resistance of the item that you attach to the 12 volts a current will flow. The wattage of a load is determined by the voltage across it multiplied by the current that it is drawing from the power source. The only way to change the current flow from a fixed voltage like 12 volts is to change the resistance of the load. Since the resistance of the ceramic heaters are fixed we don't have anyway to change the load.  You may want to begin with the heater on the low setting so you don't overload the inverter or the vehicles wiring. Also keep in mind that this type of load on a 70 Ah car battery will more or less drain it below start level in an hour or so. Sorry I don't have a more upbeat fix for you.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago

    I will bother you one more time. You mentioned that the heater is at 460 Watts when it is on high in the last posting. At 460 watts the heater would draw about 40 amps from the 12 volts. This would also exceed the rating of the inverter. If an inverter detects an over load of this nature most will just shut down and refuse to work. You had a question about Amps and volts. In your case you  have 12 volts. Depending on the resistance of the item that you attach to the 12 volts a current will flow. The wattage of a load is determined by the voltage across it multiplied by the current that it is drawing from the power source. The only way to change the current flow from a fixed voltage like 12 volts is to change the resistance of the load. Since the resistance of the ceramic heaters are fixed we don't have anyway to change the load.  You may want to begin with the heater on the low setting so you don't overload the inverter or the vehicles wiring. Also keep in mind that this type of load on a 70 Ah car battery will more or less drain it below start level in an hour or so. Sorry I don't have a more upbeat fix for you.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer