Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the correct replacement?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 8 answers
  • Subscribers 340 subscribers
  • Views 4398 views
  • Users 0 members are here
  • thermal switch
  • dehydrator
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the correct replacement?

hafcanadian
hafcanadian over 7 years ago

The thermal fuse on our old Magic Aire II dehydrator failed.  I ordered and installed what appeared to be a correct replacement, and did some soldering to reinforce and repair some connections on the heater board.  All original connections were rivets, so I don't know if solder will survive but am trying to save the device.

 

Everything seems to work except there's still no heat.  The one bad component yet seems to be a switch of some sort built into the heater circuit.  It is rectangular black, riveted to the board (asbestos(?) ring) with heat bands contacting the rivets, with brass connection arms in between, and a copper tongue inside that may have points on it, it's too hard to see very well inside.  Another dark blade is loose inside and I cannot tell how it fits, nor maneuver it very easily.  The switch is one and a quarter inch long overall and a quarter inch wide.

 

Is it a thermal switch of some sort, to keep the heater from getting too hot?  Perhaps it's failure caused the thermal fuse to fail?  After the time and effort so far, I'd like to see if I can get a replacement switch and probably a couple new rivets for it, since I'll try to drill out the old ones without destroying the fragile asbestos(?) board.  Or has my resurrection effort all been a waste of time?  There's a lot of extra trays and other accessories we've bought over the years for it... not crazy about tossing it all if I don't have to.  A new one is $120 and just the base unit is $90.

 

Thanks for any advice.

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • hafcanadian
    hafcanadian over 7 years ago in reply to jw0752 +4 suggested
    Note where I had to notch out the end so it straddled the rivet hole and screw, and add a wide washer for the lower screw to effectively clamp the cutout. This particular device was 2mm shorter than the…
  • jw0752
    jw0752 over 7 years ago +3 suggested
    Hi Joel, I could not get your pictures to load. Try replying to your own post and use the picture icon on the tool bar to insert your pictures into the text. In my experience the thermal fuses blow for…
  • jw0752
    jw0752 over 7 years ago in reply to hafcanadian +3 suggested
    Hi Joel, The pictured switch is the Auto Setting thermal cut out. It will open up if the element gets too hot due to lack of air flow and automatically close again when it cools down.. It should test with…
Parents
  • jw0752
    0 jw0752 over 7 years ago

    Hi Joel,

     

    I could not get your pictures to load. Try replying to your own post and use the picture icon on the tool bar to insert your pictures into the text. In my experience the thermal fuses blow for two reasons. First of all if there is an over heat situation and the second is if their leads do not have a good mechanical connection (Rivets) A bad connection produces heat and this travels up the wires and fuses the thermal link. Typically there are three ways to break the circuit. #1 is the thermostat which controls the temperature. The back up for this is usually a self resetting thermal cut out and the final protection is a thermal fuse. If the part you describe is the thermal cut out its failure could have caused the unit to over heat and take out the thermal fuse. Soldering will not usually work as the heat will eventually cause the solder to crystallize and make a bad connection. It is probably too late but the best way is to cut the original thermal fuse leads and use metal crimp splices to hook the new thermal fuse to the old leads. I look forward to seeing your pictures. While I have never worked on a dehydrator it sounds very similar to some of the dental lab heaters and sterilizers that I used to work on.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 7 years ago

    Hi Joel,

     

    I could not get your pictures to load. Try replying to your own post and use the picture icon on the tool bar to insert your pictures into the text. In my experience the thermal fuses blow for two reasons. First of all if there is an over heat situation and the second is if their leads do not have a good mechanical connection (Rivets) A bad connection produces heat and this travels up the wires and fuses the thermal link. Typically there are three ways to break the circuit. #1 is the thermostat which controls the temperature. The back up for this is usually a self resetting thermal cut out and the final protection is a thermal fuse. If the part you describe is the thermal cut out its failure could have caused the unit to over heat and take out the thermal fuse. Soldering will not usually work as the heat will eventually cause the solder to crystallize and make a bad connection. It is probably too late but the best way is to cut the original thermal fuse leads and use metal crimp splices to hook the new thermal fuse to the old leads. I look forward to seeing your pictures. While I have never worked on a dehydrator it sounds very similar to some of the dental lab heaters and sterilizers that I used to work on.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer