Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum What is the correct replacement?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 8 answers
  • Subscribers 340 subscribers
  • Views 4413 views
  • Users 0 members are here
  • thermal switch
  • dehydrator
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

What is the correct replacement?

hafcanadian
hafcanadian over 7 years ago

The thermal fuse on our old Magic Aire II dehydrator failed.  I ordered and installed what appeared to be a correct replacement, and did some soldering to reinforce and repair some connections on the heater board.  All original connections were rivets, so I don't know if solder will survive but am trying to save the device.

 

Everything seems to work except there's still no heat.  The one bad component yet seems to be a switch of some sort built into the heater circuit.  It is rectangular black, riveted to the board (asbestos(?) ring) with heat bands contacting the rivets, with brass connection arms in between, and a copper tongue inside that may have points on it, it's too hard to see very well inside.  Another dark blade is loose inside and I cannot tell how it fits, nor maneuver it very easily.  The switch is one and a quarter inch long overall and a quarter inch wide.

 

Is it a thermal switch of some sort, to keep the heater from getting too hot?  Perhaps it's failure caused the thermal fuse to fail?  After the time and effort so far, I'd like to see if I can get a replacement switch and probably a couple new rivets for it, since I'll try to drill out the old ones without destroying the fragile asbestos(?) board.  Or has my resurrection effort all been a waste of time?  There's a lot of extra trays and other accessories we've bought over the years for it... not crazy about tossing it all if I don't have to.  A new one is $120 and just the base unit is $90.

 

Thanks for any advice.

 

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • hafcanadian
    hafcanadian over 7 years ago in reply to jw0752 +4 suggested
    Note where I had to notch out the end so it straddled the rivet hole and screw, and add a wide washer for the lower screw to effectively clamp the cutout. This particular device was 2mm shorter than the…
  • jw0752
    jw0752 over 7 years ago +3 suggested
    Hi Joel, I could not get your pictures to load. Try replying to your own post and use the picture icon on the tool bar to insert your pictures into the text. In my experience the thermal fuses blow for…
  • jw0752
    jw0752 over 7 years ago in reply to hafcanadian +3 suggested
    Hi Joel, The pictured switch is the Auto Setting thermal cut out. It will open up if the element gets too hot due to lack of air flow and automatically close again when it cools down.. It should test with…
Parents
  • jw0752
    0 jw0752 over 7 years ago

    Hi Joel,

    I found this switch on ebay that cuts out at 105C. I do not know if this is going to work but it is the closest replacement that I have seen. If you have to replace rivets do it with screws, washers and nuts as this will make a good connection that is not susceptible to heat failure like solder is.

     

    https://www.ebay.com/itm/Bimetalic-Switch-Thermostat-Over-Temperature-Switch-221-Deg-F-in-USA/172517131295?hash=item282ad2841f:g:bkIAAOSwnHZYl5Px

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hafcanadian
    0 hafcanadian over 7 years ago in reply to jw0752

    Thanks for the link, John.  I posted my previous notes before reading your last.  It looks like a likely candidate, and obviously my idea of screws in lieu of messing with rivets was not a bad one.

     

    Come to think of it, why not clockwise loop the power wire ends and thermal fuse wire ends and tuck them under brass screw heads in the other riveted spots, as opposed to crimp connectors?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 7 years ago in reply to hafcanadian

    Hi Joel,

    ECG/NTE used to sell the proper crimps with the thermal fuses. If you do use a crimp make sure that it is a bare one so you don't get melted plastic. I like your small brass screw approach.  Good Luck.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hafcanadian
    0 hafcanadian over 7 years ago in reply to jw0752

    Update.

    A big thank you to John for the link.  I received the “thermostat” and installed it tonight, and what to my wondering eyes should happen but... it worked!  At least for the several minutes I had the unit running.  I’m not sure it’ll hold up in the long run and didn’t have the unit totally reassembled, but after an afternoon spent at the hardware store getting the correct screws, nuts, and washers to mount the device with, I was elated to see at least the thing actually working about as it used to.  I’m not sure that it heats up as much, but then it’s not reassembled and enclosed yet, and the “thermostat” didn’t break contact and kept current flowing through the coils.

     

    In this case I simply used a Dremel to cut off the old thermostat/switch/cutout, leaving the rivets intact.  By using washers to make good contact with the remaining rivet heads and brass ends of the old cutout, I planned to simply use small machine screws, washers, and nuts to clamp down the new cutout.

     

    The Klixon TH21 I had my eye on had the same dimensions as the original and would’ve fit, whereas this one turned out to be just a little short (ironically, it’s stamped on the back as a Klixon product).  I nipped off the very extreme of one end so it at least straddled the screw hole, inserted a larger washer to span the compromised area, and another washer atop of it appropriate to the screw size;  the “miniature” class screws and such were size #1 (~1/16”) round head a quarter inch long.  I was hoping for brass, but they only had stainless.  Hey, whatever works at this point.  I’m not sure I trust the unit to leave it dehydrating overnight, thermal fuse or not, but at least it can be used while monitored during the day and isn’t a bunch of money in the garbage can.

     

    If anyone would like to see a photo of the final fix, I’ll be happy to supply it here.

     

    Much obliged!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 7 years ago in reply to hafcanadian

    Hi Joel,

     

    I am very happy that you were able to fix it. I would be glad to see a final fix photo.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 7 years ago in reply to hafcanadian

    Hi Joel,

     

    I am very happy that you were able to fix it. I would be glad to see a final fix photo.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • hafcanadian
    0 hafcanadian over 7 years ago in reply to jw0752

    imageimageimageimageimage

    Note where I had to notch out the end so it straddled the rivet hole and screw, and add a wide washer for the lower screw to effectively clamp the cutout.  This particular device was 2mm shorter than the original and the other possible replacement (Klixon TH21), so notching was a way to make it reach and make good contact.

     

    Strange... after I’d cut off the old cutout I happened to look closely at it, and now it’s contact point is sitting in a normally closed position.  Don’t know what changed just from me removing it, but if it was installed now it would work as designed.  Weird.  Slight lift with a fingernail and the contact disengages the bottom brass, then springs right back like it probably did during an overheat/cool cycle.

     

    Also on the underside of the old switch was stamped “PEPI M.  42”.  I think that is Portage Electric Products Inc.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 7 years ago in reply to hafcanadian

    It looks like an excellent job. Hopefully the temperature of the new thermostat will be appropriate.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 14rhb
    0 14rhb over 7 years ago in reply to hafcanadian

    Joel,

     

    Well done (and to jw0752 for helping you) - it is always good to see something repaired rather than get scrapped. Looks like you've made a professional job of it as well.

     

    Rod