Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Low-level to High-level signal
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 314 subscribers
  • Views 1573 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Low-level to High-level signal

jimmyhu78
jimmyhu78 over 7 years ago

Hi all.

 

I tried to find the magic component on all famous retaillers but no way.

I'm looking for a solution which able to switching between a 28Vcc (state 1) and an open output (state 0), by a command signal of 200mV

 

When U>200mV is applied, that energize a relay which permit to supplied a 28V or let a 28V goes through itself.

When U<200mv is applied, relay is OFF, output is open.

 

I think it's possible to amplify the source signal before be able to command a relay.

But i'm completly lost in datasheets.

 

Does someone is able to help me for finfing an efficient solution?

 

Many thanks.

 

 

Jimmy

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 7 years ago +3 suggested
    You could do this with a 30V rail-to-rail op-amp like an OPA171 or an LT1637. If the current needs to be higher than the op-amp can supply, you can use a FET on the output.
  • dougw
    dougw over 7 years ago in reply to jimmyhu78 +3 suggested
    Diagram:
  • jw0752
    jw0752 over 7 years ago +2 suggested
    Hi Jimmy, I think a comparator circuit like I just used in my recent Interface Build might work. You will have to use a better comparator than the LM 393 or you could use a rail to rail op amp. Don't forget…
Parents
  • jimmyhu78
    0 jimmyhu78 over 7 years ago

    Hi Douglas and John.

     

    Thanks for your answers.

    If i understand well, i should use the component recommanded by Douglas, but could be safer with a Hysteresis application (as John mentionned).

     

    imageimage

    Do you think i can obtained good results with one of these kind of configurations?

     

    Thx

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 7 years ago in reply to jimmyhu78

    Diagram:

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • geralds
    0 geralds over 7 years ago in reply to dougw

    High Douglas,

     

    may be it works down closed to 0,xxx V. But normally comparators like this are working down above 1V, or 1.2V with its hysteresis.

    Here a negative supply voltage may help a bit more, so the V- supply pin would get to -1.2V supply voltage for this comparator.

    We have do not to forget  too the GND noise.

     

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • geralds
    0 geralds over 7 years ago in reply to dougw

    High Douglas,

     

    may be it works down closed to 0,xxx V. But normally comparators like this are working down above 1V, or 1.2V with its hysteresis.

    Here a negative supply voltage may help a bit more, so the V- supply pin would get to -1.2V supply voltage for this comparator.

    We have do not to forget  too the GND noise.

     

    Gerald

    ---

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer