I am a self taught pin crimper. Sounds like a personal problem, I know.
I have a crimper tool that looks like this:
I use it to crimp pins for proto board soldered wire-to-board connectors that look like this:
At first, I was unhappy with the results due to the following results:
- The wires would stab through the hole blocking the male end
- I’d lose the pin from it falling off the cable before I could crimp it
- the pins are hard to seat into the connector
- the pins back out of the connector when connected to the male end
- the wire breaks off at the base of the pin
- the male pins would not want to stab into the female after everything was crimped and ready
<EDIT: See this post below for the crowd improved troubleshooting guide: >
Here's how I adjusted my approach:
| Issue | Solution |
|---|---|
| Wires stabbing through the hole | I bend the wires back over the insulation |
| Dropping the pin | I’d pre crimp the bottom with just my fingers to hold it in place. |
| Hard to seat | After crimping the bottom of the crimp pin to the cable sheathing, I take a small plier to shape the female tip to remove any parts sticking out impeding entry into the plastic connector housing. |
| pins back out | After adjusting the pin shape in the previous step, I pull up the tab that will catch inside the connector to prevent it from backing out. |
| the wire breaks off | I stopped using jumper cables as the donor wire. Instead, I use ribbon cable. |
| Male pins not fitting | I use a single jumper male pin to pre stab in the female pins I just inserted into the connector to open it back up. |
I now get reasonable results, but what bothers me is that I have to do all this. I would think I could just crimp and insert and be done.
So, my question is, what are the community members experiences, steps, and tricks for using crimp pins?
Thanks,
Sean