Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using Heatsink to cool large volume of water
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 16 answers
  • Subscribers 338 subscribers
  • Views 13558 views
  • Users 0 members are here
  • heatsink
  • copper pipe
  • water
  • aluminium
  • radiator
  • cooling
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using Heatsink to cool large volume of water

sporkeh
sporkeh over 5 years ago

Hi everybody,

 

I'm currently trying to upgrade a cold water tank at my work.

We use this to cool down hot wax parts quickly.

Currently, its a plastic box with a large household radiator thrown in and copper pipes connecting to a constant flowing cold water source.

 

It works, however, a household radiator wasn't meant to be submerged and is quickly turning into a pile of rust.

 

So I'm looking into a variety of things, including making a whole new one. (new one will have insulated sides and top to try and keep the temp)

- one suggestion I had was to build a radiator into the skin of the tank, and then put some insulation on the outside, all of which would be a massive faf to make, and I'm not a radiator designer/engineer so I currently have no idea if that would work ether.

 

This tank is ~800 x 600 x 300mm and should hold ~140 liters of water, the current radiator is around 2200 BTU.

The room is kept at a constant 21 degrees, and the water comes in at about ~10 degrees iirc.

 

I've found a heatsink on farnell and wondered if it or something similar could be used (considering its just ally and copper, I could probably get a custom sized one made), but I have no idea if it would be suitable for this application.

 

I was originally thinking of just having copper pipe run around the inside of the tank, but a colleague mentioned that they tried to do a similar thing for a project at home and found that the copper pipes didn't do too much.

I'm not sure if there is something with the aluminium block along with the copper pipe that might work better, or if I can even get enough copper pipe in there for that kind of volume.

 

Is there anyone with a better understanding of thermal conductivity or any experience that could give me some advice?

Or maybe someone who has a spare one of these who might be able to do a simple/rough test? image

 

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago in reply to sporkeh +5 suggested
    Hi Henri, Here are the physics of your system. Thermal energy (heat) moves from warmer to colder. It can do this is three ways (1) by conduction where a hot area makes physical contact with a colder area…
  • dougw
    dougw over 5 years ago +4 suggested
    Those radiators are designed for liquid-to-air heat transfer where you need a large surface area on the air side. For liquid-to-liquid heat transfer I would expect simple copper tubing provides about the…
  • jw0752
    jw0752 over 5 years ago +4 suggested
    One other idea is to put a metal box within an outer box. Cold water is pumped into the outer box and surrounds the inner box. If you can elongate the shape of the box you will increase outer surface area…
Parents
  • colporteur
    0 colporteur over 5 years ago

    Great coffee break topic for discussion.

     

    At first I thought of the wine chillers used at the liquor store. The bottle is submersed and five minutes later the wine is cooled before you take it to the cash. Then my thoughts jumped to thermonuclear reactor coolers. I don't suppose you have the budget for that? I then settled on the swimming pool solar panels, except instead of using them to capture heat your are using them to release heat.

     

    Large surface area and temperature difference are the two factors I'm considering. The solar panels for pools are designed to take the feed pipe water into capillary like lines for the water to run and collect heat then back to a larger line for distribution back to the pool. If you roll the panel up, ensuring that there is separation between the layers in in the roll and submerse it in a water reservoir that has water moving through it, you have the start of a design.

     

    The solar panel won't give you a corrosion issue it is a form of rubber or plastic. It is designed to be under pressure from a pool pump. You would need to move the water through the panel and also move the water around in the tank.

     

    If you ever watch the moonshine television shows, you see the good old boys setting their copper pipe in a flowing stream. Got a stream to run over your solar panel. Now I don't know if it transfers heat in a liquid to the same level it does from the sun in air.

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sporkeh
    0 sporkeh over 5 years ago in reply to colporteur

    Thanks Everybody for your input;

     

    For the moment, lets forget about circulation in the tank, and lets focus on the cool stuff, I can always add circulation later on if its needed.

     

    For reference, I've included a picture of our current tank (this has been through multiple modifications since the initial design, originally we were going to have a freezer until we found that water was much more efficient)

    You can see the current radiator thats going rusty, and on top is one of the most used setters which will hold a wax component.

    image

    One thing to note, is that this particular one (and others) uses a gantry crane to assist lifting in and out the tank (H&S rules :/ )

    The plan is to replace this with a 2 hydraulic lifts for each half (we have all the bits, just waiting for our maintenance team to catch up, its only been on their list for about a year image )

     

    A bit more background; one of our most produced parts only takes up about half a tank, we inject the component, put it in its setter, then put it in the hot water tank to soften it up for 2-3 minutes(HWT to the left on the image under the lid, cant see much), and then take it out, shake off the excess water, and then put it in cold water for another 2-3 minutes to solidify the shape of the setter, and then leave it to dry.

    The CWT is checked before anything is put in to ensure the temp is below 16 degrees.

    When we are running this particular part, we would be doing 4 of these at once, 1 in each half of each tank, meaning the platforms would be going up and down every couple of minutes massively disturbing the water quite often.

     

    Currently, using the gantry crane, I wouldn't like piping go around the inside of the tank as it would probably get damaged unless I put a fence in between to protect them. However, once we have the lifts and platforms, it would make it much safer to have piping around. so it may be that this is this best option, just need to work out how much I'd need, I'm sure there is a formula somewhere for surface area per water volume... at least this would be a fairly cheap option we can test out right away rather than going all out on a new tank...

     

    Got it, I'll keep aluminium and stainless separate.

     

    Sean.... ermmm... what? wine chillers in a liquor store? I think I live in the wrong area....we have to wait until we get home and use our own fridge/freezer like peasants...please share with me what I'm missing out on!

    As for a thermonuclear reactor, I mean, how much does a black mask, some rubber gloves and a large van cost?

    However, your swimming pool solar panel idea intrigues me, my mum used to have a pool, and we used one of these solar covers, kinda looked like bubblewrap, I believe the idea was that the sun heated up these bubbles and released the energy into the water, this was really good at heating up the top inch of water, however, the rest of the pool was still freezing, and I'm pretty sure its not quite what you're suggesting...

    Ether way, as much as I like this idea, I think something rolled up as you suggest would probably take up too much room and require quite a lot of movement in a specific direction to work efficiently.

    Although I'll think about it over the weekend and see if it inspires anything.

     

    I think I may have seen the odd episode of the moonshine boys, I'll have to watch a few more over the weekend, maybe I can have two uses for this tank...

     

    Ultimately, I think the best starting point would be to have copper piping running around the inside, its cheap and quick, and less likely to get me arrested...

    If this isn't enough, then I think I'll go towards a new tank with cold water circulating around the walls and base.

    Would it be worth, going back to the idea of water in the walls, to have copper bars in the wall, going through the inner wall, and poking out into the actual tank, so that the cold water has direct contact with both the cold and warmer water.

    It might have to be a lot of bars all around, but if it works, then its not silly...

    image

    If all of this fails to be enough, I'll be interviewing for getaway drivers.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • colporteur
    0 colporteur over 5 years ago in reply to sporkeh

    I found whiteboard exercises are so enlightening and so much cheaper than prototypes.

     

    The liquor store wine chiller is a drum rather like the old wringer washers that had the roller assembly across the top. The chiller is full of water. The attendant puts the bottle in the middle of the opening and closes the clear lid to start a rotation of water creating a whorl pool effect. It was explained that the water on the outside is constantly moving taking away heat from the bottle. I have used them and they work. Now I only drank the wine in the car once, on the way home just to test the temperature.

     

    I understand there might be some used piping real cheap at these locations Fukushima Daiichi, Chernobyl or Three Mile Island. Carrying it away might be a bit of a issue.

     

    The solar mats come in about 4 X 4 foot lengths. This picture shows a ten foot roll. Rolled up in the box the mat is not that big. Laying it on its side would require a pool slightly larger than four feet. Rolling it up would give you a fairly small circumference, so the depth of the pool of water could be less than 3ft. The key is the water moving across the mat. The need to move the water become important or it will not cool in the middle.

    image

     

    Good luck on your project. I would be interested to see you final version.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 5 years ago in reply to sporkeh

    I found whiteboard exercises are so enlightening and so much cheaper than prototypes.

     

    The liquor store wine chiller is a drum rather like the old wringer washers that had the roller assembly across the top. The chiller is full of water. The attendant puts the bottle in the middle of the opening and closes the clear lid to start a rotation of water creating a whorl pool effect. It was explained that the water on the outside is constantly moving taking away heat from the bottle. I have used them and they work. Now I only drank the wine in the car once, on the way home just to test the temperature.

     

    I understand there might be some used piping real cheap at these locations Fukushima Daiichi, Chernobyl or Three Mile Island. Carrying it away might be a bit of a issue.

     

    The solar mats come in about 4 X 4 foot lengths. This picture shows a ten foot roll. Rolled up in the box the mat is not that big. Laying it on its side would require a pool slightly larger than four feet. Rolling it up would give you a fairly small circumference, so the depth of the pool of water could be less than 3ft. The key is the water moving across the mat. The need to move the water become important or it will not cool in the middle.

    image

     

    Good luck on your project. I would be interested to see you final version.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer