Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Using Heatsink to cool large volume of water
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 16 answers
  • Subscribers 338 subscribers
  • Views 13559 views
  • Users 0 members are here
  • heatsink
  • copper pipe
  • water
  • aluminium
  • radiator
  • cooling
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Using Heatsink to cool large volume of water

sporkeh
sporkeh over 5 years ago

Hi everybody,

 

I'm currently trying to upgrade a cold water tank at my work.

We use this to cool down hot wax parts quickly.

Currently, its a plastic box with a large household radiator thrown in and copper pipes connecting to a constant flowing cold water source.

 

It works, however, a household radiator wasn't meant to be submerged and is quickly turning into a pile of rust.

 

So I'm looking into a variety of things, including making a whole new one. (new one will have insulated sides and top to try and keep the temp)

- one suggestion I had was to build a radiator into the skin of the tank, and then put some insulation on the outside, all of which would be a massive faf to make, and I'm not a radiator designer/engineer so I currently have no idea if that would work ether.

 

This tank is ~800 x 600 x 300mm and should hold ~140 liters of water, the current radiator is around 2200 BTU.

The room is kept at a constant 21 degrees, and the water comes in at about ~10 degrees iirc.

 

I've found a heatsink on farnell and wondered if it or something similar could be used (considering its just ally and copper, I could probably get a custom sized one made), but I have no idea if it would be suitable for this application.

 

I was originally thinking of just having copper pipe run around the inside of the tank, but a colleague mentioned that they tried to do a similar thing for a project at home and found that the copper pipes didn't do too much.

I'm not sure if there is something with the aluminium block along with the copper pipe that might work better, or if I can even get enough copper pipe in there for that kind of volume.

 

Is there anyone with a better understanding of thermal conductivity or any experience that could give me some advice?

Or maybe someone who has a spare one of these who might be able to do a simple/rough test? image

 

 

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 5 years ago in reply to sporkeh +5 suggested
    Hi Henri, Here are the physics of your system. Thermal energy (heat) moves from warmer to colder. It can do this is three ways (1) by conduction where a hot area makes physical contact with a colder area…
  • dougw
    dougw over 5 years ago +4 suggested
    Those radiators are designed for liquid-to-air heat transfer where you need a large surface area on the air side. For liquid-to-liquid heat transfer I would expect simple copper tubing provides about the…
  • jw0752
    jw0752 over 5 years ago +4 suggested
    One other idea is to put a metal box within an outer box. Cold water is pumped into the outer box and surrounds the inner box. If you can elongate the shape of the box you will increase outer surface area…
Parents
  • beacon_dave
    0 beacon_dave over 5 years ago

    "... It works, however, a household radiator wasn't meant to be submerged and is quickly turning into a pile of rust. ..."

     

    If it works as is and the only real problem is the exterior rust, then perhaps sandblast the original enamel paint off the radiator and replace it with an epoxy-based marine paint ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 5 years ago

    "... It works, however, a household radiator wasn't meant to be submerged and is quickly turning into a pile of rust. ..."

     

    If it works as is and the only real problem is the exterior rust, then perhaps sandblast the original enamel paint off the radiator and replace it with an epoxy-based marine paint ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • sporkeh
    0 sporkeh over 5 years ago in reply to beacon_dave

    I've had a meeting with others involved and I think what we're going to do is try the copper piping first, as we can get some from across the road (which saves a trip to a nuclear facility, although I would still like to go...), and if that isn't sufficient enough, we'll try an aluminium radiator in there.

     

    The problem with the current steel radiator is that yes it rusts, but its also quite thick and so takes up a lot of room, whereas we can get a reasonably thin aluminium one rather than going through the effort of sealing this one off.

     

    I like the sound of the wine chillers, not sure how useful the concept is for this project, but I still like it image

     

    I will try and get some testing done over the next couple of weeks, I'll post updates if I remember, but I've also got quite a lot of actual work to get on with this week image

     

    Thanks for everyones input so far! its all been very interesting and helpful.

     

    I don't suppose anyone knows of a formula or online calculator I can use that looks at the heat transfer of copper piping?

    I will google this myself when I get a chance, but on the off chance that someone knows of a decent one, it would save me some googletime image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • colporteur
    0 colporteur over 5 years ago in reply to sporkeh

    Good luck. The next time I am at the liquor store I will snap a pick of the wine chiller. Maybe get a model number and send them along. Good luck in your design.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Bigmacpie
    0 Bigmacpie over 3 years ago in reply to sporkeh

    Did you get the formula or find a calculator that did the heat transfer calculations?