Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for help on how to wire a relay
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 302 subscribers
  • Views 1326 views
  • Users 0 members are here
  • wiring
  • relay
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for help on how to wire a relay

bdohrn
bdohrn over 4 years ago

Below is a picture of a relay I purchased.  I want to use it to turn my inverter (connected to a 12v battery, provides 220 to a pump) on and off.

 

Unless you have a better idea, I think I should wire it into the inverter on/off switch somehow, but I am not sure what to wire to which terminal.

Secondly there are two terminals on the back of the inverter for the 12V battery cables. I assume that I should connect those to the two wires on the clip marked 12v. Do I just do that via some extra wires connecting from one to the other?

 

Help with how to wire this super appreciated. 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +3 suggested
    This is a simple way to implement the hysteresis function you want. This circuit takes a higher battery voltage to turn power on to the inverter than to turn power off. It is not clear at what voltage…
  • shabaz
    shabaz over 4 years ago +2 suggested
    Hi Beatrice, The simplest way in this situation is to just apply 12V DC to the red and black wires, and you'll hear a click. You can use a multimeter set to 'ohms' or to 'continuity' and 'buzz out' the…
  • colporteur
    colporteur over 4 years ago in reply to colporteur +2
    It has been a while since I dabbled in electronics drafting so I figured why not napkin out a drawing for you. Here is one way the relay module could be wired. The contacts inside the box are controlled…
Parents
  • colporteur
    0 colporteur over 4 years ago

    Rather difficult to identify operation of the relay from the picture.

     

    Can you translate the details from the relay and/or a name for the module?

     

    Typically you would have a normally open (N.O.), common (COM), normally close (N.C.) contacts. C is connected to N.C. without power. When the relay is triggered C is then connected to N.O.

     

    You only have two wire connections. The relay is either going to make the circuit or break the circuit.

     

    The relay could be configured to switch the Input side power to the output side power when the relay is engaged.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • colporteur
    0 colporteur over 4 years ago

    Rather difficult to identify operation of the relay from the picture.

     

    Can you translate the details from the relay and/or a name for the module?

     

    Typically you would have a normally open (N.O.), common (COM), normally close (N.C.) contacts. C is connected to N.C. without power. When the relay is triggered C is then connected to N.O.

     

    You only have two wire connections. The relay is either going to make the circuit or break the circuit.

     

    The relay could be configured to switch the Input side power to the output side power when the relay is engaged.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • colporteur
    0 colporteur over 4 years ago in reply to colporteur

    image

     

    It has been a while since I dabbled in electronics drafting so I figured why not napkin out a drawing for you. Here is one way the relay module could be wired. The contacts inside the box are controlled (i.e. move) when the 12V is applied to the module.

     

    As shabaz has suggested a multi-meter using the OHMS function to measure resistance will enable you to determine the contact mapping. You may discover A actually connects to D and not C when the relay is engaged.

     

    You may also discover that C & D are connected to the N.C. side of the relay and the circuit actually breaks contact between input and output when 12V is applied to the module.

     

    All of this can be discovered with the multi-meter and a supply to trigger the relay.

     

    You indicate a 220V pump. Check the rating on the relay contacts. They can be rated for 220V but typically 120V is more common. If the rating is lower you run the risk of burning the contacts when the relay is engaged, Burning to the point they may weld or not work because of the current draw.

    • Cancel
    • Vote Up +2 Vote Down