Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Looking for help on how to wire a relay
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 302 subscribers
  • Views 1328 views
  • Users 0 members are here
  • wiring
  • relay
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Looking for help on how to wire a relay

bdohrn
bdohrn over 4 years ago

Below is a picture of a relay I purchased.  I want to use it to turn my inverter (connected to a 12v battery, provides 220 to a pump) on and off.

 

Unless you have a better idea, I think I should wire it into the inverter on/off switch somehow, but I am not sure what to wire to which terminal.

Secondly there are two terminals on the back of the inverter for the 12V battery cables. I assume that I should connect those to the two wires on the clip marked 12v. Do I just do that via some extra wires connecting from one to the other?

 

Help with how to wire this super appreciated. 

image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +3 suggested
    This is a simple way to implement the hysteresis function you want. This circuit takes a higher battery voltage to turn power on to the inverter than to turn power off. It is not clear at what voltage…
  • shabaz
    shabaz over 4 years ago +2 suggested
    Hi Beatrice, The simplest way in this situation is to just apply 12V DC to the red and black wires, and you'll hear a click. You can use a multimeter set to 'ohms' or to 'continuity' and 'buzz out' the…
  • colporteur
    colporteur over 4 years ago in reply to colporteur +2
    It has been a while since I dabbled in electronics drafting so I figured why not napkin out a drawing for you. Here is one way the relay module could be wired. The contacts inside the box are controlled…
Parents
  • dougw
    0 dougw over 4 years ago

    This is a simple way to implement the hysteresis function you want.

    This circuit takes a higher battery voltage to turn power on to the inverter than to turn power off.

    It is not clear at what voltage the coil turns off - you will need to experiment.

    If the circuit is turning off at too low of a voltage, add more diodes in series with D4 until it turns off at the voltage you want.

    You will need to figure out which screw terminal to connect to the inverter - it will be C or D in colporteur diagram above.

    The relay switch input will be A in that diagram.

    The coil connections are marked DC 12V in your image. (Red is +)

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 4 years ago

    This is a simple way to implement the hysteresis function you want.

    This circuit takes a higher battery voltage to turn power on to the inverter than to turn power off.

    It is not clear at what voltage the coil turns off - you will need to experiment.

    If the circuit is turning off at too low of a voltage, add more diodes in series with D4 until it turns off at the voltage you want.

    You will need to figure out which screw terminal to connect to the inverter - it will be C or D in colporteur diagram above.

    The relay switch input will be A in that diagram.

    The coil connections are marked DC 12V in your image. (Red is +)

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer