Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum FAIRCHILD SEMICONDUCTOR - MOC3052-M
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 325 subscribers
  • Views 562 views
  • Users 0 members are here
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

FAIRCHILD SEMICONDUCTOR - MOC3052-M

Former Member
Former Member over 14 years ago

hi i have a question here...what is the difference between MOC3052-without zero crossing circuit and MOC3081-MMOC3081-M with zero crossing circuit? can i replace MOC3052 to MOC3081?

  • Sign in to reply
  • Cancel

Top Replies

  • RWM
    RWM over 14 years ago +1
    It depends on application. MOC3081-M MOC3081-M is intended for on/off switching of load and MOC3052 can also be used for e.g. dimming. MOC3081 with zero crossing circuit switches on when voltage is rising…
  • RWM
    0 RWM over 14 years ago

    It depends on application. MOC3081-MMOC3081-M is intended for on/off switching of load and MOC3052 can also be used for e.g. dimming. MOC3081 with zero crossing circuit switches on when voltage is rising from zero, so it can switch on load generating low noise, but cannot be used when phase control is needed. MOC3052 can swich on load at different phases, so it can be used in dimmer, motor speed control etc.

    Additionally MOC3081-MMOC3081-M has higher LED trigger current (15mA) than MOC3052 (10mA).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Nicos_2023.
    0 Nicos_2023. over 2 years ago

    There is another type of  MOC30xx who works exactly like MOC3052 but has higher maximum working voltage (e.g. 800 V instead of 600 V ?)

    thanks !

    Nicos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer