Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum led driver circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 27 replies
  • Subscribers 321 subscribers
  • Views 4347 views
  • Users 0 members are here
  • led
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

led driver circuit

terrenone
terrenone over 11 years ago

I need some help with a circuit I need to drive 10 white leds from a 3.7v 2200mAh lipo battery it sounds simple but it has to be able to fit in a small container aproximity 1inch square and not produce a lot of heat,  its for my son's night im making.


Any help is welcome

Thanks

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    In this case I would be tempted to replace the 10 LEDs with a single 1 or 3W LED, it will fit easier and can be driven from the 3.7V LIPO with a simple constant current generator with minimal power loss…
  • jw0752
    jw0752 over 11 years ago in reply to terrenone +1
    That sounds good Dave. The battery and charging question is resolved. Let me know how your testing of the 5mm LEDs go on the 3.7Volt source. Since you are going to be dealing with relatively low mA I do…
  • jw0752
    jw0752 over 11 years ago in reply to Robert Peter Oakes +1
    Hi Peter - Whenever I try to answer one of these questions I am always pleased when one of the fellows, like yourself, with more knowledge and experience add their insight. I have come back to your recommendation…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    In this case I would be tempted to replace the 10 LEDs with a single 1 or 3W LED, it will fit easier and can be driven from the 3.7V LIPO with a simple constant current generator with minimal power loss, anything else will probably dissipate as much heat in the resistors as the LEDs them selves.

     

    something like this should last close to 7Hrs on that battery http://www.newark.com/cree/mx6awt-a1-r250-000d51/led-high-brightness-cool-white/dp/25R3684?ost=MX6AWT-A1-R250-000D51

     

    the trick is to not let the battery get too flat or it will destroy it (The battery), so some kind of cut off circuit will be needed

     

    I assume your making some kind of night light ?

     

    peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter - Whenever I try to answer one of these questions I am always pleased when one of the fellows, like yourself, with more knowledge and experience add their insight. I have come back to your recommendation for a constant current generator to power the LEDs to try to learn something new. I have attempted to build a constant current generator using a MOSFET and a 741 OP amp. While I can get it to work just fine at higher voltages I have not been able to get it to work under the circumstances that Dave is encountering. He has a 3.7 volt battery and the White LEDs have a forward junction voltage of 2.8 volts. Did you have a circuit in mind for this application or were you thinking of using a larger supply voltage than 3.7 volts? I am guessing that my circuit is not working as there is only 0.9 volts to work with between the LED's and the battery's 3.7 volts. I know you are currently busy with your project so there is no rush in answering this.

    Thanks John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 11 years ago in reply to jw0752

    Hello John,

     

    Although I don't have your circuit (you could post it) I suspect that your constant current source won't work at low supply voltages because you are using  a 741 op amp. This device was first designed and sold by Fairchild in 1968 so the design is 46 years old. Things have moved on.

    Looking at the TI data sheet (SNOSC25C –MAY 1998–REVISED MARCH 2013):

    The part is only specified for operation with +/- 15V supplies - it'll work with less but they don't guarantee anything.

    The input voltage range is worst case +/- 12V - this means that if either input gets within 3V of the supply rails then the amplifier won't work properly, so the least supply you could ever use is 6V.

    The output voltage swing is worst case +/- 12V so once again it can't drive near the supply rails.

     

    For your current source application pick a rail to rail input and output op amp (often described as RRIO in data sheets) so that you can work with inputs and outputs near the supply rails. Pick one which is specified to work with a 3V or less supply, (but OK with maximum).

     

    You could consider the Microchip MCP6281 but watch out for the maximum 5.5V supply.

    It is getting hard to find the spec you need in dual in line packages - there is much more choice in surface mount.

     

    Make sure the MOSFET in the current source will turn on enough with the gate voltage you have available.

     

     

    MICROCHIP  MCP6281-E/PMCP6281-E/P OP AMP 5MHZ SINGLE PDIP8 6281

     

     

    MICROCHIPMCP6281-E/P
    Image is for illustrative purposes only.
    Please refer to product description

     

    Manufacturer:
    MICROCHIP
    Order Code:
    1439456
    Manufacturer Part No:
    MCP6281-E/PMCP6281-E/P
    MK
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to michaelkellett

    Hi Michael -Thanks for your insight. You are surely correct. I took the circuit esign from an example in "Practical Electronics for Inventors" and I am sure it wasn't intended for a 3.7 volt source. Your comment is exactly what I like about this site. I learn new things and am starting to progress from the 46 year old technology that has been the basis of my electronics for too long. I lament the loss of the through the hole components as they were easy to work with but I am finding ways to adapt to the surface mount. Hopefully I can learn to use the surface mount before they come out with the next big paradigm shift in design. I will research the MCP 6821.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago in reply to michaelkellett

    Hi Michael -Thanks for your insight. You are surely correct. I took the circuit esign from an example in "Practical Electronics for Inventors" and I am sure it wasn't intended for a 3.7 volt source. Your comment is exactly what I like about this site. I learn new things and am starting to progress from the 46 year old technology that has been the basis of my electronics for too long. I lament the loss of the through the hole components as they were easy to work with but I am finding ways to adapt to the surface mount. Hopefully I can learn to use the surface mount before they come out with the next big paradigm shift in design. I will research the MCP 6821.

    John