Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum led driver circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 27 replies
  • Subscribers 320 subscribers
  • Views 4312 views
  • Users 0 members are here
  • led
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

led driver circuit

terrenone
terrenone over 11 years ago

I need some help with a circuit I need to drive 10 white leds from a 3.7v 2200mAh lipo battery it sounds simple but it has to be able to fit in a small container aproximity 1inch square and not produce a lot of heat,  its for my son's night im making.


Any help is welcome

Thanks

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    In this case I would be tempted to replace the 10 LEDs with a single 1 or 3W LED, it will fit easier and can be driven from the 3.7V LIPO with a simple constant current generator with minimal power loss…
  • jw0752
    jw0752 over 11 years ago in reply to terrenone +1
    That sounds good Dave. The battery and charging question is resolved. Let me know how your testing of the 5mm LEDs go on the 3.7Volt source. Since you are going to be dealing with relatively low mA I do…
  • jw0752
    jw0752 over 11 years ago in reply to Robert Peter Oakes +1
    Hi Peter - Whenever I try to answer one of these questions I am always pleased when one of the fellows, like yourself, with more knowledge and experience add their insight. I have come back to your recommendation…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Dave, Do you have any idea what the junction voltage is on your LEDs? Do you have parts like wires and resistors so you can do some experimenting? If I was going to do this I would start by putting 2 LEDs in series with a 300 ohm resistor and then hook it to the battery to see if it lights. You will have to mind the polarity of the LEDs so that they are hooked anode to cathode. If it lights, I would experiment with increasing the resistor to 470 ohms and then to 560 ohms. We are looking for the point where we feel that the LEDs are still bright enough for your purpose. I would then make up 4 more series strings using the other LEDs and a similar resistor for each string. I would then put all 5 strings in parallel across the battery. This will power all 10 LEDs safely and at a minimum current drain on the battery. Make sure your battery has internal control circuitry or you might discharge it below the level where damage can occur to the battery. If each string can be powered at 10 mA and your battery is in good shape you should get close to 2 days of light before it quits.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Hi Dave, Do you have any idea what the junction voltage is on your LEDs? Do you have parts like wires and resistors so you can do some experimenting? If I was going to do this I would start by putting 2 LEDs in series with a 300 ohm resistor and then hook it to the battery to see if it lights. You will have to mind the polarity of the LEDs so that they are hooked anode to cathode. If it lights, I would experiment with increasing the resistor to 470 ohms and then to 560 ohms. We are looking for the point where we feel that the LEDs are still bright enough for your purpose. I would then make up 4 more series strings using the other LEDs and a similar resistor for each string. I would then put all 5 strings in parallel across the battery. This will power all 10 LEDs safely and at a minimum current drain on the battery. Make sure your battery has internal control circuitry or you might discharge it below the level where damage can occur to the battery. If each string can be powered at 10 mA and your battery is in good shape you should get close to 2 days of light before it quits.

    John