Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum led driver circuit
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 27 replies
  • Subscribers 320 subscribers
  • Views 4332 views
  • Users 0 members are here
  • led
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

led driver circuit

terrenone
terrenone over 11 years ago

I need some help with a circuit I need to drive 10 white leds from a 3.7v 2200mAh lipo battery it sounds simple but it has to be able to fit in a small container aproximity 1inch square and not produce a lot of heat,  its for my son's night im making.


Any help is welcome

Thanks

Dave

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    In this case I would be tempted to replace the 10 LEDs with a single 1 or 3W LED, it will fit easier and can be driven from the 3.7V LIPO with a simple constant current generator with minimal power loss…
  • jw0752
    jw0752 over 11 years ago in reply to terrenone +1
    That sounds good Dave. The battery and charging question is resolved. Let me know how your testing of the 5mm LEDs go on the 3.7Volt source. Since you are going to be dealing with relatively low mA I do…
  • jw0752
    jw0752 over 11 years ago in reply to Robert Peter Oakes +1
    Hi Peter - Whenever I try to answer one of these questions I am always pleased when one of the fellows, like yourself, with more knowledge and experience add their insight. I have come back to your recommendation…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    The problem in driving LEDs is that they don't have the linear I/V that resistors do:  Let's imagine a one-volt potential driving a one Ohm resistor or one Siemens conductor.  Current is an ampere and power dissipation is one watt.  Double the potential, Current is two amperes and power dissipation is four watts.  If we double the potential across a diode, current increases by about a factor of ten.  This rules out voltage control and necessitates current control.  The chopper mentioned by a prior poster is the way to go because it is the alternative to simply putting a ballast resistor in series, which often draws more power than the LED.  Indicator LEDs are fine with just the ballast resistor, otherwise, 'get to the choppah.'

     

    MK is correct (there I said it!) in observing that the canonical op-amp/sense resistor/transistor CCS has stability (and outright slowness) issues  It has been found that a unity-gain buffer in the feedback path makes life much better for this circuit.  Using it in this application makes the power Q get hot rather than the ballast resistor, for what that is worth.  Chopping with a current integrator makes for a situation in which most of the power actually goes into the LED.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 11 years ago

    The problem in driving LEDs is that they don't have the linear I/V that resistors do:  Let's imagine a one-volt potential driving a one Ohm resistor or one Siemens conductor.  Current is an ampere and power dissipation is one watt.  Double the potential, Current is two amperes and power dissipation is four watts.  If we double the potential across a diode, current increases by about a factor of ten.  This rules out voltage control and necessitates current control.  The chopper mentioned by a prior poster is the way to go because it is the alternative to simply putting a ballast resistor in series, which often draws more power than the LED.  Indicator LEDs are fine with just the ballast resistor, otherwise, 'get to the choppah.'

     

    MK is correct (there I said it!) in observing that the canonical op-amp/sense resistor/transistor CCS has stability (and outright slowness) issues  It has been found that a unity-gain buffer in the feedback path makes life much better for this circuit.  Using it in this application makes the power Q get hot rather than the ballast resistor, for what that is worth.  Chopping with a current integrator makes for a situation in which most of the power actually goes into the LED.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to D_Hersey

    Thanks Don, I always learn from your explanations. As soon as I started testing I could see that the LED wasn't acting like a resistive load. I will look into the Chopping current regulator. This wasn't my thread but I seem to have hijacked it.

    John