Experts, Learning and Guidance
  • Technologies
  • More
Experts, Learning and Guidance
Ask an Expert Forum Help with Making a RPM tacho Shift Light circuit open a 12v Relay
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experts, Learning and Guidance to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 341 subscribers
  • Views 5262 views
  • Users 0 members are here
  • ask_an_expert
  • led
  • rpm
Related
See a helpful answer?

Be sure to click 'more' and select 'suggest as answer'!

If you're the thread creator, be sure to click 'more' then 'Verify as Answer'!

Help with Making a RPM tacho Shift Light circuit open a 12v Relay

e14 Contributor
e14 Contributor over 11 years ago

Hi everyone, i have a few adjustable Tachometer Shift light Circuits that i want to use to turn on a relay when the led turns on.

The way they are set up now:
You can adjust the desired rpm Shift light value with a pot then when that rpm is reached the led turns on.

 

My problem is tracing it back to the IC or to the nearest transistor.
I'm trying to turn on a 12v relay when the desired rpm is reached.

 

So there are 2 ways i am thinking of doing this...


1: is to use a transistor to allow a higher current to run through the relay's solenoid to then allow me to run a separate 12v circuit to turn on more than 1 led light. i cant find where to run the transistor off or which pin on the ic is actually the "remote wire" for the led.


2: If i can't use a transistor is it possible to use a phototransistor and just use the built in led to then turn on a second circuit with a phototransitor linked to the relay's solenoid>


Any help would be greatly appreciated please find some pictures attached of the circuitimage







image

  • Sign in to reply
  • Cancel
Parents
  • supper_slash
    0 supper_slash over 11 years ago

    Please allow more specifics. Like.

     

    What are you needing out of the relay. (12V 1A)?

    SPST or DPDT?

     

    If so, here is an idea. Remove the led, replace it with a solid state relay, And replace the led off of the relay load side of the circuit.

     

    Off the top of my head here is a relay that may work. But you will need to look around and see if this will fit your needs.

    You may need a DPDT, or something handling more power, etc.

     

    But let me know what you think of this solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to supper_slash

    It may also be possible to use a low voltage (On the input) solid state relay , this would provide isolation and an easy interface ?, optionally an opto isolator in series or replacing the LED in question with same result

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    Thankyou for your replies,

     

    I have a fairly good understanding of simple electronics and some more technical things but IC's and this style circuit are still new to me.

     

    I didn't understand this circuit and what the led was actually doing.

     

    when i tested it with a multimeter and connecting between the pos or neg pins on the led i was always getting voltage even when the led was off just when the shift light was turned on i was getting more.

     

    I only need a spst relay on it and about 1-2 amps would be max if i needed more i could run a larger relay off that one anyway.

     

    i tried unsoldering the led and running a relay off the same pins but it didnt work because it wasnt turning it on or off and of course the voltage at the pins is 3.5v for the blue led so unless i can get a relay that has a 3-5v turn on then can handle 12v through?

     

    hope this helps a little sorry for my lack of knowledge 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    the LED drivers will not have anything close to the power needed to turn on a relay, you will need to use an opto isolator or at least a transistor to do the job

     

    See this for a bit of a backgrounder http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/drive-big-things-with-added-safety-opto-isolators

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to e14 Contributor

    the LED drivers will not have anything close to the power needed to turn on a relay, you will need to use an opto isolator or at least a transistor to do the job

     

    See this for a bit of a backgrounder http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/drive-big-things-with-added-safety-opto-isolators

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to Robert Peter Oakes

    I checked out your link Peter.

    I have also tried to use a transistor on the led leg without any success. I wasnt sure what i exactly needed or what would work. When testing i know it always had voltage between both pins of the leds and their opposing supplies.

     

    For example when i tested the voltage between the pos pin on the led and the ground i got a voltage and then the same thing happened between the neg pin on the led and the positive supply even when the led was turned off yet no voltage between the led's pins themselves.

     

    I think from memory the negative pin was earthed straight to the negative so must have some form of positive change when reaching the desired rpm from the frequency- voltage chip.

     

    so if it is a "switched positive" is there a particular type of npn transistor i need to use or is there a huge range that would work?

     

    Thankyou.